Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Würth Elektronik Phototransistor Optocoupler - Isolation Characteristics

Next to the CTR value, the isolation characteristics are important to the customer. In terms of safety, creepage, clearance, and the insulation thickness are the most important parameters. The creepage is the shortest path along the surface and the clearance is the shortest path through air. The insulation thickness is the minimum thickness of insulating material. Additional information can be found in the VDE, UL, and CQC certificates.

PTM פורסם ב: