Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
ECF40 Series of 40W Open Frame Power Supplies Slide 8

In summary, the ECF40 is a 40 W AC-DC open frame power supply in a compact package and with an incredibly low profile making it one of the smallest 40 W power supplies XP has ever produced. This miniature size is achieved while maintaining a specification every bit as good as the current larger product and superior to many of the models currently available in the market. The series carries both ITE and medical safety approvals, enabling engineers to address applications in the industrial, technology and healthcare markets. The ECF40 cements XP Power’s position as one of the leading manufacturers of low power AC-DC open frame power supplies.

PTM פורסם ב: