Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Specifications

The resistance value of a platinum RTD temperature sensor is specified at 0ºC. A variety of nominal resistance values provides circuit design flexibility. For example, using higher resistance value elements such as Pt 1000 minimizes the error introduced by extension wires and eliminates the need for 4-wire connections to the RTD element. Tolerance classes are defined by DIN EN 60751, which is identical to the international standard IEC 60751.

PTM פורסם ב: