Titanium TI375 C529 Development Kit - Unboxing | DigiKey
Inside the box, you’ll find the Titanium Ti375 C529 development board, a 12 volt cooling fan, a heat sink, a 12 volt power adapter with a DC jack converter, 4 standoffs, and some additional hardware.
https://www.digikey.com/en/products/detail/efinix-inc/TI375C529C-DK/23026034
The board features high speed QSE connectors, PMOD interfaces, gigabit Ethernet, an FPGA mezzanine card with a low pin count connector, an SMA interface, RTC function support, user LEDs, and pushbutton switches. Additionally, users have access to a free Efinity® software license with 1 year of upgrades to provide a complete tool flow that includes synthesis, place and route, debugging, and timing analysis.
To demonstrate the multi-core design capability, the development board comes preloaded with an ASCII spinning donut example that’s rendered through UART.
To run the example, attach the standoffs and connect the board to your computer and plug in the 12 volt power adapter, with the PSW1 switch in the off position. Turn on the power switch and press the SW1 push button. The board LEDs will start blinking from left to right. Open a terminal on your PC. Select the serial COM port and set baud rate to 115200, data to 8 bits, stop bit to 1, and parity bit to none.
Now, press the SW4 push button to start streaming the donut program through UART.
Learn more: Maker.io - https://www.digikey.com/en/maker DigiKey’s Blog – TheCircuit https://www.digikey.com/en/blog Connect with DigiKey on Facebook https://www.facebook.com/digikey.electronics/ And follow us on X https://twitter.com/digikey