מאמרים ובלוגים

Image of What Is Cybersecurity and Why Is It Important? What Is Cybersecurity and Why Is It Important?

Small steps can help reduce the risk of cyber-attacks on peripheral devices which typically use default passwords or outdated software.

Image of Solve the Mil/Aero COTS Challenge with SET-Tested Interconnects Solve the Mil/Aero COTS Challenge with SET-Tested Interconnects

Samtec’s Severe Environment Testing (SET) brings Sudden Service to mil/aero applications; learn how URSA I/O and Tiger Eye solve the COTS connector challenge.

Image of Utilizing GMSL for High Bandwidth Robotic Vision Applications Utilizing GMSL for High-Bandwidth Robotic Vision Applications תאריך פרסום: 2026-04-23

ADI's GMSL simplifies the development of high-bandwidth, low-latency robotic vision applications.

Image of Power Resistor Selection Tips for Industrial Motor Drives Power Resistor Selection Tips for Industrial Motor Drives תאריך פרסום: 2026-04-22

Learn how carefully selected power resistors with specialized architectures solve inrush, braking, and thermal challenges in industrial motor drives.

Image of Webinar – Making CO2 Sensing Mainstream: Miniaturized, Efficient, and Cost Optimized Webinar – Making CO2 Sensing Mainstream: Miniaturized, Efficient, and Cost Optimized

This webinar will dive into how to overcome traditional CO2 sensor constraints without sacrificing performance.

Image of Beginner Parts Kit Identification Guide Beginner Parts Kit Identification Guide

In this tutorial, we'll provide a quick rundown of each part in the kit, to help reinforce your understanding of the component. For some parts, we'll include an example application, in case you're in need of a circuit to plug your new toys into.

Image of How ODU MINI-SNAP® & ODU MEDI-SNAP® Elevate the Catheter Market with Connector Solutions How ODU MINI-SNAP® & ODU MEDI-SNAP® Elevate the Catheter Market with Connector Solutions

ODU MEDI-SNAP® interconnect solutions have IEC 60601-1 compliance, sterilization compatibility, rapid custom prototyping, and regulatory alignment.

Image of Resistor-Integrated Microswitches Improve System Reliability Through Four-State Detection Resistor-Integrated Microswitches Improve System Reliability Through Four-State Detection תאריך פרסום: 2026-04-21

Resistor-integrated microswitches simplify wiring and improve system reliability with four-state detection for self-diagnosis and remote fault monitoring.

Image of How Hardware Gets Hacked (Part 3): Adopting the Attacker Mindset How Hardware Gets Hacked (Part 3): Adopting the Attacker Mindset

Explore how attackers gather device info, map inputs, and uncover vulnerabilities using reconnaissance in embedded hardware security.

Image of Webinar – Technologies Driving Drones, Autonomy, and eVTOL Webinar – Technologies Driving Drones, Autonomy, and eVTOL

This webinar introduces how the Schneider Electric Altivar™ ATV320 variable frequency drive helps address motor control challenges.

Image of Piezoelectric Ceramics: Driving the Silent Interaction Revolution Piezoelectric Ceramics: Driving the Silent Interaction Revolution

Piezoelectric ceramic technology generates an electric charge when subjected to mechanical stress and undergoes deformation when an electric field is applied.

Image of Kitronik Arcade for BBC micro:bit and MakeCode Arcade Kitronik Arcade for BBC micro:bit and MakeCode Arcade

If you want to learn to code, learning to write games is a great way to get started, and our new hand held gamer has everything you need right now and it also has the connectivity for everything you might need tomorrow.

Image of Selecting Power Supplies for Harsh Industrial Applications and Hazardous Locations Selecting Power Supplies for Harsh Industrial Applications and Hazardous Locations תאריך פרסום: 2026-04-16

Designers of industrial systems for harsh and potentially explosive environments must select power supplies that prioritize reliability and safety.

Image of Webinar – Programming Hardware Two Ways: CircuitPython and Verilog Webinar – Programming Hardware Two Ways: CircuitPython and Verilog

This webinar introduces embedded system design through both the software and hardware abstraction levels.

Image of Optimize High-Current Buck-Boost DC/DC Converter Efficiency אופטימיזציה של נצילות ממיר DC/DC‏ Buck-Boost‏ עם זרם גבוה תאריך פרסום: 2026-04-15

השתמשו במייצבי Buck-Boost‏ μModule‏ עבור שלוש גישות ארכיטקטוניות לשילוב משרנים וחישת זרם עבור המרת DC/DC‏ עם זרם גבוה.

Image of Webinar – Topology is Just the Start: Building Reliable Wide-Input SEPIC Converters Webinar – Topology is Just the Start: Building Reliable Wide-Input SEPIC Converters

Achieve a robust, production worthy design by understanding component behavior, electrical stress, and practical design limits by selecting the SEPIC topology.

Image of Sound Generation and Musical Microcontrollers Sound Generation and Musical Microcontrollers

Explore audio output options, including piezos, speakers, DACs, and playback boards for creating music and sound effects in microcontroller projects.

Image of Understanding Field Programmable Analog Arrays in Modern Mixed-Signal Design הבנת מערכים אנלוגיים ניתנים לתכנות בשטח בתכנים מודרניים של אותות מעורבים תאריך פרסום: 2026-04-14

מערכים אנלוגיים ניתנים לתכנות בשטח (FPAAs) מציעים את האפשרות של הגדרת פונקציונליות אנלוגית באמצעות תוכנה במקום שרשרות אותות אנלוגיים קבועות בחומרה.

Image of Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1) Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1)

Developing prosthetic technology that is both affordable and functional is challenging in today’s space, mainly due to the costly fabrication and specialized calibration requirements.

Image of Building a Dynamometer for the Openwheel Project - Part 1 Building a Dynamometer for the Openwheel Project - Part 1

Explore a custom-built dyno for hub motors using load cells and Arduino, enabling accurate power and torque measurements.