Maker.io main logo

Furby 2023 Teardown

1,980

2023-11-29 | By bekathwia

Welcome to another teardown! Furby 2023 edition. This new edition of the classic interactive toy is more reminiscent of the original than the 2012 version, which I also took apart at the time.

In addition to its classic touch interactivity with buttons and sensors, this new Furby also has voice recognition, differentiating between three different phrases.

It’s so friendly and not at all creepy like the last one, in my opinion, anyway. I found it almost too cute to take apart. Almost.

Thanks to David Cranor for lending his EE expertise and to Lumafield for the 3D scan.

Tools used in this teardown:

Furby 2023 Teardown

Furby 2023 Teardown

Furby 2023 Teardown

Taking apart Furby starts with the fur. The fabric is sewn to these little plastic tabs that fit into the enclosure. Nothing is glued here.

Once it’s fabric free, it becomes apparent that a few screws hold the front and back of the plastic enclosure together. Removing them and the plastic revealed even more screws.

I managed to remove all the various circuit boards like the main one that everything else plugs into, the one holding the LED in the ear and switches inside the face.

I disassembled the rest of her by undoing as many screws as I could find until I got to the sticky motor area. Since my friends at Lumafield put this thing in their CT scanner before I took it apart, I let my urge not to get motor grease all over the place express itself.

Furby 2023 Teardown

Furby 2023 Teardown

Furby 2023 Teardown

The main board has connectors to receive the plugs coming from various components throughout the Furby.

Here are all the components we could identify:

  1. W1084S 2113H - DC motor driver
  2. 25L3233F M2I-08G 22B2348 L224624 - Flash memory
  3. B1F69 - Step-Up DC-DC Converter
  4. Tilt ball switch
  5. LP16 110 - PTC fuse
  6. Microphone
  7. Inductor
  8. Microcontroller under an epoxy blob

You can explore the scans of the 2023 Furby on Lumafield.

Furby 2023 Teardown

Furby 2023 TeardownFlash memory

Furby 2023 TeardownDC motor driver

Furby 2023 TeardownInductor

Furby 2023 TeardownPower conversion circuitry, including step-up converter

Furby 2023 TeardownUnknown

Furby 2023 TeardownTilt ball switch for determining when Furby is lying down and being shaken

Furby 2023 TeardownConnectors on the main board

Furby 2023 TeardownMicrophone

Furby 2023 TeardownTongue switch

Furby 2023 TeardownEar LED board

Furby 2023 TeardownForehead gem LED/switchboard

Furby 2023 Teardown

Furby 2023 TeardownCT scan of Furby

Furby 2023 TeardownThe rotary encoder is visible in the upper right corner

Furby 2023 TeardownGearbox contains tracks to shape the motion of the ears, eyes, and feet

Furby 2023 TeardownGearbox and top of battery compartment

מק"ט יצרן # 92 28 72 ESD
PRECISION TWEEZERS ESD
Knipex Tools LP
מק"ט יצרן # PA1180
PLIERS NEEDLE NOSE
Tempo Communications
מק"ט יצרן # 32614
POCKET PRECISION 4-IN-1 SCREWDRI
Klein Tools, Inc.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.