Maker.io main logo

Introducing the Raspberry Pi 500: A Leap in All-in-One Computing

1,157

2025-02-12 | By Travis Foss

Single Board Computers Raspberry Pi SBC

TL;DR: The Raspberry Pi 500 integrates a Raspberry Pi 5–class 2.4GHz Cortex A76 processor, 8GB LPDDR4X memory, improved ISP, and a redesigned, easier-to-access port layout into a sleek keyboard-style all-in-one computer. A dedicated power button, Kensington lock, and right side GPIO header modernize its usability, while the newly introduced 15.6″ Pi Monitor provides a portable Full HD USB-C powered display with built-in speakers. Together, they deliver a compact, affordable desktop experience ideal for learning, programming, and everyday multitasking — with NVMe and mechanical keyboard features available only in the Pi 500+ variant.

Introducing the Raspberry Pi 500: A Leap in All-in-One Computing

Raspberry Pi has recently announced the highly anticipated Raspberry Pi 500, the next evolution of their all-in-one computer in a keyboard form factor. Packed with powerful upgrades over its predecessor, the Pi 400, this sleek device combines cutting-edge features with the simplicity Raspberry Pi is known for.

The Pi 500 is equipped with the Broadcom BCM2712D0 processor, which boasts a quad-core Arm Cortex A-76 architecture. This processor operates at a remarkable speed of 2.4 GHz, matching the performance specifications found in the Raspberry Pi 5. In addition to its powerful processing capabilities, the Pi 500 integrates Raspberry Pi’s custom-developed Image Signal Processor (ISP). This ISP significantly enhances the device's multimedia performance, allowing for improved image and video processing.

Introducing the Raspberry Pi 500: A Leap in All-in-One Computing

Key Features of the Pi 500

  • 8GB LPDDR4X-4267 SDRAM for faster multitasking and smoother performance.
  • Two USB 3.0 ports supporting simultaneous 5Gbps operation, plus one USB 2.0 port.
  • A dedicated power button for convenient operation, echoing the Pi 5 case.
  • A Kensington lock to secure your device in shared or public spaces.

Thoughtful Design Enhancements

A closer look reveals subtle yet meaningful changes in the Pi 500’s layout:

  • The GPIO header now resides on the right side, next to the Gigabit Ethernet port, for easier accessibility.
  • USB ports have shifted to the left, with the USB 2.0 port, typically used for a mouse connection, farthest left and the two USB 3.0 ports beside it.
  • The Micro SD card slot, USB-C power connector, and dual micro-HDMI connectors are neatly aligned for streamlined connectivity.

Introducing the Raspberry Pi 500: A Leap in All-in-One Computing

Enhance Your Pi 500 with the Raspberry Pi Monitor

To heighten your experience with the Pi 500, Raspberry Pi proudly introduced the Pi Monitor, a sleek and portable 15.6" display that perfectly complements the new keyboard computer, making it an essential addition for every tech enthusiast.

Introducing the Raspberry Pi 500: A Leap in All-in-One Computing

Pi Monitor Highlights

  • 1920 x 1080 Full HD resolution on a vibrant IPS LCD panel with 16.2 million colors.
  • Powered efficiently via USB-C, with the ability to run directly from a Raspberry Pi USB port at reduced brightness.
  • Built-in 2 x 1.2W speakers and a 3.5mm headphone jack for versatile audio options.
  • HDMI connectivity for seamless pairing with other devices.

With its sleek design and energy efficiency (just 1A at 5V DC), the Pi Monitor is ideal for work, learning, or entertainment.

Introducing the Raspberry Pi 500: A Leap in All-in-One Computing

The Pi 500 and Pi Monitor are the ultimate duo for an exceptional computing experience. Together, they deliver powerful performance in a portable and affordable package. Transform your setup today with the Raspberry Pi 500 and Pi Monitor—where innovation meets accessibility.

מק"ט יצרן # SC0940
MONITOR 15.60" NON-TOUCH
Raspberry Pi
מק"ט יצרן # SC1228
MONITOR 15.60" NON-TOUCH
Raspberry Pi
מק"ט יצרן # SC0442
RASPBERRY PI MOUSE RED
Raspberry Pi
מק"ט יצרן # SC0202
RASPBERRY PI MOUSE BLACK
Raspberry Pi
מק"ט יצרן # SC0358
CBL HDMI-A M TO MCR HDMI-D M 1M
Raspberry Pi
מק"ט יצרן # SC0546
CBL HDMI-A M TO MCR HDMI-D M 1M
Raspberry Pi
מק"ט יצרן # SC0224
WHITE MICROHDMI TO STANDARD ADAP
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.