Maker.io main logo

Introduction to the Raspberry Pi GPIO and Physical Computing

876

2024-12-31 | By SparkFun Electronics

License: See Original Project Single Board Computers Raspberry Pi SBC

Courtesy of SparkFun

Guide by asassy

Introduction

If you’ve recently picked up your first Raspberry Pi, congrats on purchasing perhaps the cheapest ‎and smallest computer you’ll ever own! However, it sure doesn’t look like any computer you’re ‎accustomed to, so let’s talk through the basics to get your Raspberry Pi up and running as a full ‎desktop. We're also going to learn to interact with the GPIO and hook up an atmospheric sensor to ‎read in some data with Python.‎

parts_1

We'll be reading data from an atmospheric sensor with the Raspberry Pi.‎

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.‎

qwiic_2

The Qwiic Connect System is designed to keep your projects moving.‎

We would also recommend taking a look at the following tutorials and if you aren't familiar with them.‎

Hardware Overview and Hookup

As the Raspberry Pi is a fully functioning computer, it needs the peripherals that a computer you ‎may be accustomed to has to be fully interactive. We’ll need six crucial components to get the ‎Raspberry Pi up and running, but we’ll also take a look at some additional hardware that are often ‎times used with the Pi. Let’s start with what’s required!‎

General hardware for setup

  • Monitor - A monitor is basically required for the initial setup and configuration of the operating ‎system. If you’ll be using SSH to connect to your Raspberry Pi, then you won’t need the ‎monitor after setup (Check out this tutorial that walks you through SSH and the Pi!) Make sure ‎your monitor has an HDMI input.‎

  • microSD Card - The microSD Card stores the operating system and files. If you bought a kit, ‎the microSD card might have already been formatted for use. Otherwise, you’ll to manually ‎install an OS’s image onto the microSD card to load it on your Pi

  • Keyboard and Mouse - You can either buy these together (the mouse is a part of the ‎keyboard) or separately

  • HDMI Cables - You’ll need an HDMI cable to connect the Raspberry Pi to a monitor. Different ‎Raspberry Pi models have different HDMI cable requirements, but the newest model ‎‎(Raspberry Pi 4) requires an HDMI to Micro HDMI Cable.‎

  • Power Supply - Different Raspberry Pi models have different USB connections and power ‎requirements, but the newest model (Raspberry Pi 4) requires a USB Type C to C Cable and ‎Wall Adapter.‎

Additional hardware

  • Heat Sink - Heat sinks are popular for users who are overclocking the CPU, so the Pi is ‎running too hot. If the temperature of the CPU becomes too hot, a heat sink will passively cool ‎air near the CPU to assist in cooling the processor. The heat sink can double as somewhat of ‎a protective case as well. If you think you might need a heat sink, you can use the following ‎command in the terminal to see the temperature of your Pi: hot./opt/vc/bin/vcgencmd ‎measure_temp

  • Case - Since the Raspberry Pi comes as an exposed circuit board, you might want to protect it ‎from dust and damage with a case. A variety of companies make cases for the Pi; perhaps the ‎most notable case is the Raspberry Pi 400, which essentially uses a keyboard as a case for the ‎Raspberry Pi. Built by the Raspberry Pi Foundation, it extends the Pi ports through the back of ‎the keyboard as to not limit intractability.‎

  • Ethernet Cable - Depending on the Raspberry Pi model you have, and if you'd like to bypass ‎wireless connections, pick up an ethernet cable to plug into the world wide web!‎

  • Speakers - If you'd like to play music or sound from your Pi, you'll need a set of speakers. ‎Any standard set of speakers with a 3.5 mm jack should do...they will connect into the AV jack ‎on the side of the board.‎

Quick Note on the Different Raspberry Pi Versions

The Raspberry Pi comes in a variety of form factors and generations - Zero, 2, 3, etc., - for ‎different use cases. The layout varies slightly between the boards, but most of the connections are ‎the same. For the purpose of this tutorial, we'll be focusing on the most recent version, ‎the Raspberry Pi 4. Still, if you're using another model, double check the connections required by ‎consulting the hookup guide for the exact model when collecting the hardware you need.‎

Specific Hardware Required

SparkFun Raspberry Pi 4 Desktop Kit - 4GB‎

Lucky for us, SparkFun has a kit that practically does the work for you in supplying the appropriate ‎hardware and supporting the least frustrating experience possible - the SparkFun Raspberry Pi 4 ‎Desktop Kit includes the following:‎

  • Raspberry Pi 4 - 4GB Model‎

  • Logitech K400 Plus Wireless Keyboard with Touchpad

  • Kingston Canvas Go! Plus 64GB MicroSD Card with Adapter

  • USB Type C to Type C Male Cable (1 Meter)‎

  • USB Type C Wall Adapter

  • Metal Heatsink Case with Thermal Tape - Black

  • HDMI to Micro HDMI Cable

  • SparkFun Qwiic SHIM for Raspberry Pi

The dark horse of this kit is the aforementioned Qwiic SHIM, which is a crucial component that we ‎will use to interact with the GPIO later on in this tutorial.‎

SparkFun Atmospheric Sensor Breakout - BME280

We will also utilize one of the BME280 environmental breakout because it has a wide variety of ‎precise data to offer and can be connected through Qwiic, which means we won't be hindered by ‎soldering and can get right into coding.‎

Putting it All Together

Fortunately, there is very little additional knowledge for putting it all together. Simply connect the ‎mouse and keyboard via USB, the power supply via USB-C (don't forget to plug the other end into a ‎wall adapter), the HDMI into the both the monitor and the Pi and load the microSD card into its slot. ‎Besides making sure the wires don't crisscross and make a mess, you're ready to start your desktop ‎computer!

connections_5

GPIO Pins Overview

Okay, so we've hooked up the necessary hardware to the Raspberry Pi, and you're itching to start ‎using it as a general-purpose PC for web surfing and YouTube watching and looking at cat memes. ‎But where the Pi really shines is with its 40-pin GPIO (General Purpose Input & Output). The GPIO ‎enables you to switch devices on and off (output) or receive data from sensors and switches (input). ‎What this really means is that you can connect the Raspberry Pi to everything from a smart mirror to ‎a weather station, to an asset tracking robot that displays its coordinates on a web server. Let's take ‎a deeper dive into what's possible with the GPIO header! We can reference the GPIO Pinout ‎Diagram provided by the Raspberry Pi Foundation below as a visual guide for understanding the ‎pins:‎

pins_6

Power Pins

Let's start with the power pins, which include both 3.3V and 5V. These pins transmit power as ‎output to power attached peripherals.‎

Ground

And if we’re going to be rigging up electrical circuits here with power, then we’ll need a ground. ‎You’ll find plenty of grounds within the pins as well.‎

Standard GPIO Pins

Take out the power and ground pins, and you’ll be left with the pins that are dedicated to sending ‎output and receiving input. All of these can be used for straightforward input/output tasks!‎

Chatty Cathy Pins

Some of the standard GPIO pins are used for communication purposes. Here's a quick overview of ‎these communication protocols!‎

  • SPI pins – The Serial Peripheral Interface (SPI) is a communication protocol used to transfer ‎data between micro-computers like the Raspberry Pi and peripheral devices. The MISO pin ‎receives data, and the MOSI pin sends data from the Raspberry Pi. Furthermore, the serial ‎clock pin sends pulses at a regular frequency between the Raspberry Pi and the SPI device at ‎the same speed in which the devices to transfer data to each other.‎

  • UART pins – UART stands for universal asynchronous receiver-transmitter, which is a ‎physical circuit designed to send and receive data.‎

  • PWM pins – PWM means “pulse width modulation,” which is a communication protocol best ‎used with stuff that moves and lights up: motors, LEDs, and so on.‎

  • I2C pins – I2C is short for inter-integrated circuit (two “inters” or I"squared"C). It works ‎similarly to SPI, but it doesn’t force you to use nearly so many pins.‎

Identifying Pins

There are two ways to identify GPIO pins...the first is by its physical position on the board, or its ‎BOARD name. It also has a Broadcom SOC channel (BCM) name. By opening the terminal and ‎running pinout as a command, it will return a map of the Raspberry Pi GPIO pins and their names ‎based on the Broadcom chip on board.

identify_7

Map for the Raspberry Pi 4 based on the pinout command.‎

If you really want to get deep into the Raspberry Pi GPIO pinout, there is an incredibly ‎thorough Raspberry Pi GPIO pinout guide that is interactive and steps through each type of pin on-‎board. This general overview outlined above should be enough to get us started on our project ‎though!‎

Operating System Setup

Okay, so the hardware is setup properly! If you picked up a kit like we did for this project, the ‎Raspberry Pi OS image should be installed on the microSD card. If you're using a blank microSD ‎card, you'll have to either visit The Raspberry Pi Foundation to install the appropriate image, or you ‎can install a different operating system image on the MicroSD card. Some other notable operating ‎systems are OSMC, RetroPie, Ubuntu, Rokos, and dozens others.‎

For the purpose of this tutorial, we will stick with Raspberry Pi's official supported operating system, ‎Raspberry Pi OS (formally known as Raspbian).‎

When the Raspberry Pi receives power and boots up, it will load the desktop with a glorious ‎wallpaper of the sun rising over Bagan, Myanmar.‎

system_8

It will quickly have a pop-up that will guide you through setting up the OS, including setting the ‎location, date, time, password, WiFi, and doing a few software updates. The screens should ‎progress like the images below, and then the Raspberry Pi will update.‎

Set country, language, and time zone

country_9

Change password to something other than password

password_10

Select your local WiFi network

network_11

The Pi will update the software

software_12

Once the Pi restarts, it will bring you back to main desktop page once more. The main menu on the ‎lower left is comprised of a lightweight open-source programs packaged within Raspbian.‎

desktop_13

Also, along the top right of the screen, you should see a globe icon for Chromium. This is your ‎Internet browser, and if you set up your network settings you can browse the web here. Next along ‎is the file manager, which allows you to browse the files on your SD card and external USB storage. ‎Finally, the black icon opens up Terminal. This allows you to type commands directly, and for ‎advanced users can be a faster and more flexible way to perform certain tasks.‎

There are other applications within the operating system that will prove useful for us, specifically a ‎text editor so that we can write and run code. For this project, we'll specifically use Thonny, which ‎is a Python(3) IDE that can both write and run code from the application. Another notable ‎application in Raspbian is VNC, which allows you to remotely control the desktop interface of your ‎Pi from another computer.‎

Python Overview and Reading in Sensor Data

The Raspberry Pi Foundation has specifically selected Python as the main language for Raspberry ‎Pi because of its ease of use, power, versatility, and open-source mentality. Python comes pre-‎installed on Raspbian, so you can load an IDE like Thonny and quickly start coding.‎

If you've never coded in Python before, be sure to check out our tutorial on Coding in Python...it ‎will get you up and running with variables, operators, objects, data structures, and much more. It will ‎be important to have a basic understanding of Python to interact with the GPIO, so knowing ‎variables, functions, operators, and classes is good, even if you just understand them at a high level ‎and can't write them yourself!‎

Using gpiozero to Interact With GPIO

We want to dip our toes into the world of physical computing with the world of Raspberry Pi, and ‎one way to do this is to learn to interact with the GPIO. There's a fantastic Python library ‎called gpiozero that makes it quite easy to interact with the GPIO, and it already comes pre-installed ‎on Raspbian.‎

In Python, libraries and functions used in a script must be imported by name at the top of the file, ‎so you can either import the entire library,‎

Copy Code
import gpiozero

or you can import just a component or two:

Copy Code
from gpiozero import Button

You'll need to set the GPIO pins you're using on the Pi to the respective component chosen with gpiozero. For example, if you have hooked up an LED to pin number 17 on the Pi, you could refer to it a multitude of ways with this Python library (remember how the GPIO pins can have many names?)

Copy Code
led = LED(17)
led = LED("GPIO17")
led = LED("BOARD11")

If you wanted to hook up an LED to pin 17 and a ground pin (along with a current limiting resistor), ‎you could blink the LED simply with the code below. It imports the LED component from the library, ‎as well as pause. After letting the board know what pin the LED is connected to, it will call that LED ‎to blink, and then pause.‎

Copy Code
from gpiozero import LED
from signal import pause

red = LED(17)

red.blink()

pause()

Using a breadboard and wires, you can practically hook up anything to the GPIO and interact with it ‎through gpiozero.‎

Using the Qwiic Way to Interact With GPIO

For our project, we want to hook up a Qwiic sensor to the Raspberry Pi, so we'll actually use ‎the Qwiic SHIM included in the kit. We can just align the Qwiic SHIM with Pin 1 on the GPIO header, ‎and slide it in. We don't need to assign which pins we're using - the SHIM is aligned with Pin 1 - but ‎we do need import other libraries that are necessary for the additional atmosphere sensor.‎

With your Qwiic SHIM mounted on your Pi it should look like this:‎

shim_14

Qwiic SHIM mounted on a Pi 4.‎

sensor_15

Your sensor on the other end of the Qwiic Cable.‎

Copy Code
sudo pip install sparkfun-qwiic-bme280

Now, we can import the BME280 library, as well as a time and system library to read in some basic ‎temperature values. We'll need to ensure that the BME280 set to a variable, connected to the ‎system, and then begin running the sensor like we would with Arduino.‎

The library that's important here is the qwiic_bme280. As you can see, the sensor itself will be set ‎to mySensor the for the duration of the function, so whenever you see mySensor."something", it is ‎calling an instance variable unique to each instance.‎

Copy Code
import qwiic_bme280
import time
import sys

def runExample():

    print("\nSparkFun BME280 Sensor + Raspberry Pi Example \n")
    mySensor = qwiic_bme280.QwiicBme280()

    if mySensor.isConnected() == False:
        print("The Qwiic BME280 device isn't connected to the system.", 
            file=sys.stderr)
        return

    mySensor.begin()

    while True:
        print("Humidity:\t%.3f" % mySensor.humidity)

        print("Pressure:\t%.3f" % mySensor.pressure)    

        print("Altitude:\t%.3f" % mySensor.altitude_feet)

        print("Temperature:\t%.2f" % mySensor.temperature_fahrenheit)       

        print("")

        time.sleep(1)

Challenge: How might you change the code above to only print the temperature if it exceeds 80 ‎degrees Fahrenheit? (Hint: Remember your operators!)‎

Solution:‎

Copy Code
import qwiic_bme280
import time
import sys

def runExample():

    print("\nSparkFun BME280 Sensor  Example 1\n")
    mySensor = qwiic_bme280.QwiicBme280()

    if mySensor.isConnected() == False:
        print("The Qwiic BME280 device isn't connected to the system.", 
            file=sys.stderr)
        return

    mySensor.begin()

    if mySensor.temperature_fahrenheit > 80:

        print("It's hot!")       

        time.sleep(1)
מק"ט יצרן # 15794
QWIIC SHIM FOR RASPBERRY PI
SparkFun Electronics
מק"ט יצרן # 15440
QWIIC BME280 ATMOSPHERIC SENSOR
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.