Maker.io main logo

Arduino IoT Glass Break Sensor

911

2025-01-14 | By Maker.io Staff

License: See Original Project LEDs / Discrete / Modules Arduino

Copy-of-cover

Learn how to build a cost-effective, cloud-connected intruder alert that detects when someone ‎tries to break a window. The project utilizes a handful of readily available standard electronics ‎components and a cloud-ready Arduino Nano 33 IoT.‎

Bill of Materials

‎In summary, this project employs a low-cost piezo element to detect vibrations. A transistor ‎amplifies and inverts the signal and triggers a 555-based circuit to generate pulses of predictable ‎length, which the Arduino subsequently detects. The following table lists all components that are ‎required for this project:‎

Quantity Item

‎1‎ Piezo Element

‎4‎ ‎10K Resistor‎

‎1‎ ‎470 Ohm Resistor‎

‎1‎ NPN Transistor

‎1‎ ‎33 µF Polarized Capacitor

‎1‎ ‎10nF Non-Polarized Capacitor

‎1‎ Red 5mm LED

‎1‎ NE555P Timer IC

‎1‎ Arduino Nano 33 IoT

The project’s simple and flexible nature allows the easy substitution of different development ‎boards for the Arduino to accommodate other setups. Similarly, tweaking the passive ‎component’s values allows for generating longer or shorter output pulses if necessary.‎

Understanding the Basic Glass-Break Sensor Circuit

‎The circuit is based around a standard 555 timer IC running in monostable mode. This mode is ‎often also called one-shot mode since the timer IC generates a single pulse of predictable ‎duration when its trigger pin is pulled low. The accompanying passive components determine the ‎generated pulse length. This project uses commonly available values of 10K for the resistor and ‎‎33µF for the capacitor, resulting in roughly one-third of a second output pulses with each trigger ‎event. You can use this handy online calculator to experiment with different values and see how ‎they affect the generated pulse duration.‎

However, the exact duration does not matter much in this project since the Arduino on the ‎receiving end of the output pulses only detects rising edges. The main idea behind using the 555 ‎timer IC is not to generate precise pulses but to make the piezo element’s output more ‎deterministic and predictable.‎

Copy of breadboard

This image depicts the project being assembled in an online circuit simulator. It shows how the ‎‎555 timer produces predictable output waves whenever it is triggered.‎

Piezoelectric components translate physical vibrations into electrical voltages and vice versa. ‎For example, piezo-beepers can vibrate to produce signals that can produce an audible single-‎frequency tone. Conversely, these components can also translate vibrations to an electrical ‎voltage. However, the produced signal is often not clean enough to reliably trigger an alarm or ‎other parts of a circuit. Further, the produced currents are usually not significant enough to result ‎in predictable and reliable input detections.‎

The NPN transistor in this project’s circuit acts as a switch that pulls the 555 timer’s trigger pin ‎low whenever the piezo element outputs a voltage. The transistor effectively inverts and ‎amplifies the signal, resulting in more predictability. The 555 timer generates an even more ‎predictable output pulse that ultimately triggers the alarm.‎

These measures help ensure that real alarms are not missed because the generated signal is not ‎strong enough. Conversely, electrical noise from the piezo element does not lead to frequent ‎false alarms.‎

Copy-of-schematic

This schematic diagram depicts the project’s circuit. Scheme-it link

In this project’s schematic diagram, C2 and R3 configure the timer IC’s output pulse width. R1 ‎and R4 are external pull-down resistors that ensure that input pins are not left floating. Similarly, ‎R2 guarantees that the 555 timer’s reset pin is constantly pulled high to keep the IC from ‎resetting. Finally, R5 is a simple current-limiting resistor for the red LED, which flashes briefly ‎with each output pulse of the timer IC.‎

You can omit the LED and its accompanying resistor, but I found them helpful for debugging. ‎Similarly, assembling the project on a breadboard and experimenting with different resistor and ‎capacitor values was very valuable. I recommend taking this extra step to test whether the piezo ‎element behaves as expected and how strong the vibrations need to be to trigger an alarm.‎

Copy-of-breadboard-photograph

This image shows the project assembled on a breadboard and supplied by a standard 3V coin ‎cell battery. The LED simulates the Arduino, and the push button triggers the timer without using ‎the piezo element.‎

Connecting the Sensor to the Cloud

‎The Arduino SBC employed in this project receives the 555 timer’s final output and triggers the ‎alarm if necessary. Connecting the development board to the Arduino IoT Cloud platform is a ‎breeze, and the process only requires a few straightforward configuration steps. Using the ‎Arduino IoT Cloud offers an online dashboard that allows the alarm status to be tracked from ‎anywhere in the world, and it also lets the Arduino interface with smart home systems to take ‎further action when it detects an alarm. Newcomers to the Arduino IoT Cloud should take some ‎time to check out this introductory article that explains the steps for getting the Arduino online in ‎great detail.‎

Once you have the Arduino connected to the cloud platform, add a new thing to the project. ‎Then, add two boolean variables to the newly created thing. Set the update policy of both ‎variables to “On Change.” Then name the first one “resetRequested” and ensure it’s writable. ‎Users will later set this variable via the online dashboard to let the Arduino know it should reset a ‎previously triggered alarm. The second boolean variable, “vibrationTrigger,” can be read-only. ‎The Arduino will use it to inform the dashboard that the alarm has been triggered. The cloud ‎platform can then display a warning on the web dashboard or perform further steps, such as ‎turning on the lights in a room.‎

Copy-of-iot-cloud-variables

Create a new thing and add variables, as shown in this screenshot. Remember to enter your ‎local network’s credentials.‎

Next, create a simple dashboard for the glass break sensor system containing a status label and ‎a push button. Link the status label widget to the previously created “vibrationTrigger” variable. ‎Then, add a push button widget to let users reset the alarm. Link the button widget to the ‎‎“resetRequested” boolean variable from before and arrange the items to your liking:‎

Copy-of-iot-cloud-dashboard

This screenshot shows a simple Arduino IoT Cloud dashboard for tracking the glass break ‎alarm state and resetting a previously triggered alarm.‎

Making the Arduino Push and Receive Cloud Updates

Once everything’s set up in the Arduino IoT Cloud, it’s time to make the Arduino react to the 555 ‎timer’s output and communicate status updates to the cloud dashboard. To get started, navigate ‎to the thing’s auto-generated sketch in the IoT Cloud web IDE and add the following variables to ‎the top of the main code file:‎

Copy Code
#define TRIGGER_PIN 3

unsigned long lastUpdate = 0UL;

volatile boolean resetTriggered = false;
volatile boolean triggerReceived = false;

The define preprocessor statement contains the GPIO pin number connected to the 555 timer ‎IC’s output pin. The lastUpdate variable is used within the loop method to wait a few milliseconds ‎between status updates, and the volatile boolean variables are used within the interrupt and cloud ‎callback functions.‎

The trigger input pin of the Arduino needs to be configured as an interrupt pin in the setup ‎function using the following two lines of code:‎

Copy Code
pinMode(TRIGGER_PIN, INPUT_PULLDOWN);
attachInterrupt(digitalPinToInterrupt(TRIGGER_PIN), onTriggerReceive, RISING);

These lines ensure that the pin is an input connected to an internal pull-down resistor, keeping the ‎pin low when not triggered by the 555 timer. The attachInterrupt call results in the Arduino calling ‎the onTriggerReceive function whenever the 555 timer pulls the trigger pin high. The ‎onTriggerReceive ISR (interrupt service routine) is basic, and it only sets the previously ‎mentioned volatile triggerReceived flag:‎

Copy Code
void onTriggerReceive() {
  triggerReceived = true;
}

Interrupt handlers should be as short and fast-returning as possible to ensure that subsequent ‎events are not blocked. For this reason, the ISR only sets a single flag that is then further ‎processed within the loop method. Similarly, the onResetRequestedChange function, generated ‎by the Arduino IoT Cloud, also just sets the other volatile boolean flag:‎

Copy Code
void onResetRequestedChange()  {
  resetTriggered = true;
}

The code’s loop function then checks whether these flags are set, and it performs certain actions ‎based on their state:‎

Copy Code
void loop() {
  // Update Arduino Cloud data
  ArduinoCloud.update();
  
  unsigned long currentMillis = millis();
  
  if (lastUpdate - currentMillis >= 500) {  
    if (resetTriggered) {
      vibrationTrigger = false;
      triggerReceived = false;
      resetTriggered = false;
      Serial.println("Alarm reset!");
    } else {
      vibrationTrigger = triggerReceived;
    }
    lastUpdate = currentMillis;
  }
}

The program pushes an update to the ArduinoCloud in each loop iteration before obtaining the ‎current millis value. The code uses this value to check whether enough time has elapsed since it ‎last inspected the two boolean flags. It waits approximately half a second between checks to ‎help free up some CPU time for other tasks running in the background. If enough time has ‎elapsed, the code inspects whether users requested a reset via the web interface, and it resets ‎the alarm state if the “resetTriggered” flag is set. If no reset was requested, the program ‎communicates the alarm state to the web interface.‎

Testing the Sensor

‎You can use the Arduino IoT Cloud’s online IDE to upload the program code to the Arduino once ‎you’re done implementing the firmware for this project:‎

Copy-of-iot-cloud-sketch

Use the highlighted buttons in the Arduino IoT Cloud web IDE to compile and upload the Arduino ‎sketch.‎

Once the upload finishes, you can navigate to the newly created dashboard to test the sensor ‎and reset functions. Tap the sensor to simulate strong vibrations, and the label on the dashboard ‎should then flip and show that the alarm got triggered. Clicking the reset button to its left should ‎change the label back to “false.”‎

Copy-of-dashboard-triggered

The web UI informs you about the alarm state and allows you to reset a previously triggered ‎alarm from anywhere in the world.‎

Summary

‎This article explains how to build a simple glass break sensor and connect it to the Arduino IoT ‎Cloud. The sensor is based on commonly available and cost-effective components. A ‎piezoelectric element translates physical vibrations into an electrical voltage that switches a ‎transistor. The transistor acts as an inverter and as an amplifier that pulls the trigger pin of a ‎standard 555 timer to a low state. The timer IC is configured to operate in monostable mode, ‎which outputs a single predictable high pulse whenever triggered. The output waveform feeds an ‎interrupt pin on the Arduino board, ultimately triggering the alarm.‎

The Arduino is connected to the Arduino IoT Cloud platform and communicates with the online ‎service via two boolean flags. One flag allows resetting the alarm, and the other transmits the ‎alarm state to the web dashboard. With this dashboard, users can inspect the alarm state from ‎anywhere in the world. Additionally, the IoT Cloud service allows the Arduino to interface with ‎other smart-home devices to trigger subsequent actions, for example, turning on the lights in a ‎room or sending out a message in reaction to the alarm.

מק"ט יצרן # AB2025B-LW100-R
BUZZER ELEMENT STD 2.5KHZ 20MM
PUI Audio, Inc.
מק"ט יצרן # CF14JT10K0
RES 10K OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
מק"ט יצרן # CF14JT470R
RES 470 OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
מק"ט יצרן # 2N4401BU
TRANS NPN 40V 0.6A TO-92-3
onsemi
מק"ט יצרן # 860010572004
CAP ALUM 33UF 20% 35V RADIAL TH
Würth Elektronik
מק"ט יצרן # K103K10X7RF5UL2
CAP CER 10000PF 50V X7R RADIAL
Vishay Beyschlag/Draloric/BC Components
מק"ט יצרן # C5SMF-RJF-CT0W0BB2
LED RED CLEAR 5MM OVAL T/H
Cree LED
מק"ט יצרן # NE555P
IC OSC SINGLE TIMER 100KHZ 8-DIP
Texas Instruments
מק"ט יצרן # ABX00032
ARDUINO NANO 33 IOT WITH HEADERS
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.