Maker.io main logo

Bluetooth LE Sensor Nodes to Raspberry Pi WiFi Bridge

154

2024-04-02 | By Adafruit Industries

License: See Original Project Raspberry Pi SBC

Courtesy of Adafruit

Guide by John Park

Overview

 

Use sensor packed Bluefruit boards and a Raspberry Pi to build a ‎network of sensors that send data to Adafruit IO!‎

This project takes advantage of CircuitPython running on ‎the Feather Bluefruit Sense and CLUE boards (any nRF52840 ‎Adafruit board will work) and Python running on the Raspberry Pi.‎

The Pi receives advertised BLE sensor data from the Feather and ‎CLUE and then sends that data over WiFi or Ethernet to your ‎Adafruit IO feed.‎

It’s a super easy way to make a wireless sensor node, using the built ‎in wireless/networking capabilities of the Raspberry Pi!‎

raspberry_pi_bridge1

Parts

You can use any of the Adafruit nRF52840 boards and sensors you ‎like. We'll show how it works with the Feather Sense and CLUE ‎boards, since they pack so many sensors right on board.‎

Optional Parts

If you want to use, say, a Feather nRF52840 plus some plug-in ‎STEMMA QT breakouts, here are some great options:‎

Prepare the CLUE

clue_1

We'll set up the CLUE board to act as a sensor for the BroadcastNet.‎

First, set up CircuitPython on the CLUE following the instructions on ‎this page.‎

Libraries

Next, install the libraries needed. This guide page will show you ‎where to download them.‎

You'll need the following libraries for this project:‎

  • adafruit_apds9960
  • adafruit_ble
  • adafruit_ble_broadcastnet
  • adafruit_bmp280.mpy
  • adafruit_bus_device
  • adafruit_clue.mpy
  • adafruit_register
  • adafruit_lis3mdl.mpy
  • adafruit_lsm6ds
  • adafruit_sht31d.mpy
  • neopixel.mpy

libraries_2

Text Editor

Adafruit recommends using the Mu editor for using your ‎CircuitPython code with the CLUE board. You can get more info ‎in this guide.‎

Alternatively, you can use any text editor that saves files.‎‎ ‎

Code.py

Copy the code shown below, paste it into Mu. Save the code from Mu ‎to the CLUE's CIRCUITPY drive as code.py

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

"""This uses the CLUE as a Bluetooth LE sensor node."""

import time
from adafruit_clue import clue
import adafruit_ble_broadcastnet

print("This is BroadcastNet CLUE sensor:", adafruit_ble_broadcastnet.device_address)

while True:
measurement = adafruit_ble_broadcastnet.AdafruitSensorMeasurement()

measurement.temperature = clue.temperature
measurement.pressure = clue.pressure
measurement.relative_humidity = clue.humidity
measurement.acceleration = clue.acceleration
measurement.magnetic = clue.magnetic

print(measurement)
adafruit_ble_broadcastnet.broadcast(measurement)
time.sleep(60)

View on GitHub

How It Works

When this code runs on the CLUE board, it'll first import the time, clue, ‎and adafruit_ble_broadcastnet libraries.‎

Then, it will print the unique ID for the board based on the board's ‎BLE adapter's MAC address. This address will be used when ‎messages are sent so there won't be any clashes when multiple ‎microcontroller boards are in range of the BroadcastNet base station.‎

NOTE: This is not a secure connection, so think of this system as ‎‎"broadcasting" in the truest sense of the word!‎

Download File

Copy Code
import time
from adafruit_clue import clue
import adafruit_ble_broadcastnet

print("This is BroadcastNet CLUE sensor:", adafruit_ble_broadcastnet.device_address)

Measurements

Next, we will have the main loop of the program. In it, the board ‎sends out an advertisement to alert the base station central device ‎that it is there.‎

Next, we collect the different sensor readings such ‎as measurement.temperature = clue.temperature

We then print the combined measurement to the screen and ‎broadcast it.‎

Finally, the code will sleep for a certain amount of time. Depending ‎on your needs this can be as frequent as every two seconds if ‎sending a single data point to Adafruit IO* (or every one second to ‎AIO+) to many minutes or hours between sensor measurement ‎broadcasts. In this case, it is pausing for 60 seconds between ‎broadcasts.‎‎

‎‎*The data limit on Adafruit IO is 30 data points per minute and ‎‎60/min on Adafruit IO+)‎

Even if you only measure one data point, there will always also be an ‎additional data point sent for the 'missed-message-count' value ‎used as a type of error check. This counts toward the rate limit on ‎AIO.‎

Download File

Copy Code
while True:
measurement = adafruit_ble_broadcastnet.AdafruitSensorMeasurement()

measurement.temperature = clue.temperature
measurement.pressure = clue.pressure
measurement.relative_humidity = clue.humidity
measurement.acceleration = clue.acceleration
measurement.magnetic = clue.magnetic

print(measurement)
adafruit_ble_broadcastnet.broadcast(measurement)
time.sleep(60)

Once we set up the Raspberry Pi to act as a Broadcastnet base ‎station, the CLUE sensor data will be able to make its way all the ‎way to Adafruit IO!‎

Prepare the Feather Sense

sense_3

We'll set up the Feather Sense board to act as a sensor for the ‎BroadcastNet.‎

First, set up CircuitPython on the Feather Sense following ‎the instructions on this page. NOTE: This board is so new, the ‎instructions are actually for the regular nRF52840 Feather, so when ‎you go to the CircuitPython.org download page, be sure to use ‎the download for the Sense board instead!‎

Libraries

Next, install the libraries needed. This guide page will show you ‎where to download them.‎

You'll need the following libraries for this project:‎

  • adafruit_apds9960
  • adafruit_ble
  • adafruit_ble_broadcastnet
  • adafruit_bmp280
  • adafruit_bus_device
  • adafruit_register
  • adafruit_lis3mdl
  • adafruit_lsm6ds
  • adafruit_sht31d
  • neopixel.mpy

libraries_4

Text Editor

Adafruit recommends using the Mu editor for using your ‎CircuitPython code with the Feather Sense board. You can get more ‎info in this guide.‎

Alternatively, you can use any text editor that saves files.‎‎

‎Code.py

Copy the code shown below, paste it into Mu. Save the code from Mu ‎to the Feather's CIRCUITPY drive as code.py.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

"""This uses the Feather Sense as a Bluetooth LE sensor node."""

import time
import adafruit_ble_broadcastnet
import board
import adafruit_lsm6ds # accelerometer
import adafruit_sht31d # humidity sensor
import adafruit_bmp280 # barometric sensor
import adafruit_lis3mdl # magnetic sensor

i2c = board.I2C() # uses board.SCL and board.SDA
# i2c = board.STEMMA_I2C() # For using the built-in STEMMA QT connector on a microcontroller

sense_accel = adafruit_lsm6ds.LSM6DS33(i2c)
sense_humid = adafruit_sht31d.SHT31D(i2c)
sense_barometric = adafruit_bmp280.Adafruit_BMP280_I2C(i2c)
sense_magnet = adafruit_lis3mdl.LIS3MDL(i2c)

print("This is BroadcastNet Feather Sense sensor:", adafruit_ble_broadcastnet.device_address)

while True:
measurement = adafruit_ble_broadcastnet.AdafruitSensorMeasurement()

measurement.temperature = sense_barometric.temperature
measurement.pressure = sense_barometric.pressure
measurement.relative_humidity = sense_humid.relative_humidity
measurement.acceleration = sense_accel.acceleration
measurement.magnetic = sense_magnet.magnetic

# print(measurement)
adafruit_ble_broadcastnet.broadcast(measurement)
time.sleep(60)

View on GitHub

How It Works

When this code runs on the Feather Sense board, it'll first import ‎the time, board, and adafruit_ble_broadcastnet libraries, along with the library ‎for each sensor in the board that we're using.‎

Next, I2C is instantiated on the board for communications with the ‎sensors.‎

We create an object (with a nice name!) for each sensor as well and ‎instruct them to use I2C.‎

Then, it will print the unique ID for the board based on the board's ‎BLE adapter MAC address. This address will be used when messages ‎are sent, so there won't be any clashes when multiple ‎microcontroller boards are in range of the BroadcastNet base station.‎

NOTE: this is not a secure connection, so think of this system as ‎‎"broadcasting" in the truest sense of the word!

‎‎Download File

Copy Code
import time
import adafruit_ble_broadcastnet
import board
import adafruit_lsm6ds # accelerometer
import adafruit_sht31d # humidity sensor
import adafruit_bmp280 # barometric sensor
import adafruit_lis3mdl # magnetic sensor

i2c = board.I2C()

sense_accel = adafruit_lsm6ds.LSM6DS33(i2c)
sense_humid = adafruit_sht31d.SHT31D(i2c)
sense_barometric = adafruit_bmp280.Adafruit_BMP280_I2C(i2c)
sense_magnet = adafruit_lis3mdl.LIS3MDL(i2c)

print("This is BroadcastNet Feather Sense sensor:", adafruit_ble_broadcastnet.device_address)

Measurements

Next, we will have the main loop of the program. In it, the board ‎sends out an advertisement to alert the base station central device ‎that it is there.‎

Next, we collect the different sensor readings such ‎as measurement.temperature = sense_barometric.temperature (we're using the ‎temperature sensor that is built onto the barometric pressure sensor ‎package.)‎

We then broadcast the combined measurement over BLE.‎

Finally, the code will sleep for a certain amount of time. Depending ‎on your needs, this can be as frequent as every two seconds, if ‎sending a single data point to Adafruit IO* (or every one second to ‎AIO+) to many minutes or hours between sensor measurement ‎broadcasts. In this case, it is pausing for 60 seconds between ‎broadcasts.‎‎ ‎‎

*The data limit on Adafruit IO is 30 data points per minute and ‎‎60/min on Adafruit IO+)‎

Download File

Copy Code
measurement = adafruit_ble_broadcastnet.AdafruitSensorMeasurement()

measurement.temperature = sense_barometric.temperature
measurement.pressure = sense_barometric.pressure
measurement.relative_humidity = sense_humid.relative_humidity
measurement.acceleration = sense_accel.acceleration
measurement.magnetic = sense_magnet.magnetic

# print(measurement)
adafruit_ble_broadcastnet.broadcast(measurement)
time.sleep(60)

Once we set up the Raspberry Pi to act as a BroadcastNet base ‎station, the CLUE sensor data will be able to make its way all the ‎way to Adafruit IO!‎

Other Boards

If you choose to use a different Adafruit nRF52840 board and ‎external sensors, the setup will be very nearly the same. Check the ‎guide for the board and sensors for the particulars.‎

Raspberry Pi Quick Setup

quickset_5

This quick-start guide will get you ready to connect and run all sorts ‎of Adafruit projects on your Raspberry Pi computer.‎

You will need:‎

SD Card Prep

First, we need to perform the basic set up the Raspberry Pi. These ‎are the first steps:‎

  • download the latest Raspbian desktop operating system
  • burn the OS to an SD card
  • enable SSH
  • add WiFi settings and credentials

For details on doing these things, follow the first four pages of this ‎guide to get your Pi setup with Raspbian Lite (for 'headless' or ‎remote operation) or NooBs (for graphical / desktop use), WiFi, and ‎ssh enabled.‎

Once the SD card is prepared, come back here so we can continue.‎

Power to the Pi

Safely eject the SD card from your main computer. Then, with the Pi ‎unplugged from power, insert the SD card into the Pi's SD card slot.‎

Then, plug in the power to the Pi. You should see some LEDs light up.‎

From here forward, we'll be connecting to the Pi remotely from our ‎main computer. Make sure your computer is on the same WiFi ‎network as the Pi.‎

Ping

After a minute or two, you can try and ping the Pi to see if it has ‎connected to your network. Open a terminal on your computer, such ‎as Terminal.app on a mac (Windows users will require some ‎additional setup. Read here), and type this and press return:‎

ping -c 3 raspberrypi.local

You should see an output similar to this:‎

Download File

Copy Code
jep@machine ~ % ping -c 3 raspberrypi.local
PING raspberrypi.local (192.168.1.68): 56 data bytes
64 bytes from 192.168.1.68: icmp_seq=0 ttl=64 time=14.993 ms
64 bytes from 192.168.1.68: icmp_seq=1 ttl=64 time=20.565 ms
64 bytes from 192.168.1.68: icmp_seq=2 ttl=64 time=50.571 ms

--- raspberrypi.local ping statistics ---
3 packets transmitted, 3 packets received, 0.0% packet loss
round-trip min/avg/max/stddev = 14.993/28.710/50.571/15.625 ms

This tells us that the Pi is on the network and has an address of ‎‎192.168.1.68.‎

SSH

We can now connect to it through the secure shell (SSH) so we can ‎control it remotely.‎

Here's some great info on SSH from the Raspberry Pi Foundation.‎

Type the following in your terminal:‎

ssh pi@raspberrypi.local

or

ssh pi@192.168.1.68 (or whatever address you saw returned earlier when ‎you pinged it.)‎

You may see a message warning you that the authenticity of the ‎host can't be established, are you sure you want to continue ‎connecting (yes/no)?‎

To this question you can reply by typing yes and pressing return. This ‎will add the Pi to your list of known hosts and should not pop up ‎again with this question.‎

You will now see the password prompt for the Pi:‎

pi@raspberrypi.local's password:‎

Go ahead and type in the default password, which is: raspberry

Change the Password!‎

You will now be logged into the Pi over ssh! There will be a warning ‎about changing your password from the default and instructions on ‎how to do so. Do it now! Type passwd, hit return and follow the ‎instructions to create a new, secure, non-default password!‎

Rename the Pi

You may end up with multiple Pi computers on your network, which ‎can get confusing if they are all named raspberrypi. To rename this ‎one for this project, type in sudo raspi-config and press return.‎

sudo? What's sudo? It stands for "superuser do", and it's a program ‎that lets you run powerful commands which are normally restricted ‎for reasons of safety and security. Or just to prevent accidents!‎

Use the arrows and enter key on your keyboard to navigate. Pick ‎‎2 Network Options and press return on your keyboard.‎

Then, pick N1 Hostname.‎

Enter a new hostname -- I typed raspberrypiBlinkaBridge

Use the Tab key to get to the <Ok> button and press return.‎

Press tab twice to get to the <Finish> button and press return.‎

Now, we'll restart the Pi to make the changed host name show up ‎on the network by typing sudo reboot and pressing return.‎

Note, this will close the SSH session. After the Pi restarts, wait about ‎a minute, and then reconnect over SSH. This time, you'll use the new ‎name: ssh pi@raspberrypiBlinkaBridge

rename_6

rename_7

rename_8

rename_9

Update Application List

Once logged into the Pi, we'll do some software updates to make ‎sure we have the latest of everything.‎

We really really recommend the lastest Raspbian only. If you have an ‎older Raspbian install, run "sudo apt-get update" and "sudo apt-get ‎upgrade" to get the latest OS!‎

Type:‎

sudo apt-get update

And then press return. This will run for a little bit as it reads the ‎available package lists, and then finish, reporting that it is done.‎

You can now apply any of these changes by typing:‎

sudo apt-get upgrade

sudo_10

Type Y and press enter to continue.‎

Software Setup

Now that the Pi is updated and renamed on the network, we'll make ‎sure we have Python 3 setup, as Python 2 is no longer used or ‎supported.‎

pip3, is the software package installer we'll use. Let's upgrade it to ‎the latest version with this command:‎

sudo pip3 install --upgrade setuptools

If above doesn't work, try

sudo apt-get install python3-pip

Once that has finished, you'll be returned to the prompt.‎

Make sure you're using Python 3!‎

The default Python on your computer may not be Python 3. Python 2 ‎is officially discontinued, ‎and all our libraries are Python 3 only.‎

We'll be using python3 and pip3 in our commands, use those versions of ‎Python and pip to make sure you're using 3 and not 2.‎

Install Blinka

Blinka is the software that allows us to run CircuitPython and its ‎libraries on Linux. You can read more about it here.‎

To install blinka, type:‎

sudo pip3 install adafruit-blinka

That's it! You can reboot again if you like.‎

Install Pi Bridge Software

BLE Support

Next, we'll set up BLE support with the BlueZ Bluetooth protocol ‎stack. Type this and hit return:‎

sudo apt-get install bluez-hcidump

sudo_11

Adafruit Blinka BLEio

‎"Old MacDonald had a snake, BLEeeee-iiiiii-BLEeeee-iiiiii-oooooo!"‎

Next, we'll install the Adafruit Blinka bleio library, which is required ‎for CircuitPython BLE to work properly.‎

In the ssh terminal type:‎

Download File‎

Copy Code
pip3 install adafruit-blinka-bleio

Bluetooth Group

In order to have the Pi scan for BLE devices we need to increase the ‎permissions granted to the pi user.‎

To add the user to the bluetooth group do:‎

sudo usermod -a -G bluetooth pi

‎(Or whatever your username is if not the default.)‎

Now, the pi user won't actually have these new permissions until the ‎next time we log in, so type exit and then re-login to the ssh with

ssh pi@raspberrypiblinkabridge.local

Enter your password when promted, then you can check the groups ‎the pi user is in by typing:‎

groups

Download File

Copy Code
pi@raspberrypiBlinkaBridge:~ $ groups
pi adm dialout cdrom sudo audio video plugdev games users input netdev bluetooth gpio i2c spi

Now, we'll set permissions so that we can do comprehensive BLE ‎scanning.‎

Type the following lines into the ssh terminal, pressing enter after ‎each one:‎

Download File

Copy Code
sudo chown :bluetooth /usr/bin/hcidump /usr/bin/hcitool
sudo chmod o-x /usr/bin/hcidump /usr/bin/hcitool
sudo setcap 'cap_net_raw,cap_net_admin+eip' /usr/bin/hcitool
sudo setcap 'cap_net_raw,cap_net_admin+eip' /usr/bin/hcidump

Install Python libraries

Now you're ready to install the Python support library for the BLE ‎BroadcastNet bridge. Run the following command to install it:‎

pip3 install adafruit-circuitpython-ble-broadcastnet

Add Examples

Let's add some example code to try by cloning a Git repository ‎locally.‎

Type cd to go to your home directory on the Pi.‎

Note, you can type pwd (print working directory) to see where you are ‎at any time:‎

Download File

Copy Code
pi@raspberrypiBlinkaBridge:~ $ pwd
/home/pi

Here we will clone the example directory. Type:‎

git clone https://github.com/adafruit/Adafruit_CircuitPython_BLE_BroadcastNet.git

Once it finishes copying the files, you can have a look. Go to the ‎directory by typing cd Adafruit_CircuitPython_BLE_BroadcastNet (Hint, you can ‎press Tab to complete that long directory name after you type a ‎couple of the letters.)‎

Check out the contents by typing ls -1‎

Download File

Copy Code
pi@raspberrypiBlinkaBridge:~/Adafruit_CircuitPython_BLE_BroadcastNet $ ls -1
adafruit_ble_broadcastnet.py
CODE_OF_CONDUCT.md
docs
examples
LICENSE
README.rst
requirements.txt
setup.py

The adafruit_ble_broadcastnet.py file is the Python library we'll be ‎using when we run the code. The code we want to run on the Pi is ‎inside the /examples directory. Let's go there by typing:‎

cd ./examples/‎

ble_broadcastnet_blinka_bridge.py is the one we'll run on the Pi ‎‎(after setting up the secrets.py file below), while the others are ‎examples, we can run on different microcontrollers such as the CLUE, ‎Circuit Playground Bluefruit, Feather nRF52840, Feather Sense, and ‎ItsyBitsy nRF52840.‎

  • ble_broadcastnet_battery_level_neopixel.py
  • ble_broadcastnet_battery_level.py
  • ble_broadcastnet_cpb.py
  • ble_broadcastnet_expo_backoff.py
  • ble_broadcastnet_multisensor.py
  • ble_broadcastnet_simpletest.py

Adafruit IO

In order to use the Adafruit IO Internet of Things service (which is ‎absolutely free to use) you'll need to log in with your Adafruit ‎account. If you don't already have an Adafruit login, create one here.‎

If you haven't used Adafruit IO before, check out this guide for more ‎info.‎

Once you have logged into your account, there are two pieces of ‎information you'll need to place in your secrets.py file: Adafruit IO ‎username, and Adafruit IO key. Head to io.adafruit.com and simply click ‎the View AIO Key link on the left-hand side of the Adafruit IO page ‎to get this information.‎

Shhh Secrets

The ble_broadcastnet_blinka_bridge.py program will need to ‎authenticate your Adafruit IO credentials in order to run. So, we'll ‎create a file called secrets.py to contain this info.

‎Inside is a Python dictionary named secrets with a line for each entry. ‎Each entry has an entry name (say 'aio_username') and then a colon to ‎separate it from the entry key 'daphne_von_person'‎

Download File

Copy Code
secrets = {
'aio_username' : '_your_aio_username_',
'aio_key' : '_your_big_huge_super_long_aio_key_'
}

Don't share your secrets.py - keep that out of GitHub, Discord or ‎other project-sharing sites.‎

Use a text editor to create and save this file into ‎the /Adafruit_CircuitPython_BLE_Broadcast/examples directory. ‎Since you are ssh'd into the Pi, the easiest way to do this is with ‎the nano text editor. Type:‎

nano secrets.py

In the nano editor that launches, copy and paste the secrets text ‎from above, replacing the username and key with your own, then ‎save & exit.‎

Your /examples directory should now look like this:‎

  • ble_broadcastnet_battery_level_neopixel.py
  • ble_broadcastnet_battery_level.py
  • ble_broadcastnet_blinka_bridge.py
  • ble_broadcastnet_cpb.py
  • ble_broadcastnet_expo_backoff.py
  • ble_broadcastnet_multisensor.py
  • ble_broadcastnet_simpletest.py
  • secrets.py

Service Identity

Next, we'll install the service_identity module, which is used behind the ‎scenes for certificate verification. Type this into the ssh terminal and ‎press return:‎

Download File

Copy Code
pip3 install service_identity

Launch BroadcastNet Bridge

We're now ready to run the broadcast bridge software on the Pi! ‎When this runs it will look for BLE sensors, collect their message ‎data, and then send it to your Adafruit IO account as a uniquely ‎named feed.‎

To run it, type this in the ssh shell and press return:‎

Download File

Copy Code
python3 ble_broadcastnet_blinka_bridge.py

If your Feather Sense and/or CLUE boards you set up earlier are ‎powered on and within range, you will start to see the measurement ‎values being received successfully:‎

Download File

Copy Code
bridge-dca63202680a-sensor-fdc492775544 [{'key': 'missed-message-count', 'value': 0}, {'key': 'acceleration-0-x', 'value': -5.6099700927734375}, {'key': 'acceleration-0-y', 'value': 2.15712833404541}, {'key': 'acceleration-0-z', 'value': 7.956132888793945}, {'key': 'pressure-0', 'value': 992.184814453125}]
Done logging measurement to IO. Took 0.628571397000087 seconds

bridge-dca63202680a-sensor-fdc492775544 [{'key': 'missed-message-count', 'value': 2}, {'key': 'acceleration-0-x', 'value': -5.6506500244140625}, {'key': 'acceleration-0-y', 'value': 2.1284141540527344}, {'key': 'acceleration-0-z', 'value': 7.968097686767578}, {'key': 'pressure-0', 'value': 992.178955078125}]
Done logging measurement to IO. Took 1.1094765150000967 seconds

bridge-dca63202680a-sensor-fdc492775544 [{'key': 'missed-message-count', 'value': 1}, {'key': 'magnetic-0-x', 'value': -0.9061675071716309}, {'key': 'magnetic-0-y', 'value': -21.879562377929688}, {'key': 'magnetic-0-z', 'value': -100.5845947265625}, {'key': 'temperature-0', 'value': 24.0244140625}]
Done logging measurement to IO. Took 0.6365861880001376 seconds

bridge-dca63202680a-sensor-fdc492775544 [{'key': 'missed-message-count', 'value': 0}, {'key': 'acceleration-0-x', 'value': -5.626718521118164}, {'key': 'acceleration-0-y', 'value': 2.1152544021606445}, {'key': 'acceleration-0-z', 'value': 7.981258392333984}, {'key': 'pressure-0', 'value': 992.23876953125}]
Done logging measurement to IO. Took 0.6315450570000394 seconds

If you open your Adafruit IO Feeds page, you'll see this feed there.‎

feed_12

Let's have a look at how to work with your feed data.‎

BroadcastNet on AIO

 

Adafruit IO Getting Started

If you're new to Adafruit IO, this guide page has lots of great info and ‎links to check out.‎

raspberry_pi_bridge1

Renaming AIO Feeds

When you head to your Adafruit IO Feeds page, you'll see the ‎Raspberry Pi bridge name and sensor name pairings of any sensor ‎boards you're running. Here, I have two:‎

feed_13

Since these names are derived from the MAC addresses of the ‎devices themselves, they are good unique IDs, but not very friendly ‎looking! Let's change them.‎

First, look at the CLUE screen and make note of the sensor ID. In my ‎case it reports caa19e07860b.‎

Then, click on the feed group of the same name. You'll see a settings ‎gear icon in the Group Info box. Click that.‎

In the Edit Group popup, give the Name field a more descriptive ‎name. Be sure to leave the Key value as it is or things will break!‎

Repeat this process for any other boards you're using.‎

process_15

process_16

process_17

Dashboard Setup

Set up a new dashboard -- I named mine BroadcastNet Dashboard.‎

Hit Create to make the new dashboard, which we can then fill with ‎feed data blocks.‎

dashboard_18

Blocks

Now we'll add feed data blocks to the Dashboard.‎

Press the + icon to add new blocks.‎

Here I've added a graph widget with the two temperatures from the ‎two different boards.‎

blocks_19

blocks_20

blocks_21

blocks_22

You can continue to add elements to the dashboard depending on ‎what you'd like to see!‎

elements_23

Measurement List

The BroadcastNet library has many different measurements it can ‎read with the measurement command. You can check out ‎the documentation here.‎

For convenience, this is the full list:

‎TVOC

Total Volatile Organic Compounds as a float in parts per billion.

‎acceleration

Acceleration as (x, y, z) tuple of floats in meters per second per ‎second.‎

battery_voltage

Battery voltage in millivolts. Saves two bytes over voltage and is ‎more readable in bare packets.‎

color

Color as RGB integer.

‎current

Current as a float in milliamps.‎

distance

Distance as a float in centimeters.‎

duty_cycle

‎16-bit PWM duty cycle. Independent of frequency.‎

eCO2‎

Equivalent CO2 as a float in parts per million.‎

frequency

As integer Hertz

gyro

Gyro motion as (x, y, z) tuple of floats in radians per second.

‎light

Brightness as a float without units.

‎lux

Brightness as a float in SI lux.

‎magnetic

Magnetism as (x, y, z) tuple of floats in micro-Tesla.

‎orientation

Absolution orientation as (x, y, z) tuple of floats in degrees.‎

pressure

Pressure as a float in hectopascals.

‎relative_humidity

Relative humidity as a float percentage.‎

temperature

Temperature as a float in degrees centigrade.‎

value‎

16-bit unit-less value. Used for analog values and for booleans.‎

voltage

Voltage as a float in Volts.‎

weight

Weight as a float in grams.‎

מק"ט יצרן # 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
מק"ט יצרן # 4399
STEMMA QWIIC JST SH CABLE 50MM
Adafruit Industries LLC
מק"ט יצרן # 4494
BAROMETRIC PRESSURE / ALTITITUDE
Adafruit Industries LLC
מק"ט יצרן # 4369
PCT2075 STEMMA QWIIC TEMP SENSOR
Adafruit Industries LLC
מק"ט יצרן # 3595
PROXIMITY LIGHT GESTURE SENS
Adafruit Industries LLC
מק"ט יצרן # 2651
SENSOR BARO/ALT BMP280 I2C/SPI
Adafruit Industries LLC
מק"ט יצרן # 2436
ADDRESS LED STRIP SERIAL WHT 4M
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.