Maker.io main logo

CircuitPython BLE Libraries on Any Computer

87

2024-03-25 | By Adafruit Industries

License: See Original Project Arduino Circuit Playground Adafruit Feather Raspberry Pi SBC

Courtesy of Adafruit

Guide by Dan Halbert

Overview

three_1

Adafruit CircuitPython supports using Bluetooth Low Energy (BLE) ‎to communicate wirelessly with BLE devices, phones, tablets, and ‎with other CircuitPython boards. Adafruit provides many libraries to ‎make this easy and to support specific devices.‎

Now you can use those same libraries (or write your own) on any ‎host computer--Windows, Mac, or Linux--that has BLE hardware. ‎Most modern computers, especially laptops, already have Bluetooth ‎hardware built in. If not, you can plug in a USB adapter such as ‎Adafruit's Bluetooth 4.0 USB Module.‎

The Adafruit Blinka bleio library makes this possible. It is a regular ‎Python library that runs on desktop Python, not on CircuitPython ‎boards. It re-implements the _bleio module that is part of ‎CircuitPython: all our BLE libraries are ultimately based on _bleio.‎

The Blinka bleio library only supports acting in a BLE central ‎role. You can connect to peripheral devices, such as heart rate ‎monitors, pulse oximeters, bicycle sensors, etc., but you cannot act as ‎a peripheral yourself with this code. ‎

The Blinka bleio library is part of the family of "Blinka" libraries that ‎run under regular Python and implement CircuitPython functionality, ‎including Blinka and Blinka displayio.‎

This guide will explain how to get Python set up on your host ‎computer, how to install the Blinka bleio library, and then give some ‎examples of how to use it.‎

Bluetooth Capable Devices from Adafruit

Some Adafruit Microcontrollers with ‎Bluetooth

Install Python on Your Host Computer

You Need Python 3 and pip3‎

To run CircuitPython BLE libraries on a host computer, you'll need at ‎least Python 3.9, and you'll need the pip3 program to install the ‎libraries. You may have pip already, but often the pip (not pip3) ‎command installs software for Python 2, so make sure you are ‎using pip3.‎

Windows 10‎

You can install Python from https://python.org, or from the Windows ‎Store. See our guide Using Python on WIndows 10 for an easy way to ‎get Python installed.‎

If you don't use the Windows Store version, make sure you check the ‎box to add Python to your PATH when you run the installer. See the ‎screenshot below.‎

install_2

Starting Python 3 on Windows

Depending on how you install Python 3, the command to start it in a ‎command shell in Windows can be different.‎

  • Installed from the https://python.org download:‎
    • Works: python (python.exe)
    • Works:py (py.exe, the Python launcher).
    • Does not work: python3 (python3.exe). You'll get directed to the ‎Windows Store to install Python 3 yet again.‎
  • Installed from the Windows Store:
    • Works: python (python.exe)
    • Does not work: py (the Python launcher is not installed).
    • Works: python3 (python3.exe)

These differences can be confusing; see this page for detailed ‎documentation.‎

macOS

Modern macOS comes with Python 3, but it may be an older version. ‎Instead of using the system-supplied version, we recommend that ‎you use the Homebrew system to install a more recent version of ‎Python 3 and keep it up to date. The Homebrew installation will not ‎interfere with the system-installed Python, and does not replace it.‎

This article describes in detail various ways of managing Python on ‎macOS. It's worth reading to understand the issues, and to see ‎various ways of managing multiple versions of Python.‎

Bluetooth Permissions

A user has reported that, at least as of macOS Big Sur, you must add ‎your terminal application to the Bluetooth Privacy Settings ‎in System Preferences > Security & Privacy > Privacy > Bluetooth.‎

Linux

Modern versions of Linux always come with Python. They may ‎include both Python 2 and Python 3. See if the version supplied with ‎your Linux distribution is at least 3.9. If not, your distribution may ‎allow you to install additional versions that do not interfere with the ‎original system-supplied version. If you can upgrade your ‎distribution, considering doing so. For instance, Ubuntu 22.04 comes ‎with Python 3.10.‎

Make sure you have pip3 installed as well, by trying to run it. If it's not ‎installed, install it in the appropriate way for your Linux distribution. ‎For instance, for Ubuntu and Debian, do:‎

Download File

Copy Code
sudo apt install python3-pip

Raspberry Pi OS

Raspberry Pi OS (the new name for Raspian), which is based on ‎Debian Linux, also comes with Python. The latest version as of this ‎writing (April 2023), bullseye, comes with Python 3.9, invoked with ‎the python3 command.‎

If you are using Raspberry Pi OS Lite, it may not come with pip3. You'll ‎need to install it by doing: ‎

Download File

Copy Code
sudo apt install python3-pip

Do not use sudo when running pip3.‎

Do Not Use sudo When ‎Running pip3

You may see Internet advice to install libraries using sudo pip3 on Linux ‎or MacOS. This is in general a bad idea because you can damage the ‎libraries that the underlying system depends on, and in general end ‎up trashing your system in mysterious ways. Always install ‎using pip3 without sudo. If your pip3 is old, you may need to specify pip3 --‎user, but these days --user is often the default.‎

Here's a detailed discussion of why sudo pip3 is a bad idea.‎

Install BLE Libraries

Once you have installed Python 3 and pip3, you are ready to install the ‎Blinka bleio library and the base CircuitPython BLE library. In your ‎shell, enter this command to install both:‎

Download File

Copy Code
pip3 install --upgrade adafruit-blinka-bleio adafruit-circuitpython-ble

The --upgrade will ensure that you get the latest versions, even if either ‎library was previously installed. The adafruit-blinka-bleio library depends ‎on a number of other libraries, which will be installed automatically, ‎and upgraded if necessary.‎‎ ‎

Linux and Raspberry Pi: Add User ‎to bluetooth Group

On Linux, including on Raspberry Pi, you must also add your user to ‎the bluetooth group. Reboot after doing this to ensure your user is ‎added to the group and also to ensure that ~/.local/bin is added to ‎your path (after doing pip3 above). To add yourself to the group, do ‎this:‎

Download File

Copy Code
sudo usermod -a -G bluetooth $USER
sudo reboot

Raspberry Pi 3B+ and 4B Firmware ‎Fix

Raspberry Pi 3B+ and 4B boards use different hardware for BLE and ‎WiFi than Raspberry Pi 3B and Pi Zero W boards. There was a bug in ‎the firmware for the 3B+ and 4B boards, in the bluez-‎firmware package. bluez-firmware-1.2-4+rpt2 worked, but ‎versions rpt3, rpt4, rpt5, and rpt6 did not. Make sure your version is at ‎least rpt8, as rpt8 includes a security fix does not present in rpt7.‎

Download File

Copy Code
$ apt list bluez-firmware
Listing... Done
bluez-firmware/testing,now 1.2-4+rpt8 all [installed,automatic]
N: There is 1 additional version. Please use the '-a' switch to see it

If you need to upgrade bluez-firmware, do:‎

Download File

Copy Code
$ sudo apt upgrade bluez-firmware

Pulse Oximeter, Heart Rate Monitor, and ‎BBQ Thermometer

Once the base BLE libraries are installed, you can install helper ‎libraries for various third-party BLE peripherals, and access them ‎directly. We'll show examples of peripherals accessed from several ‎different host computers.‎

Pulse Oximeter

This example uses the BerryMed Pulse Oximeter sold by Adafruit. Install ‎the pulse oximeter library by typing the pip3 command below into ‎your shell. Then download the example program below.‎

pulse_3

Download File

Copy Code
pip3 install adafruit-circuitpython-ble-berrymed-pulse-oximeter

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 ladyada for Adafruit Industries
# SPDX-License-Identifier: MIT

"""
Read data from a BerryMed pulse oximeter, model BM1000C, BM1000E, etc.
"""

# Protocol defined here:
# https://github.com/zh2x/BCI_Protocol
# Thanks as well to:
# https://github.com/ehborisov/BerryMed-Pulse-Oximeter-tool
# https://github.com/ScheindorfHyenetics/berrymedBluetoothOxymeter
#
# The sensor updates the readings at 100Hz.

import _bleio
import adafruit_ble
from adafruit_ble.advertising.standard import Advertisement
from adafruit_ble.services.standard.device_info import DeviceInfoService
from adafruit_ble_berrymed_pulse_oximeter import BerryMedPulseOximeterService

# CircuitPython <6 uses its own ConnectionError type. So, is it if available. Otherwise,
# the built in ConnectionError is used.
connection_error = ConnectionError
if hasattr(_bleio, "ConnectionError"):
connection_error = _bleio.ConnectionError

# PyLint can't find BLERadio for some reason so special case it here.
ble = adafruit_ble.BLERadio() # pylint: disable=no-member

pulse_ox_connection = None

while True:
print("Scanning...")
for adv in ble.start_scan(Advertisement, timeout=5):
name = adv.complete_name
if not name:
continue
# "BerryMed" devices may have trailing nulls on their name.
if name.strip("\x00") == "BerryMed":
pulse_ox_connection = ble.connect(adv)
print("Connected")
break

# Stop scanning whether or not we are connected.
ble.stop_scan()
print("Stopped scan")

try:
if pulse_ox_connection and pulse_ox_connection.connected:
print("Fetch connection")
if DeviceInfoService in pulse_ox_connection:
dis = pulse_ox_connection[DeviceInfoService]
try:
manufacturer = dis.manufacturer
except AttributeError:
manufacturer = "(Manufacturer Not specified)"
try:
model_number = dis.model_number
except AttributeError:
model_number = "(Model number not specified)"
print("Device:", manufacturer, model_number)
else:
print("No device information")
pulse_ox_service = pulse_ox_connection[BerryMedPulseOximeterService]
while pulse_ox_connection.connected:
print(pulse_ox_service.values)
except connection_error:
try:
pulse_ox_connection.disconnect()
except connection_error:
pass
pulse_ox_connection = None

View on GitHub

Run the example program, and turn on the pulse oximeter, reading ‎from your finger. Here's a screenshot from running it on Windows, in ‎PowerShell. In this example, I typed ctrl-C after getting a few ‎readings.‎

Pulse Oximeter

Heart Rate Monitor

This is a Schoshe Heart Rate Monitor, which transmits data using the ‎standard BLE Heart Rate Monitor service. Install the heart rate library ‎by typing the pip3 command below into your shell. Then download ‎the example program below.‎

heart_5

Download File

Copy Code
pip3 install adafruit-circuitpython-ble-heart-rate

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 ladyada for Adafruit Industries
# SPDX-License-Identifier: MIT

"""
Read heart rate data from a heart rate peripheral using the standard BLE
Heart Rate service.
"""

import time

import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.standard.device_info import DeviceInfoService
from adafruit_ble_heart_rate import HeartRateService

# PyLint can't find BLERadio for some reason so special case it here.
ble = adafruit_ble.BLERadio() # pylint: disable=no-member

hr_connection = None

while True:
print("Scanning...")
for adv in ble.start_scan(ProvideServicesAdvertisement, timeout=5):
if HeartRateService in adv.services:
print("found a HeartRateService advertisement")
hr_connection = ble.connect(adv)
print("Connected")
break

# Stop scanning whether or not we are connected.
ble.stop_scan()
print("Stopped scan")

if hr_connection and hr_connection.connected:
print("Fetch connection")
if DeviceInfoService in hr_connection:
dis = hr_connection[DeviceInfoService]
try:
manufacturer = dis.manufacturer
except AttributeError:
manufacturer = "(Manufacturer Not specified)"
try:
model_number = dis.model_number
except AttributeError:
model_number = "(Model number not specified)"
print("Device:", manufacturer, model_number)
else:
print("No device information")
hr_service = hr_connection[HeartRateService]
print("Location:", hr_service.location)
while hr_connection.connected:
print(hr_service.measurement_values)
time.sleep(1)

View on GitHub

Turn on your heart rate monitor and run the example program. ‎reading from your finger. Here's a screenshot from running it on ‎Ubuntu Linux. In this example, I typed ctrl-C after getting a few ‎readings.‎

Heart rate monitor example program

iBBQ Thermometer

Here's a BLE-enabled food thermometer, which can take two probes. ‎It and similar models are readily available under the "nutrichef" ‎brand name and identify as "iBBQ" in their BLE advertisements.‎

Install the iBBQ library by typing the pip3 command below into your ‎shell. Then download the example program below.‎

thermometer_7

Download File

Copy Code
pip3 install adafruit-circuitpython-ble-ibbq

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 ladyada for Adafruit Industries
# SPDX-License-Identifier: MIT

import time

import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble_ibbq import IBBQService

# PyLint can't find BLERadio for some reason so special case it here.
ble = adafruit_ble.BLERadio() # pylint: disable=no-member

ibbq_connection = None

while True:
print("Scanning...")
for adv in ble.start_scan(ProvideServicesAdvertisement, timeout=5):
if IBBQService in adv.services:
print("found an IBBq advertisement")
ibbq_connection = ble.connect(adv)
print("Connected")
break

# Stop scanning whether or not we are connected.
ble.stop_scan()

if ibbq_connection and ibbq_connection.connected:
ibbq_service = ibbq_connection[IBBQService]
ibbq_service.init()
while ibbq_connection.connected:
print(
"Temperatures:",
ibbq_service.temperatures,
"; Battery:",
ibbq_service.battery_level,
)
time.sleep(2)

View on GitHub

Turn on your thermometer and run the example program. Here's a ‎screenshot from running it on MacOS. In this example, I typed ctrl-C ‎after getting a few readings.‎

Thermometer example program

BLE UART

One simple way of communicating between two BLE devices is to ‎use a simulated "UART". A UART provides a bi-directional byte ‎stream, so that both ends of a connection can transmit and receive ‎bytes with each other.‎

There are standard BLE UART services, such as the Nordic UART ‎Service (NUS). The Adafruit Bluefruit Connect app uses NUS to talk to ‎BLE boards.‎

Once you get the UART service working, it's easy to invent your ‎own ad hoc protocol that sends and receives commands and data ‎over the serial stream.‎

BLE UART Python eval() Example

Here's a simple example that uses BLE UART to send a text string ‎from a host computer to a CircuitPython board over BLE. The board ‎calls the Python function eval() on the string, to evaluate it as a ‎Python expression, and sends the result back as a string to the host ‎computer. For instance, the host might send 2+2, and the board will ‎send back 4.‎

To try this example, first install this library from the latest library ‎bundle on your BLE-capable CircuitPython board, such as a Feather ‎nRF52840 or a Circuit Playground Bluefruit:‎

  • adafruit_ble

Then copy the program below to CIRCUITPY on your CircuitPython ‎board as code.py:‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 Dan Halbert for Adafruit Industries
#
# SPDX-License-Identifier: MIT

# Provide an "eval()" service over BLE UART.

from adafruit_ble import BLERadio
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.nordic import UARTService

ble = BLERadio()
uart = UARTService()
advertisement = ProvideServicesAdvertisement(uart)

while True:
ble.start_advertising(advertisement)
print("Waiting to connect")
while not ble.connected:
pass
print("Connected")
while ble.connected:
s = uart.readline()
if s:
try:
result = str(eval(s))
except Exception as e:
result = repr(e)
uart.write(result.encode("utf-8"))

View on GitHub

Now copy the second program to your host computer and run it. ‎Wait for it to connect to your board, and then type some Python ‎expressions at the Eval: prompt. ‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 Dan Halbert for Adafruit Industries
#
# SPDX-License-Identifier: MIT

# Connect to an "eval()" service over BLE UART.

from adafruit_ble import BLERadio
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.nordic import UARTService

ble = BLERadio()

uart_connection = None

while True:
if not uart_connection:
print("Trying to connect...")
for adv in ble.start_scan(ProvideServicesAdvertisement):
if UARTService in adv.services:
uart_connection = ble.connect(adv)
print("Connected")
break
ble.stop_scan()

if uart_connection and uart_connection.connected:
uart_service = uart_connection[UARTService]
while uart_connection.connected:
s = input("Eval: ")
uart_service.write(s.encode("utf-8"))
uart_service.write(b'\n')
print(uart_service.readline().decode("utf-8"))

View on GitHub

Here's an example of running the ble_eval_client.py program on a ‎Raspberry Pi Zero W, talking to a Circuit Playground Bluefruit.‎

Note that errors, like division by zero, are caught and reported. Also ‎note you can only type Python expressions, not statements. ‎So, a = 3 doesn't work.‎

Python expressions

Troubleshooting

Reset Bluetooth

Sometimes the Bluetooth system software on the host computer ‎becomes stuck, confused, or in a bad state. This can cause Blinka ‎bleio programs to stop working. Often a simple fix is just to turnBluetooth off and then back on, on the host computer.‎

Windows

There are two ways to cycle Bluetooth off and on in Windows. In ‎Settings, find the Bluetooth setting page, and turn Bluetooth off and ‎then back on:‎

Windows Bluetooth

Or select the Notification area by clicking the Notification icon in the ‎taskbar (1), and then toggle Bluetooth off and then back on (2):‎

notification_11

macOS

Go to System Preferences and choose Bluetooth (1). Then toggle ‎Bluetooth off and on (2). If you check the box that says, "Show ‎Bluetooth in menu bar" (3), you can toggle Bluetooth more quickly ‎‎(4).‎

system_12

system_13

system_14

Linux and Raspberry Pi

Depending on which Linux distribution and desktop software you're ‎using, there might be a Bluetooth item in the task bar or menu bar ‎for your desktop that will allow to you cycle Bluetooth off and back ‎on easily. For instance, the default Raspberry Pi desktop has a ‎Bluetooth icon in the top menu bar; you can turn Bluetooth off and ‎then back on from there.

bluetooth_15

If you don't have a desktop icon to use, you can cycle Bluetooth from ‎the command line. For Raspberry Pi OS, Debian, and Ubuntu, type ‎these commands into your shell:‎

Download File

Copy Code
rfkill block bluetooth
rfkill unblock bluetooth

You may find it convenient to create a script to do this. For instance, ‎you can put these commands into a file called btcycle, make it ‎executable, and put it in some directory on your PATH:‎

Download File

Copy Code
#!/bin/bash
# Cycle Bluetooth on and off to reset it.
rfkill block bluetooth
rfkill unblock bluetooth
# Wait for bluetooth to come back on. You may need to change this delay.
sleep 1.5
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.