Maker.io main logo

Getting Started with Electroluminescent (EL) Wire

928

2018-07-25 | By SparkFun Electronics

License: See Original Project Wearables

Courtesy of SparkFun

Introduction

When it comes to creating projects that glow, nothing beats Electroluminescent wire (or EL wire for short). LEDs are fun and all, but EL wire is what all the hip kids are using. Whether you just want to light up your bicycle for an evening cruise or you’re creating an entire light up costume for Burning Man, EL wire is a great solution.

In this tutorial, we will show you how to get started with EL wire. With the right parts, EL wire can be very easy to integrate into any project! 

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing. A general understanding of electricity is necessary to understand the theory behind EL Wire operation. EL Wire is powered with AC power. It’s not as dangerous as the electricity coming from you home outlets, but it does deserve the same respect. Depending on your setup, you will need to understand how a circuit works.

Suggested Videos

 

 

 

Having a hard time seeing the videos? Try viewing them in a full screen mode.

How EL Works

EL wire (short for electroluminescent wire) is particularly useful for many reasons. Nevertheless, there are a few characteristics to keep in mind.

Note: For the sake of this tutorial, we will refer to EL wire, tape, and panels simply as EL wire unless stated otherwise.

EL Wire, Tape, Panel, Chasing Wire, Bendable Wire Forms

Electroluminescent products come in many different shapes and sizes. You can get it in wire (the most typical shape), tape, panels, and bendable form. All of these can be cut to any shape or size to achieve the desired effect. Just be sure to reseal the ends that have been cut.

Heads up! The benefit of bendable EL wire is that it allows you to articulate and mold your EL wire any way that you want! However, it is thicker than standard EL wire and chasing wire due to the additional bendable wire that runs alongside the phosphor wire. The extra bendable wire makes it ideal for art projects but it can be still used for e-textiles depending on the application.

Colors

EL also comes in many different colors. Below are a few options for standard EL wire.

There are other options available for EL tape, panel, chasing wire, and bendable wire.

CLICK TO BROWSE MORE COLORS OPTIONS FOR DIFFERENT EL MATERIALS

Heads up! Depending on the manufacturer, the color may vary between standard EL wire, tape, panel, chasing wire, and bendable wire.

Flexible

EL wire is flexible to a point. It allows you to sew it into clothing, attach it to moving parts, and bend it into any shape you desire. EL wire is more flexible than using LED strips but you will want to avoid sharp bends.

EL Wire Bends on a DIY Neon Sign

EL Wire Bends on a DIY Neon Sign

EL tape and panels can also be used in e-textile projects. However, they are not as flexible as EL wire. They are better in projects when there is reinforced fabric to support the material.

EL Tape and Panels on Shirts

EL Tape and Panels on Shirts

EL Panel Patches on a Hat, Bag, and Jacket

EL Panel Patches on a Hat, Bag, and Jacket

Low Power Consumption

EL requires less power to operate compared to using several LEDs for a project. EL is also great because it is cool to the touch, even after being on for hours. Hence why it is often seen in clothing applications. The EL does not heat up because, rather than heating an element to achieve an optical phenomenon, the glowing in EL comes from sending an electrical current through the material, which is comprised of semiconducting mixtures. The electrons flowing through the material create photons, which create the glowing that we see as a result.

EL Wire

Let It Glow… In a Dark Room

While EL has a nice glowing effect, it can be hard to see in the daylight or when there is light in a room. It would be better to use EL in low light conditions for the best effect.

use EL in low light conditions for the best effect

Left: EL in a Bright Room, Right: EL in Low Lighting

AC Power

Many people ask, "Can’t I just hook up EL wire to a battery?" The answer is, no! In order to operate EL wire properly, you must use AC (alternating current) power. This is similar to the power that comes out of your wall outlets at home, though outlets provide much more current than needed for EL wire. That’s where the inverter comes in!

The battery pack included in the EL starter kit and the chasing inverter are not just a battery holder. It houses an inverter as well. This inverter takes the DC (direct current) power produced by the batteries and turns it into AC. If you listen very closely to the inverter battery pack while it’s on, you will hear a slight hum, similar to what you would hear if you stand under power lines or close to transformer boxes. Compared to the battery pack however, the 3V and 12V inverters do not have a battery holder build in.

Note: SparkFun does not condone hanging out around high voltage areas.

With that, it’s important to mention that the AC power coming from the inverter is not enough to hurt or kill you. However, it is enough to give you a good shock. Be careful when handling EL products and any exposed circuits that are powered on the AC side. You can cut EL to any length or shape, but you must reseal the ends you cut. If you do not have an end cap for the EL wire, you can still seal the ends with hot glue or epoxy to seal cut wire. If you don’t reseal, you could end up getting a good jolt.

Anatomy of EL

EL consists of a few layers. Let's take a look at the anatomy of standard EL wire.

  • Colored, Clear PVC Sleeve – On the outside is a colored PVC sleeve. Depending on the manufacturer and color, this may be clear or translucent.

  • Clear PVC Sleeve – A second layer is yet another PVC sleeve. This sleeve is not as thick as the outer layer and is also clear.

  • Corona Wires – There are two thin wires that wrap around and extend to the end of the EL wire. These are very fine and can sometimes be referred to as angle wires. The wire pair is isolated from the center core.

  • Phosphor Coating – Applying AC power around the coating creates that nice glowing effect from the phosphor being excited. It also separates the corona wires and core.

  • Core Wire – At the center of EL wire is another wire.

The first image is a physical diagram of EL wire. The second is a close up of white EL wire opened up. Regardless of the labels in the images, each component functions the same.

physical diagram of EL wire

Image courtesy of LogiNevermore from Wikipedia: Electroluminescent Wire

Closeup of Standard EL Wire

Closeup of Standard EL Wire

Hardware Hookup - EL

Recommended Materials

At a minimum, you'll need the following to power EL. We will be using the following components to get started. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Note: You may have opted for Chasing EL Wire instead of the standard solid colors. That's fine. This tutorial will focus on both kinds of EL Wire and how to use each. We'll discuss this in detail a little later.

Depending on your inverter, you may also need the following:

  • Wires (Optional) – Depending on your setup and inverter being used, you may need wires.

  • Insulation (Optional) – Electrical tape, heat shrink, hot glue, or epoxy to seal the exposed pins and wires connected to the AC side.

Note: SparkFun sells a kit with the parts available in the EL Wire Starter Kit with one strand of blue EL wire (3m).

EL Inverter - Battery Pack

Using the EL is about as simple as it gets when using the EL inverter battery pack.

EL Inverter - Battery Pack

EL Inverter - Battery Pack

Take the battery cover off by sliding in the direction indicated on the pack. Place your two AA batteries in the battery pack inverter, and put the cover back on. Plug in the male JST connector from your EL wire into one of the two female JST connectors on the inverter battery pack. Make sure there is a solid connection between the two.

Plug in male connector into female connectors

Press the button on the case and your EL wire should illuminate. Press it again for a slow blinking effect, and press it once more for a fast blink. This inverter pack allows you to connect two EL products of your choice at a time. You can mix and match colors as well as shapes. You could have a red panel with blue wire, green tape with a pink wire, or two yellow and purple wires. The possibilities are endless!

Press button on case and your wire should illuminate

Note: The following current readings were taken while the pack was connected to one or more of our 3m of EL wire:

  • Single Strand Always On: 190mA to 260mA

  • Single Strand Blinking: 90mA to 120mA

  • Two Strands Always On: ~300mA

  • Two Strands Blinking: ~150mA

Different color strands were used but the lengths were identical. Your mileage may vary.

Modifying the EL Inverter Battery Pack: We got a chance to play with these inverters and you can easily hack these to work with our Li-Po batteries (yep, fully charged at 4.2V). To get inside, you’ll need to remove a pair of screws (one is hiding under the CE sticker) and afterwards you’ll want to wrap things up with electrical tape to avoid getting shocked (it just tingles a little).

EL Inverter - 3V

We also have a 3V inverter. The wires are terminated at the end with JST PH connectors. These require a little bit more work to get started since they are designed to plug directly into our EL Escudo Dos or EL Sequencer. They are ideal for small EL displays.

EL Inverter - 3v

EL Inverter - 3v

This particular EL inverter accepts an input (on the red/black pair of wires for VCC and GND, respectively) anywhere from 2.5V-4.2V, so you can use them with batteries. Once powered, it can output up to 110VAC (on the black/black pair of wires) to drive EL wire.

⚡ Note: While that datasheet states that the input is between 2.5V-3.5V, we have tested the inverter with LiPo batteries. The 3V inverter can take up to 4.2V, so it's safe to run on a LiPo battery.

With the 3V inverter, you can drive EL wires directly without using an EL Escudo Dos or EL Sequencer. However, you may need to re-terminate them, make an adapter, or possibly regulate the voltage down from your power supply. Below is a simple connection if you are just powering one strand for an installation using a 5V USB power supply, 3.3V FTDI to regulate the voltage down, M/M jumper wires, and one strand EL wire. The pins of the jumpers are small enough to be inserted into a JST connector.

simple connection if you are just powering one strand

You can even connect two strands together by making a parallel connection. For testing purposes, the circuit was placed on a breadboard. It should not matter what color of wire is connecting on the inverter's output since it is AC. The wire colors were connected together for consistency.

Connect two strands together

Tests with Different Lengths of EL Wire: Some real-world testing revealed that this inverter can easily drive a 3m length of EL wire. When adding a second 3m length, the two get a bit dimmer, but still close to full brightness. At three 3m lengths, you can only tell all three wires are on if the room is dark. While the inverter can light up 4 strands, they are barely visible in normal light and very dim in the dark as well.

As you can see from the images below, connecting more EL wire in parallel with the 3V inverter will cause both EL wires to dim. The brightness can depend on the length of EL you are using, how you are wiring the EL, and the type of inverter.

Connecting wires in parallel causes both wires to dim

Left: One 3M EL Wire Lit Up, Right: Two 3M EL Wires Lit Up but Dimmer

When you are done testing and integrating the EL wire in a project, make sure to seal any exposed EL wire or connections on the AC side. Electrical tape is a good option to secure the connection and insulate any exposed pins should you decide to continue using M/M jumper wire between an inverter and EL wire.

seal any exposed EL wire

EL Inverter - 12V

When using several strands of EL, you may want to consider using the 12V inverter. The inverter consists of a barrel jack connector and a pair of wires terminated with a JST PH connector. These are ideal for the biggest, brightest display possible!

EL Inverter - 12v

EL Inverter - 12v

This particular EL inverter accepts an input via the 5.5mm x 2.1mm barrel jack connector. Simply connect a power source with a center positive barrel jack connector. The output (red/black pair or wires) was designed to connect to a mating JST connector on the EL Escudo Dos or EL Sequencer board. There is also a small switch on the side which allows you to switch between "on", "blink", and "off" settings.

As with the 3V inverter, you can drive EL wires with the 12V inverter directly. However, you may need to re-terminate them or make an adapter. Below is a simple connection if you are just powering one strand for an installation using a 12V power supply, M/M jumper wires, and one strand EL wire.

you can drive EL wires with the 12V inverter directly

Again, you can connect two strands together by making a parallel connection. For testing purposes, the circuit was placed on a breadboard. It should not matter what color of wire is connecting on the inverter’s output since it is AC. The wire colors were connected together for consistency.

Connect two strands together

Remember to seal any exposed EL wire or connections on the AC side when you are done.

seal any exposed EL wire or connections

⚡ Remote/Mobile Applications: While that datasheet states that the input is between 11V-13V, you can power the 12V EL Inverter with 9V alkaline battery and adapter for remote applications. The EL might not be as bright as using a 12V power supply but you will not notice a significant difference in the dark with a few meters of EL.

Stress Tests with the 12V Inverter: The 12V inverter has been tested to run 8x strands of 3m EL wire using an EL Sequencer and a 12V power supply. Remember, as you increase the length or wire more in parallel, this will increase the load on the inverter causing the EL to dim.

How EL Chasing Wire Works

EL chasing wires work in a similar fashion to standard EL wire. Instead of one core wire, there are three thin wires coated in phosphor. Basically, you can think of three strands of standard EL wire smashed into one EL chasing wire. As a result, EL chasing wire requires 4x connections: three for each strand and one for common ground. By sequencing each strand inside by turning them on and off, we have a cascading or "chasing" effect.

EL chasing wire

Let's take a look at the anatomy of EL chasing wire.

  • Colored, Clear PVC Sleeve – On the outside is a colored PVC sleeve. Depending on the manufacturer and color, this may be clear or translucent.

  • Clear PVC Sleeve – A second layer is yet another PVC sleeve. This sleeve is not as thick as the outer layer and is also clear.

  • Corona Wires – There are two thin wires that wrap around and extend to the end of the EL wire. These are very fine and can sometimes be referred to as angle wires. The wire pair is isolated from the center core wires.

  • Phosphor Coating – Applying AC power around the coating creates that nice glowing effect from the phosphor being excited. It also separates the corona wires and core wires.

  • Core Wires – At the center of EL chasing wire are three thin wires coated and twisted at the center.

anatomy of EL chasing wire

If you compare the size of EL standard wire and chasing wire, you will not notice the difference until you are modifying and repairing the core wire. As you can see, EL chasing wire uses three thin wires at the core.

compare the size of EL standard wire and chasing wire

Hardware Hookup - EL Chasing

EL Inverter - 3v (Chasing)

The EL chasing inverter works similar to the 3V EL inverter battery pack.

EL Inverter - 3v (Chasing)

EL Inverter - 3v (Chasing)

Simply take the battery cover off by sliding it off, insert two AA batteries for power, slide the cover back on, and connect one EL chasing wire to the 4-pin mating connector. Press the button to turn on and begin sequencing the three strands of EL wire in one. Continue pressing the button to cycle through the three modes: slow, fast, and super-duper fast chase!

EL chasing wire

Stress Tests with the EL Chasing Inverter: It is recommended that these inverters only run up to 5m of EL wire, you may not have enough power to support longer lengths.

EL Wire Extension Cables

Need just a little more length in between your JST connector and EL? There are few methods to extend the wires to your EL. One method is splicing the wires leading to the EL material. Below is an example of extending the wires to an EL panel but it can be used for wires leading to any EL. For more information about how to extend the wires, head over to the Pokémon Go Patches with EL Panels: Adding EL Extension Cables tutorial.

Spliced Wires to Extend Wires to EL

Spliced Wires to Extend Wires to EL

Controlling and Sequencing EL

Working with a just a few EL products is fairly straight forward. However, if you are looking for more of a challenge, fear not. EL projects can become very complex, very quickly. You may have noticed that the effects are somewhat limited on the inverter, and both products hooked up behave the same when plugged into it.

Let’s say you want one color to blink while the other stays solid. You could purchase another inverter battery pack, or you could get one of the many boards out there that are specifically designed to work with EL products. SparkFun carries two such boards, the EL Sequencer and the EL Escudo Dos. Both of these boards are designed to handle many EL products hooked up to them at once, and there are many different effects you can create with both.

SparkFun Animated Flame

SparkFun Animated Flame from Setting Up an EL Display with the EL Escudo Dos Tutorial

For more information, check out the hookup guide on those products.

Resources and Going Further

Thanks for checking out our tutorial! Now that you’ve successfully got your EL wire/panel/strip up and running, it’s time to incorporate it into your own project! For more information, check out the resources below:

מק"ט יצרן # 11222
EL INVERTER - BATTERY PACK
SparkFun Electronics
מק"ט יצרן # 13746
BRIDGE USB 2.0 MODULE
SparkFun Electronics
מק"ט יצרן # 08431
JUMPER WIRE M/M 6" 10PCS
SparkFun Electronics
מק"ט יצרן # 09518
BATT CONNECT SNAP 9V BARREL PLUG
SparkFun Electronics
מק"ט יצרן # 10512
BATTERY HOLDER 9V BARREL PLUG
SparkFun Electronics
מק"ט יצרן # 12781
EVAL BOARD FOR ATMEGA328P
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.