Maker.io main logo

LED Noodle Lamp

530

2025-01-17 | By Adafruit Industries

License: See Original Project 3D Printing Addressable LEDs Solder / Desoldering

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

lamp_1

Unique LED Bulb

You can build a Victorian-era inspired lamp using an LED Noodle ‎and 3D printed parts.‎

This features a 12V LED noodle that’s shaped in a zigzag pattern that ‎wraps around a transparent 3D printed core. A glass dome fits over ‎the LED giving this a unique aesthetic.‎

led_1

USB-C Power Delivery

The HUSB238 breakout is a power delivery board that lets you power ‎devices using USB-C wall adapters with multiple voltages.‎

This features the HUSB238 chip, STEMMA QT for I2C control, screw ‎block terminals and dip switches so you can easily toggle your ‎preferred voltage.‎

usb_3

Light Switch

Mounted inside the base is a 3D printed switch that is inspired by ‎the humble household light switch. It’s a print-in-place part that has ‎a really satisfying click that lets you turn the lamp on and off.‎

leds_onoff

switch_4

Parts

Additional Parts

USB PD power supply must be able to supply 12V at 1A minimum.‎

Hardware

  • ‎4x M2.5 x 6mm long steel screws‎

  • ‎10x M3 x 6mm long steel screws‎

  • ‎4x M3 x 10mm long steel screws‎

  • ‎2x M3 x 20mm long steel screws‎

  • ‎2x M3 hex nuts‎

PLA Filament

Choose your own preferred brand and colors of filament. The colors ‎listed below were used in this project.‎

Circuit Diagram

The diagram below provides a general visual reference for wiring the ‎components once you get to the Assembly page. This diagram was ‎created using the software package Fritzing.‎

Adafruit Library for Fritzing

Adafruit uses the Adafruit Fritzing parts library to create circuit ‎diagrams for projects. You can download the library or just grab ‎individual parts. Get the library and parts from GitHub - Adafruit ‎Fritzing Parts.‎

  diagram_5

Wired Connections

Slide Switch

  • PIN#1 from switch to ON Pin (either pad) on HUSB238 ‎Breakout

  • PIN#2 from switch to ON Pin (either pad) on HUSB238 ‎Breakout

‎12V LED Noodle‎

  • Anode from LED to Positive pin on HUSB238 Breakout

  • Cathode from LED to Negative pin on HUSB238 Breakout

PD USB Power Supply

The HUSB238 Breakout is powered by a PD USB power supply ‎‎(capable of 12V 1A output) into a wall outlet.‎

CAD Files

‎3D Printed Parts‎

STL files for 3D printing are oriented to print "as-is" on FDM style ‎machines. Parts are designed to 3D print without any support ‎material using PLA filament. Original design source may be ‎downloaded using the links below.‎

printed_6

Download STLs.zip

Download CAD source

CAD Assembly

The LED noodle is press fitted into the LED holder. The LED holder is ‎secured to the coupler and base with screws. The LED subassembly ‎is secured to the top base cover.‎

leds_cad

The main case is secured to the top base cover with screws. The ‎switch plate slides into the main case. The slide switch is press fitted ‎into the toggle switch adapter. The toggle switch is secured to the ‎switch plate.‎

The bottom frame and base are secured together, then it snap fits ‎into the main case. The HUSB238 breakout is secured to the bottom ‎cover using screws. The bottom cover snap fits under the bottom ‎base.‎

Build Volume

The parts require a 3D printer with a minimum build volume.‎

  • ‎120mm (X) x 120 (Y) x 120mm (Z)‎

build_8

Transparent PLA

The LED holder looks the best when printed using a ‎clear/transparent filament. The 3D model is thin and should only use ‎a single parameter when 3D printed.‎

pla_9

Design Source Files

The project assembly was designed in Fusion 360. This can be ‎downloaded in different formats like STEP, STL and more.‎

Electronic components like Adafruit's boards, displays, connectors ‎and more can be downloaded from the Adafruit CAD parts GitHub ‎Repo.

components_10

Wiring

Set Voltage

Using a fine precision tool, enable the dip switch to set the voltage to ‎‎12V. ‎

wiring_11

Wire for Switch

Use the silicone ribbon cable to create a piece of 2-wire cable that ‎measures 7 inches in length.‎

Using wire strippers, remove a bit of insulation from each end of the ‎wires.‎

Tin the exposed wires with a bit of solder – this prevents the wires ‎from fraying when soldering. ‎

wire_12

Prep Switch

Use flush snips to remove one of the legs (either far left or right but ‎not the middle).‎

Trim the remaining two legs so they're about half their length.‎

prep_13

Solder Wire to Switch

Tin the legs of the switch with a bit of solder. ‎

Attach the 2-wire cable to the two pins on the slide switch using a bit ‎of solder.‎

attach_14

attach_15

Attach Switch Wire to HUSB ‎Breakout

Solder the cable from the slide switch to the switch pins on the ‎HUSB238 breakout.‎

breakout_16

breakout_17

Prep Resistor

Pick out a single 100ohm resistor from the pack and trim the two ‎legs short using flush snips.‎

prep_18

Wire for LED Noodle

Use the silicone ribbon cable to make two long wires for the LED ‎noodle, preferably one wire with a marking to indicate polarity.‎

Create a piece of 2-wire cable that measures 9 inches in length. ‎

noodle_19

Solder Wire to LED

Locate the end of the LED with the anode pin (the one with the hole).‎

Solder the marked wire to the anode pin on the LED noodle.‎

solder_20

Heat Shrink

Add a piece of colored heat shrink tubing to the anode connection. ‎This helps to insulate the exposed pin and denotes the voltage wire.‎

Continue to solder the cathode pin on the LED noodle to the ‎remaining wire. ‎

Add another piece of heat shrink (preferably black) to insulate the ‎exposed connection.‎

heat_21

Ground Wire

Locate the end of the ground wire connection and cut off about 4 ‎inches.‎

Use wire stripper to remove a bit of insulation from the freshly cut ‎wires.‎

The 100ohm resistor will be soldered in-line with the ground wires.‎

ground_22

Attach Resistor

Solder the 100ohm resistor in line with the short wire and the longer ‎ground wire.‎

resistor_23

Wired LED

Double check the 100ohm resistor has been properly soldered to the ‎wires.‎

wiredled_24

Test LED

Insert the cathode wire from the LED noodle to the negative marked ‎screw block terminal on the HUSB238 breakout. Then use a ‎screwdriver to secure the wire.‎

Secure the anode wire to the positive voltage screw block terminal.‎

Power the HUSB238 breakout using the USB PD wall adapter and ‎USB-C cable.‎

Use the slide switch to power on the LED noodle.‎

test_25test_26

LED Assembly

LED Holder

Get the 3D printed LED holder and LED noodle ready for assembly.‎

holder_27

Clean 3D Print

Use a hobby knife to remove any excess material from the outer ‎edge of the bottom of the 3D print.‎

clean_28

Use caution when working with a hobby knife. Eye and hand ‎protection would be prudent.‎

Installing the LED Noodle

Locate the bottom of the 3D printed LED holder. Begin fitting the ‎two ends of the LED noodle into the channels.‎

Make sure the two ends of the LED noodle are in a position that is ‎similar to the assembly photo.‎

locate_29

locate_30

Press Fitting LED

Continue to press the LED noodle into the channel, following the ‎zigzag shape.‎

Repeat the installing for the opposite end of the LED noodle.‎

press_31

Zigzag Loop

A lengthy loop of the LED noodle should be remaining. The ‎remaining noodle will loop over the top of the holder.‎

zigzag_32

Excess Top

Loop the remaining noodle over the top of the holder and start press ‎fitting the remainder into the closest channel.‎

Repeat the installation for the opposite end of the LED noodle.‎

excess_33

Installed LED Noodle

The LED noodle should have enough length to fit through the ‎bottom of the channel.‎

Double check the entire length of the LED noodle is pressed into the ‎channels.‎

double_34

Test LED Noodle

Connect the positive and negative wires from the LED noodle into ‎the corresponding pins in the HUSB238 breakouts screw-block. Use ‎a screwdriver to secure the connections. ‎

Power the USB breakout using a USB-C cable and the USB PD wall ‎adapter. ‎

Use the slide switch to power the LED noodle.‎

power_35

Coupler & Base

Get the LED coupler and base ready to assemble together.‎

Use the following hardware to secure the parts together.‎

  • ‎2x M3 x 6mm long steel machine screws‎

coupler_36

Install LED Coupler

Press the LED coupler into the bottom of the LED holder so it is fitted ‎into the recess.‎

Orient the parts so the two mounting tabs are lined up.‎

coupler_37

coupler_38

Install LED Base

Insert the LED wiring through the top of the LED base.

Orient the ‎LED base so the mounting tabs are lined up with the holder and ‎coupler.‎

insert_39

insert_40

Secure LED Base

Use the following hardware to secure the LED parts together.‎

  • ‎2x M3 x 6mm long steel screws‎

Fasten the two screws to secure the LED holder, coupler, and base.‎

base_41

Assembled LED Holder

Take a moment to ensure all of the parts have been properly ‎assembled.‎

assembled_42

Enclosure Assembly

Top Base Cover

Use the following hardware to secure the LED base to the top base ‎cover.‎

  • ‎2x M3 x 6mm steel screws‎

top_43

Install LED to Top Base Cover

Insert the LED wires through the center hole of the top base cover.‎

Place the LED base over the Top Base Cover so the mounting holes ‎are lined up.‎

Insert and fasten the M3 screws to secure the LED base to the Top ‎Base Cover.‎

fasten_44

fasten_45

Secured Top Base Cover

Take a moment to ensure the LED base has been properly installed ‎to the top base cover.‎

securetop_46

securetop_47

Base Case Installation

Get the base case ready to attach to the top base cover. Use the ‎following hardware to secure the parts together.‎

  • ‎4x M3 x 10mm long steel screws‎

base_48

Orient the top base cover with the case so the four mounting holes ‎in the corners are lined up.‎

Insert the LED wire through the top of the base case.‎

led_49

Secure Top Cover to Case

Begin inserting and fastening the screws to secure the top cover to ‎the case.‎

begin_50

Assembled Case

Take a moment to ensure the case has been properly secured to the ‎top base cover.‎

case_51

Light Switch Parts

Get the three light switch parts ready to assemble. Use the following ‎hardware.‎

  • ‎2x M3 x 20mm long steel screws‎

  • ‎2x M3 x 6mm long steel screws‎

  • ‎2x M3 hex nuts‎

light_52

Install Plate Decal

Place the plate decal over the switch plate and line up the mounting ‎holes.‎

Insert and fasten the two M3 x 6mm long screws to secure the parts ‎together.‎

decal_53

decal_54

Install Toggle Switch Adapter

Orient the toggle switch adapter and place it into the switch plate.‎

Insert the toggle switch through the opening in the switch plate and ‎line up the two mounting holes.‎

adapter_55

Secure Toggle Switch

Insert and fasten the two M3 x 20mm long machine screws through ‎the mounting tabs.‎

Use the two M3 hex nuts to secure the parts together.‎

toggle_56

toggle_57

Install Slide Switch

Orient the slide switch with the cavity in the toggle switch.‎

Press fit the slide switch into the cavity in the toggle switch adapter.‎

Test the toggle switch mechanism by flipping the actuator.‎

orient_58

orient_59

Bottom Base & Frame

Get the bottom base and frame ready to secure together using the ‎following hardware.‎

  • ‎4x M3 x 6mm long machine screws‎

bottom_60

Orient the bottom base and frame so the snaps are correctly lined ‎up. Reference the assembly photo for the correct orientation.

Place the bottom frame over the bottom case and line up the four ‎mounting holes.‎

place_61

Secure Base and Frame

Insert and fasten the M3 screws through the four mounting holes to ‎secure the parts together.‎

secure_62

secure_63

Install Light Switch Plate

The switch plate subassembly is fitted through the opening in the ‎base case. ‎

The outer edges will prevent the plate from falling through the ‎opening.‎

Slide the switch plate all the way through the opening in the case.‎

plate_64

Install Bottom Frame to Case

Orient the bottom frame with the case so the snaps are oriented ‎correctly.‎

frame_65

Secured Bottom

Firmly press the bottom frame into the case so the parts snap fit ‎together.‎

snap_66

HUSB238 Breakout Placement

Place the HUSB238 breakout onto the bottom cover so the ‎mounting holes are lined up with the built-in standoffs.‎

Use the four M2.5 x 6mm long steel screws to secure the PCB to the ‎standoffs.‎

husb_67

husb_68

Secure LED Wires

Insert and secure the LED wires to the HUSB238 breakout so the ‎negative and positive are on the proper pins in the screw block.‎

wires_69

Test Toggle Switch

Power the HUSB238 breakout using a USB-C cable and a USB PD ‎wall adapter.‎

Use the toggle switch to test the LED noodle.‎

If the switch actuator feels incorrect, take the moment to flip and ‎reverse the switch plate so it's in the correct orientation.‎

testswitch_70

Install Bottom Cover

Orient the bottom cover with the bottom base so the USB port on ‎the breakout is facing the port opening.‎

Firmly press the bottom cover into the bottom base so they are snap ‎fitted together.‎

cover_71

cover_72

Install Glass Dome

Press the glass dome into the recess in the top base cover. It should ‎have a nice and snug fit.‎

dome_73

Final Build

Congratulations on your build! ‎

Take a moment to inspect your work and ensure all of the part have ‎been securely fastened together.‎

final_74

מק"ט יצרן # 5991
ADAFRUIT USB TYPE C POWER DELIVE
Adafruit Industries LLC
מק"ט יצרן # 5731
LED MOD WARM WHT LINEAR STRIP
Adafruit Industries LLC
מק"ט יצרן # 4293
THROUGH-HOLE RESISTORS - 100 OHM
Adafruit Industries LLC
מק"ט יצרן # 3891
CBL RIBN 4COND FLAT BLACK 3.28'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.