Maker.io main logo

Getting Started with Home Automation

384

2025-04-24 | By Pimoroni

License: See Original Project Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

We've been getting big into Home Automation recently and have added lots of exciting new ‎smart home products to our shop. If you're new to home automation, bewildered by the ‎choice and would like some pointers of what works nicely with what, then read on for a brief ‎primer.‎

We'll be covering a couple of different local home automation hub options and showing you ‎how to hook up the Zigbee sensors and devices that we stock. We'll also show you how you ‎can set up a simple automation.‎

What is home automation?‎

Home Automation involves making your home 'smart' by getting it to do things ‎automatically based on programmatically defined rules - so you can do cool stuff like ‎turning your lights on when it gets dark or when motion is detected in an area, turning on ‎your coffee maker in the morning or turning down the heating in your bedroom if it gets too ‎warm - once you get started, the possibilities are endless! To be able to do this kind of thing, ‎your devices need to be able to talk to each other - either through the internet or via a hub ‎connected to your local network.‎

Cloud vs local

Many smart devices that you can buy come with a link to install a proprietary app on your ‎phone to control your devices through 'the cloud'. Advantages of this method are that it's ‎super quick to get going and you can turn your devices on and off from anywhere (as long ‎as you and they both have an internet connection). However, there are a number of ‎disadvantages to this approach:‎

  • You'll typically need a different app for every manufacturer, so getting devices from ‎different ecosystems to talk to each other is often not possible.‎

  • As every instruction is transmitted over the internet to a remote server, ‎communication may be slow, or your devices may stop working in case of internet ‎outages.‎

  • Depending on the service you're using, there may be data security concerns.‎

  • Some manufacturers charge (or decide to start charging!) for their cloud services or ‎for storing historical data.‎

  • If a manufacturer stops trading or shuts down its cloud services, it might not be ‎possible to use your devices anymore.‎

The alternative to using cloud services is installing a smart hub or server in your home so ‎your devices can communicate with each other over your local network. That way, all your ‎data stays safely in your house, and internet connectivity is not required.‎

Choosing devices

Some sensors and devices are easier to get working over a local network than others - if ‎you're new to home automating we'd recommend starting with Zigbee devices. Zigbee is a ‎low-power, secure radio protocol that's used by many big manufacturers of home ‎automation devices, and it uses clever mesh networking to maintain robust local networks ‎of devices, even if some of them go offline. Zigbee is well supported in home automation ‎software and adding devices is typically very straightforward.‎

Here's a list of some of the Zigbee devices that we sell that would all be great options to start ‎with:‎

You may also want to check out Ikea's range of Zigbee smart home devices - they do some ‎nice ones including RGB LED strips, air quality sensors, and smart air purifiers (look for ‎products that say Zigbee on the box). Philips Hue smart bulbs also use Zigbee under the ‎hood and are generally easy to work with.‎

Choosing a smart hub

We sell a couple of different smart hubs, or you could build your own. Here's a quick ‎overview of the options.‎

Sonoff iHost

Sonoff iHost is a smart home hub that is a good choice if you're primarily planning on using ‎it with other Sonoff devices (though it does have some support for devices from other ‎manufacturers). It has a simple interface, is quick to get started with and it can connect to ‎both Wi-Fi and Zigbee devices without the need for additional hardware. It comes with a ‎USB-C cable but not a wall plug, so you'll need to pick up something like this USB-C power ‎supply if you want to plug it into a wall outlet.‎

Home Assistant Green

If you're up for something with a little more complexity (but a lot more power), check ‎out Home Assistant Green which comes pre-loaded with our favourite smart home hub ‎software - Home Assistant.‎

We love Home Assistant because it's open source, has a large user base and is very actively ‎developed. It's compatible with many different devices from many different manufacturers ‎and is perfect if you're like us and have amassed quite a collection of random smart devices ‎and want them all to work together. Check out NetworkChuck's video for an introduction ‎the kind of things it can do!‎

Home Assistant Green comes in a nice enclosure with silent passive cooling and built on ‎fast in eMMC storage, with Home Assistant pre-installed and ready to go straight out of the ‎box. Note that Wi-Fi and Zigbee connectivity is not built-in, so you'll need to pick up ‎a seperate Zigbee USB adapter if you want to use it with Zigbee sensors.‎

Home Assistant on a Raspberry Pi

Alternatively, Home Assistant will run great on a Raspberry Pi 4 or 5, so you could design ‎your own hardware based on your preferences or make use of kit that you already have. ‎Here's our suggested kit list for building a capable Home Assistant machine using ‎Raspberry Pi 5.‎

  • Raspberry Pi 5 (we'd suggest going for 4GB RAM or larger, so you have plenty of RAM ‎to handle lots of devices and integrations)‎

  • A micro-SD card (32GB or larger)‎

  • Power supply

  • Some sort of cooling - for a minimal setup you could add an Active Cooler, or if ‎you'd prefer to keep everything enclosed you could get a case with active and ‎passive cooling built in, like the Argon ONE V5.‎

  • USB Zigbee adapter (if you want to use Zigbee sensors). The official Home ‎Assistant one or the Sonoff one will both work (though note that the Sonoff adapter ‎is bigger than the HA one, so it might not fit neatly into all setups).‎

You could keep all your data on your SD card, but you might also want to consider adding ‎some speedy solid-state storage, with an NVMe Base and SSD or a case that includes ‎NVMe functionality.‎

Instructions on how to install Home Assistant on your SD card can be found here (TLDR; ‎you can flash it with Raspberry Pi Imager - find it under 'other specific purpose OS').‎

If you want to install Home Assistant on a NVMe drive, you'll first need to update your ‎Raspberry Pi's firmware to the most recent version. You can do this by installing Raspberry ‎Pi OS on your SD card and following the instructions in this guide. Once that's done, you'll ‎be able install Home Assistant on your SSD using Pi Imager on the Pi or by the network boot ‎utility.‎

First time setup

Setting up Home Assistant

Comprehensive instructions how to set up and get started with Home Assistant can be ‎found here.‎

Here's the TLDR; connect your smart home hub to your home router via a wired ethernet ‎connection. Power it up and give it a couple of minutes to get connected - once it's up and ‎running you'll be able to access it by going to http://homeassistant.local:8123/‎

Adding Zigbee functionality to Home Assistant

If you're using a separate Zigbee USB adapter, plug this into your Raspberry Pi or Home ‎Assistant Green. Our adapter was autodetected and the web interface prompted us to ‎install the Zigbee Home Automation integration. We'd suggest restarting Home Assistant ‎after that (from Settings, the option to restart can be found under the menu at the top right):‎

adding_1

Once the integration is installed and running, connecting a new device should be as simple ‎as putting both the device and the Zigbee Home Automation integration into pairing mode, ‎and waiting for the device to be detected.‎

Setting up Sonoff iHost

Sonoff's instructions for how to get iHost up and going can be found here. Connect it to ‎your router with the ethernet cable and press the power button to turn it on. When the light ‎on the front turns blue it's connected to the network, and you can access the hub's interface ‎by going to http://ihost.local in your web browser.‎

Adding some sensors

Your new smart hub probably looks pretty empty - so we'd suggest adding some sensors ‎and devices to it!‎

Putting devices into pairing mode

Many of the battery powered Sonoff sensors ship with plastic battery tabs that you will need ‎to remove to power up the device. When you do that, they will automatically go into pairing ‎mode and an LED somewhere on the device will start flashing. Pairing mode can also be ‎activated manually - the Sonoff devices have a button (some are externally visible; some are ‎hidden within the battery compartment) that you can hold down until the LED starts ‎flashing.‎

Different manufacturers have different 'secret knocks' for putting their Zigbee devices into ‎pairing mode. The documentation that comes with the device should let you know how to ‎put your device into pairing mode.‎

Putting Home Assistant into pairing mode

You can tell Home Assistant to start searching for new Zigbee devices by going to Settings > ‎Devices and Services > Add Integration > Add Zigbee Device.‎

For best results, put your device close to the hub whilst it's pairing - the connection range ‎will be reduced until it's established in the Zigbee mesh network.‎

searching_2

Once Home Assistant sees your sensor, it should show up like this:‎

searching_3

It can sometimes take a few goes to get the timing right, and we've found some sensors are ‎quicker to pair than others - battery powered ones tend to poll the server less frequently.‎

After your sensor is successfully paired, it should show up automatically in your default ‎dashboard.‎

dashboard_4

You can give the sensor a more memorable name, change the icon and assign the sensor ‎to an area by clicking on the sensor in the dashboard, and then clicking on the cog:‎

name_5

Putting Sonoff iHost into pairing mode

Pairing devices works in a similar way if you're using a Sonoff iHost. Go ‎to http://ihost.local/ and click on the '+' button at the top right, then choose 'Add Zigbee ‎Device'.‎

pairing_6

Setting up your first automation

Now that you've got some devices added, you can get to the good stuff - setting up things to ‎happen automatically, so you don't have to use valuable brain power worrying about them ‎anymore.‎

Setting up automations in Home Assistant

To set up an automation in Home Assistant, go to Settings > Automations & Scenes > ‎Create Automation.‎

setting_7

Here's a simple one we've got set up to make an Ikea LED strip light up red when our ‎window is open (so we remember to close it at the end of the day!):‎

lightup_8

And one to turn it off when the window is closed:‎

turnoff_9

Setting up Automations with Sonoff iHost

Automations are 'scenes' if you're using a Sonoff iHost - that's the second icon down on the ‎menu bar that looks like a cube. You can add a new automation by clicking on the '+' at the ‎top right.‎

Here's an example of an automation that we've set up to turn our desk lights on when ‎motion is detected by a sensor. The lights are plugged into a USB switch:‎

example_10

And here's an associated automation to turn the lights off when motion is not detected:‎

example_11

Next steps

If you want to learn more about Home Assistant and all the amazing things you can do with ‎it check out the Home Assistant Community forums. You can also come and chat about ‎home automation on our forums or Discord - we'd love to know what you've been ‎automating!‎

That's all folks!

מק"ט יצרן # SC1629
MEM CARD MICROSD 64GB CLASS 10
Raspberry Pi
מק"ט יצרן # SC1148
HEATSINK ALUMINUM
Raspberry Pi
מק"ט יצרן # PIM699
NVME BASE FOR RASPBERRY PI 5
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.