Maker.io main logo

Getting Started with Raspberry Pi Pico

570

2023-11-16 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

What a time, eh? After an absolute whirlwind of a launch, Raspberry Pi Picos is starting to land through ‎people's letterboxes and a lot of folks who've not had much to do with microcontrollers before are ‎looking for a place to start figuring out what to do with them. Welcome! Now is the perfect time to get ‎onboard the microcontroller train - you're going to love it.‎

What is this guide?‎

In this guide, we're going to give a brief, beginner friendly primer on the Pico and show you the steps ‎necessary to get it set up and ready for programming with MicroPython. We'll also cover what you ‎need to do to be able to play with various Pimoroni add-on boards. We'll have more specific content ‎for individual boards in the future, but hopefully this guide will be just enough to get you started ‎experimenting with your Pico.‎

We're not going to go into huge detail about everything the Pico can do here - for a comprehensive, ‎beginner friendly guide with lots of fun experiments to do with physical hardware we'd recommend ‎the excellent Getting Started with MicroPython on the Raspberry Pi Pico book. If you're after technical ‎detail we'd suggest checking out the resources on the Raspberry Pi site, including the extensive Pico ‎datasheet. If you know how to program a microcontroller already you can find function references for ‎our boards and suchlike in our Pico GitHub repo.‎

raspberry_1

About Raspberry Pi Pico

Raspberry Pi Pico is Raspberry Pi's first microcontroller board, designed around their very own ‎microcontroller chip - the RP2040. A Pico is not a replacement or upgrade for a Raspberry Pi - they're ‎very different beasts! A Raspberry Pi is a Single Board Computer that runs Linux, to which you can ‎connect a monitor, keyboard and mouse and interact with via a terminal prompt or a graphical user ‎interface such as the Raspberry Pi OS desktop. You can run many different Linux applications on a ‎Raspberry Pi, and it has a ton of processing power and RAM.‎

While Raspberry Pi’s are champion multi-taskers, microcontrollers shine in projects where they have ‎one job and need to do it well. Because they're programmed from another computer and don't need ‎to run a full OS, they have greatly reduced power consumption compared to SBCs and are ideal for ‎powering from batteries. Programs on microcontrollers just start running once they're powered up, so ‎there's no boot up time, and you usually don't need to shut them down safely. Focusing on just one ‎thing means that microcontrollers are typically more stable and predictable, making them perfect for ‎using as the brains of projects that need to Just Work, like industrial machines, coffee makers or ‎emergency zombie defence turrets.‎

Interfacing with hardware is also more straightforward with microcontrollers, and Raspberry Pi Pico is ‎specifically geared towards physical computing (AKA connecting it to interesting stuff that lights up, ‎moves, or makes noise). Unlike a Pi, Pico has inbuilt Analog to Digital Convertors (ADCs) so you can ‎connect it to a wider range of sensors and inputs. It also has Programmable IOs (PIOs) which are used ‎behind the scenes in our libraries, outsourcing simple bits of programs to run in the background and ‎freeing up the majority of the Pico's CPU to concentrate on the trickier parts. If you're interested in ‎the possibilities of PIOs check out our Unicorn Pack page, where we describe how we managed to get ‎‎14 bits of resolution from the LED drivers on the Pico version (meaning improved rainbows!)‎

As of July 2022, you can also get a Pico W (aka Picow 🐄) which has wireless connectivity - exciting!‎

What you'll need

  • A Raspberry Pi Pico (or Pico W)‎

  • A USB cable - you'll need a microB USB cable to plug your Pico into your computer to be able to ‎program it. You may well have one already, from an old phone, a Pi Zero or a micro:bit but you'll need ‎it to be capable of transmitting data over USB as well as power. All the cables we sell are data capable

  • Header pins - to be able to plug your Pico into our Packs and Bases (or a breadboard) it will need to be ‎equipped with header pins. We'll cover how to solder them to your Pico later in this guide. You'll also ‎need soldering supplies - a soldering iron, solder, and tip cleaner. A breadboard is handy for keeping ‎your pins in place while you solder

  • A computer to program your Pico from (the software you'll need, Thonny, is free and available for ‎Raspberry Pi, PC, Mac, or Linux)

  • One (or more!) of our Pico addons - you can browse them all here

MicroPython or C/C++?‎

You can program Pico with MicroPython (a version of Python especially for microcontrollers) or the ‎C/C++ SDK (you might be familiar with C/C++ if you've had anything to do with Arduinos) - we have code examples and libraries for both! It's also possible to use CircuitPython (Adafruit's version of ‎MicroPython) on the Pico but Pimoroni boards may not currently be easily compatible if you go down ‎this route.‎

This guide is going to use MicroPython as it's super simple to get going with our custom firmware, and ‎you can use Thonny to program your Pico from a PC, Mac or even a Raspberry Pi.‎

Installing the custom firmware

To be able to use our Pico addons (or Breakout Garden breakouts) you'll need to download our ‎custom build of MicroPython which comes with all the drivers baked in. You can find pre-built ‎MicroPython images for Raspberry Pi Pico, Pico W and our other RP2040 boards on the releases page ‎of our pimoroni-pico Github repository - scroll down to the assets section of the most recent release ‎for a list of .uf2 files. For a Raspberry Pi Pico, you'll need to download the Pico-flavoured .uf2:‎

install_2

If you have a Pico W, be sure to download the Pico W specific image which has all the wireless stuff ‎built in.‎

To copy this file to your Pico, you'll need to put it into bootloader mode. To do this, hold down the ‎BOOTSEL button whilst plugging the USB cable into your computer - it should now show up as a drive ‎called RPI-RP2. Here's what it looks like in Windows:‎

file_3

Copy the downloaded .uf2 file across to this new drive. Your Pico will now reboot, and after a few ‎seconds it will be running pirate-brand MicroPython (you probably won't notice any difference, but it's ‎actually singing sea shanties very quietly to itself.)

Once you've done this your Pico won't show up as a drive anymore when you plug it in, you'll need to ‎use an interpreter to talk to it. We're using Thonny!‎

Installing Thonny

Thonny is a Python IDE (an Integrated Development Environment). It's the software you'll install on ‎your computer to program your Pico.‎

If you're programming your Pico from a Raspberry Pi running the desktop version of Raspberry Pi OS, ‎Thonny should be installed already. You may need to update it to the most recent version to get the ‎Pico specific options, you can do this by opening up a terminal (find it in the menus or hit Ctrl-Alt-T) and ‎typing.‎

Copy Code
sudo apt update && sudo apt upgrade -y

and pressing enter.‎

You can download Thonny in Windows, Mac, or Linux flavours here. Once it's installed, open it up!‎

download_4

You'll need have 'MicroPython (Raspberry Pi Pico)' selected as your Python interpreter - you can do ‎that by clicking on the box at the bottom right. Thonny might offer to install MicroPython for you, you ‎don't need to do this as you should already have our variant of MicroPython installed.‎

If you don't see a MicroPython prompt with three arrows like the one above, try clicking the red stop ‎button to interrupt any processes that are running.‎

COULDN'T FIND DEVICE AUTOMATICALLY?

‎If Thonny has problems automatically detecting your board, you can select your board manually by ‎clicking on 'MicroPython (Raspberry Pi Pico)' at the bottom right and clicking on 'Configure Interpreter'. ‎You can then select the correct board under 'Port' - our Pico showed up as COM46.‎

select_5

Using Thonny (Hello World and Blink)

With your Pico connected to your computer with the USB cable (no need to hold down the button this ‎time, you don't want to be in bootloader mode), click on the bottom 'Shell' box, so you get a flashing ‎cursor. By typing instructions into this box, you can give commands to your Pico directly, one command ‎at a time (this is called REPL or Read-Eval-Print Loop.)‎

Try typing

print("hello world")‎

and pressing enter. See how it parrots hello world right back at you? Your Pico is talking back to you via ‎the serial console, and it can tell you all sorts of useful things - error messages and anything you print ‎‎(such as sensor readings) will show up in this box. This can be very handy for debugging your code!‎

box_6

Of course, you will probably want to queue up more than one line of instructions to make up a ‎program- that's what the top box is for. Here's a basic program you can try to test out your Pico is ‎working properly, before soldering anything to it. You can either copy and paste it into Thonny or type ‎it in. If you're typing it in, make sure the bottom two lines have four spaces in front of them to indent ‎them (indents are used in Python to denote when code is part of a loop.)

Copy Code
import machine
import time

led = machine.Pin('LED', machine.Pin.OUT)

while True:
    led.toggle()
    time.sleep(2)

This program

  • imports the modules necessary to let your Pico interact with basic hardware and know about ‎the concept of time

  • gives the Pico's onboard LED a friendly name (led) so it's easy to refer to in code and sets it as ‎an OUTput

  • sets up a simple loop, which turns the onboard LED on or off, waits two seconds, and then ‎repeats

thonny_7

Once you're ready to transfer the program to your Pico, press the green 'run current script' button in ‎the top toolbar. You may be prompted to give it a name - you can use any name you like, but if you ‎save the file to your Pico as main.py it will run automatically when the Pico is connected to power, you ‎won't need to start it in Thonny. This is useful if you want to make a battery powered project that ‎won't be connected to a PC!‎

Note that when using MicroPython you won't be able to copy code that you've written to your Pico by ‎holding the button down to put it into bootloader mode and copying the file across - you'll always ‎need to transfer it using Thonny.‎

Soldering the headers

To plug in our addon boards or to plug your Pico into a breadboard, your Pico will need to have headers ‎soldered to it, with the pins sticking out of the back. Soldering headers is not hard with modern PCBs ‎and we'd encourage you to give it a go (but if you'd rather skip the soldering, we should have pre-‎soldered Picos available very shortly.)‎

Your headers might come pre-separated into two 20 pin lengths, or in one long length. If it's the latter, ‎you can separate them in to two lengths with side cutters (it's also possible to break them apart with ‎sturdy scissors, or even your thumbnail.)‎

You'll need to solder your headers so that the pins are sticking out of the back of the Pico, with the ‎long pins sticking out of the side with the labels and the soldering itself on the side with the button. ‎The pins should be at right angles to the Pico so that they can plug into things nicely. Using a ‎breadboard to hold the pins in place while you solder is a good way of making sure things remain ‎square while soldering, but you can also use a large blob of blu-tack or similar to hold things together ‎‎(or even a helping hand, if you're fancy.)

Poke the long ends of your two lengths of header into your breadboard, the same width apart as the ‎two rows of holes on your Pico.‎

headers_8

Place your Pico on top of the short ends with the button and the raspberry facing upwards.‎

headers_9

Make sure your workspace has adequate ventilation and consider wearing eye protection as solder ‎can sometimes behave unexpectedly. Once you're ready to start soldering, make sure to tin the end ‎of your iron - wait until it's up to temperature, melt a little bit of solder onto the tip and then clean off ‎the excess using your tip cleaner. You're ready to go!‎

tip_10

You'll want to position your soldering iron so it's applying heat evenly to the header pin and the pad on ‎the board, and then hold it in place for a few seconds. You can then feed a little bit of solder into the ‎place where the pad, the iron and the header pin meet - don't go overboard with the solder, you only ‎need a tiny bit, and you can always add more later. The solder should flow satisfyingly down the iron ‎and form a joint between the pad and the pin.‎

We'd suggest soldering one pin at each end, and then checking again to make sure the headers are ‎square. You can adjust them at this point if you need to, but you won't be able to later. Once you're ‎satisfied that everything is 90°, go ahead and solder the rest of the pins.‎

solder_11

When you're done, check your solder joints from all angles. A good joint should surround the pin on all ‎sides, and ideally should be shaped like a squat little cone. If you have joints that don't quite surround ‎the pin, heat up the solder again to reflow it, and hopefully it will fill the gaps. If it doesn't, you can add ‎a bit more solder (but try reflowing the solder on its own first). You'll also want to check for solder ‎joints that touch and bridge two pins - if you have any of these you can fix them by holding your iron to ‎the middle of the unwanted join for a second or two, which should make the two blobs separate.‎

remove_12

When removing your Pico from the breadboard we'd suggest holding on to the long edges and rocking ‎it gently from side to side whilst pulling upwards slowly - try to avoid putting too much pressure on the ‎pins at the ends as these are most liable to bend. If they do get bent you can bend them back, but ‎doing this too many times can cause metal fatigue.‎

Using Pimoroni Bases and Packs

Once your Pico has headers attached, it's fully equipped for plugging into one of our Packs or Bases. All ‎our Pico addons have markings that should make it obvious which way round you need to plug it in - ‎here is a upside down Display Pack, ready for plugging in to a Pico (the surfaces shown in the photo ‎below will be on the inside of the Pico+Pack sandwich.)‎

pack_13

Double check you've got the male and female headers lined up and push on the edges of the board to ‎join them together (if you're using a Display Pack, take care not to apply pressure to the screen.)‎

line_14

line_15

Pico landing areas on Bases are similarly marked, just match up the markings on the PCB to figure out ‎which way round the Pico should go.‎

marking_16

Removing Pimoroni Bases and Packs

If you need to remove your Pico from a base or pack, hold on to the long edges of the boards and ‎wiggle them gently from side to side whilst slowly pulling the boards away from each other. The ‎headers can grip on quite securely so it's best to hold onto the edges of the PCBs while you're ‎separating them, don't pull on the Pico's USB port or any of the components on your Pack or Base.‎

Running our examples

Once everything's assembled, we'd suggest checking out our example code - you can find the ‎MicroPython examples here. Once you've found the .py file for the demo you want to try, you can ‎copy and paste it into Thonny and run it in the same way as you ran the blink example (if you click on ‎the 'Raw' button it will strip out all the GitHub formatting, making it easier to copy and paste.)‎

running_17

Troubleshooting

My Pico doesn't show up as a drive when I connect it to my computer!‎

Unlike some other microcontroller boards, you'll need to hold down the BOOTSEL button whilst ‎plugging it in to your computer for it to show up as a drive. If you're doing that and it's still not showing ‎up, you might be using a power only USB cable - try a different one!‎

I get an ImportError in Thonny when I try and flash my code!‎

If you get an error that looks something like ImportError: no module named 'picographics' then you ‎probably have the vanilla Raspberry Pi MicroPython .uf2 installed instead of the Pimoroni one. Scroll ‎back up to the 'Installing the Custom Firmware' section for instructions on how to download and install ‎the correct firmware.‎

I get a 'Device is busy' error in Thonny when I try and flash my code!‎

If you get this error when you press the 'run current script' button to send code to your Pico, press the ‎red 'stop/restart backend' button first to stop it from doing whatever it's doing.‎

How do I factory reset/delete files from my Pico?‎

If you need to delete all your programs from your Pico's flash memory and start again from scratch, ‎you can do that by downloading this special .uf2 file and copying it to your Pico whilst it's in bootloader ‎mode. We found this useful when we had a malfunctioning main.py which was locking up the Pico to ‎the extent that it could longer communicate with Thonny. You'll need to copy the MicroPython image ‎across again afterwards.‎

That's all folks!‎

מק"ט יצרן # PIM546
PICO UNICORN PACK
Pimoroni Ltd
מק"ט יצרן # PIM543
PICO DISPLAY PACK
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.