Maker.io main logo

Raspberry Pi Pico and LED Arcade Button MIDI Controller

321

2025-06-13 | By Adafruit Industries

License: See Original Project 3D Printing Raspberry Pi MCU

Courtesy of Adafruit

Guide by Ruiz Brothers and Liz Clark

Overview

DIY MIDI Controller

Build your own CircuitPython powered MIDI controller! This "MIDI fighter"-like controller ‎features 16 arcade buttons with built-in LEDs, an OLED screen and joystick. Play drums, ‎synthesizers or anything MIDI related! All of the electronics are housed in a snap-fit 3D ‎printed case.‎

3d_printing_loop-thumb-hq

Buttons and LEDs

The Raspberry Pi Pico has plenty of GPIO for connecting 4x4 buttons. The AW9525 GPIO ‎expander / LED driver powers the LEDs and connects to the Raspberry Pi Pico over I2C.‎

The LEDs light up when the buttons are pressed and stay lit until released. Awesome!‎

buttons_1

Edit MIDI on the Fly

This MIDI controller's special sauce is the ability to change and save MIDI notes directly on ‎the device. This allows quick MIDI notes remapping. Perfect for crafting your own kits and ‎setups for performances.‎

3d_printing_oled-demo-loop

Intuitive UI/UX

The OLED screen shows the 16 buttons as little circles with numbers. The numbers are the ‎MIDI notes assigned to each button. Use the joystick to select a button and edit the MIDI ‎note. In edit mode, the button will blink the LED, letting you know it's been activated. While ‎in edit mode, the buttons can be pressed to compare MIDI notes.‎

intuitive_2

Kickstand Handle

Lunchbox vibes? Yes! The handle is 3d printed, print-in-place, with no support material. ‎Can you handle it? It also works great as a kickstand to prop up the case.‎

kickstand_3

box_4

Prerequisite Guides

Take a moment to walk through the following guides:‎

Parts from Adafruit

List of parts required for this build.‎

Hardware List

Screws, nuts, and standoffs used in this build.‎

Handle

  • ‎4x M3 x 10mm long screws‎

USB Extension Cable

  • ‎2x M3 x 10mm long screws‎

  • ‎2x M3 locknuts‎

OLED

  • ‎4x M2.5 x 12mm long screws‎

  • ‎4x M2.5 nuts‎

‎5-way navigation PCB0

  • ‎2x M3 x 4mm long screws‎

PCB Mount

  • ‎4x M3 x 12mm long FF standoffs‎

  • ‎4x M2.5 x 8mm long FF standoffs

  • ‎4x M2 x 6mm long FF standoffs‎

  • ‎8x M3 x 6mm long screws‎

  • ‎8x M2.5 x 4mm long screws‎

  • ‎8x M2 x 4mm long screws‎

Author Credits

CAD by Noe Ruiz and Code by Liz Clark.‎

Inspired by MIDI Fighter by DJTechTools

 

 

Installing CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify experimentation and ‎education on low-cost microcontrollers. It makes it easier than ever to get prototyping by ‎requiring no upfront desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython QuickStart

Follow this step-by-step to quickly get CircuitPython working on your board.‎

Download the latest version of CircuitPython for the Raspberry Pi Pico from ‎circuitpython.org

Click the link above and download the latest UF2 file.

Download and save it to your desktop (or wherever is handy).‎

click_5

Start with your Pico unplugged from USB. Hold down the BOOTSEL button, and while ‎continuing to hold it (don't let go!), plug the Pico into USB. Continue to hold the BOOTSEL ‎button until the RPI-RP2 drive appears!‎

If the drive does not appear, unplug your Pico, and go through the above process again.‎

A lot of people end up using charge-only USB cables and it is very frustrating! So, make ‎sure you have a USB cable you know is good for data sync.‎

start_6

You will see a new disk drive appear called RPI-RP2.‎

Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.‎

drive_7

drive_8

The RPI-RP2 drive will disappear, and a new disk drive called CIRCUITPY will appear.‎

That's it, you're done! :)‎

disappear_9

Flash Resetting UF2‎

If your Pico ever gets into a really weird state and doesn't even show up as a disk drive when ‎installing CircuitPython, try installing this 'nuke' UF2 which will do a 'deep clean' on your ‎Flash Memory. You will lose all the files on the board, but at least you'll be able to revive it! ‎After nuking, re-install CircuitPython

flash_nuke.uf2‎

Coding the Raspberry Pi Pico MIDI Controller

Installing the CircuitPython Library Bundle

We're constantly updating and improving our libraries, so we don't (at this time) ship our ‎CircuitPython boards with the full library bundle. Instead, you can find example code in the ‎guides for your board that depends on external libraries. Some of these libraries may be ‎available from us at Adafruit, some may be written by community members!‎

Either way, as you start to explore CircuitPython, you'll want to know how to get libraries on ‎board.‎

You can grab the latest Adafruit CircuitPython Bundle release by clicking the button below.‎

Click for the Latest Adafruit CircuitPython Library Bundle Release

Once you've finished setting up your Raspberry Pi Pico with CircuitPython, you can add the ‎libraries to the lib folder of the Pico's CIRCUITPY drive which should appear when the board ‎is plugged into your computer via USB. Copy these folders:‎

  • adafruit_bus_device

  • adafruit_display_shapes

  • adafruit_display_text

  • adafruit_midi

  • adafruit_register

And these files:‎

  • adafruit_aw9523.mpy

  • adafruit_ssd1327.mpy

  • simpleio.mpy

To the CIRCUITPY flash drive /lib directory (create the directory if it doesn't exist).‎

Then, you can click on the Download: Project Zip link in the window below to download the ‎code file.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 Liz Clark for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import time
import board
import i2cdisplaybus
import displayio
import terminalio
import adafruit_aw9523
import busio
import adafruit_ssd1327
import digitalio
from adafruit_display_text import label
from adafruit_display_shapes.circle import Circle
from adafruit_display_shapes.rect import Rect
import usb_midi
import adafruit_midi
from adafruit_midi.note_on          import NoteOn
from adafruit_midi.note_off         import NoteOff

displayio.release_displays()

# i2c setup, higher frequency for display refresh
i2c = busio.I2C(board.GP1, board.GP0, frequency=1000000)
#  i2c display setup
display_bus = i2cdisplaybus.I2CDisplayBus(i2c, device_address=0x3D)
#  i2c AW9523 GPIO expander setup
aw = adafruit_aw9523.AW9523(i2c)
#  MIDI setup as MIDI out device
midi = adafruit_midi.MIDI(midi_out=usb_midi.ports[1], out_channel=0)

# display dimensions
WIDTH = 128
HEIGHT = 128
#  display setup
display = adafruit_ssd1327.SSD1327(display_bus, width=WIDTH, height=HEIGHT, brightness=0.01)

#  main display group, shows default GUI menu
splash = displayio.Group()
#  group for circle icons
circle_group = displayio.Group()
#  group for text labels on circles
text_group = displayio.Group()

#  list of circle positions
spots = (
    (16, 16),
    (48, 16),
    (80, 16),
    (112, 16),
    (16, 48),
    (48, 48),
    (80, 48),
    (112, 48),
    (16, 80),
    (48, 80),
    (80, 80),
    (112, 80),
    (16, 112),
    (48, 112),
    (80, 112),
    (112, 112),
    )

#  creating the circles & pulling in positions from spots
for spot in spots:
    circle = Circle(x0=spot[0], y0=spot[1], r=14, fill=0x888888)
    # adding circles to their display group
    circle_group.append(circle)
#  square to show position on menu
rect = Rect(0, 0, 33, 33, fill=None, outline=0x00FF00, stroke=3)

splash.append(circle_group)
splash.append(rect)

#  strings and positions for the MIDI note text labels
texts = [
    {'num': "60", 'pos': (12, 16)},
    {'num': "61", 'pos': (44, 16)},
    {'num': "62", 'pos': (76, 16)},
    {'num': "63", 'pos': (108, 16)},
    {'num': "64", 'pos': (12, 48)},
    {'num': "65", 'pos': (44, 48)},
    {'num': "66", 'pos': (76, 48)},
    {'num': "67", 'pos': (108, 48)},
    {'num': "68", 'pos': (12, 80)},
    {'num': "69", 'pos': (44, 80)},
    {'num': "70", 'pos': (76, 80)},
    {'num': "71", 'pos': (108, 80)},
    {'num': "72", 'pos': (12, 112)},
    {'num': "73", 'pos': (44, 112)},
    {'num': "74", 'pos': (76, 112)},
    {'num': "75", 'pos': (108, 112)},
    ]
text_labels = []

for text in texts:
    text_area = label.Label(terminalio.FONT, text=text['num'], color=0xFFFFFF)
    text_area.x = text['pos'][0]
    text_area.y = text['pos'][1]
    text_labels.append(text_area)
    text_group.append(text_area)
splash.append(text_group)

#  secondary display group, shows large circle when button is selected
big_splash = displayio.Group()
#  large circle to fill display
big_circle = Circle(x0=64, y0=64, r=62, fill=0x888888)
big_splash.append(big_circle)
#  large text to fill circle
big_text = label.Label(terminalio.FONT, text='   ', color=0xFFFFFF)
big_text.x = 43
big_text.y = 62
big_text.scale = 4
big_splash.append(big_text)

#  array for LEDs on AW9523
leds = []
led_pins = [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15]
#  setup to create the AW9523 outputs for LEDs
for led in led_pins:
    led_pin = aw.get_pin(led)
    led_pin.direction = digitalio.Direction.OUTPUT
    leds.append(led_pin)



#  button pins, all pins in order skipping GP15
note_pins = [board.GP7, board.GP8, board.GP9, board.GP10, board.GP11,
             board.GP12, board.GP13, board.GP14, board.GP16, board.GP17,
             board.GP18, board.GP19, board.GP20, board.GP21, board.GP22, board.GP26]

note_buttons = []

for pin in note_pins:
    note_pin = digitalio.DigitalInOut(pin)
    note_pin.direction = digitalio.Direction.INPUT
    note_pin.pull = digitalio.Pull.UP
    note_buttons.append(note_pin)

#  note states
note0_pressed = False
note1_pressed = False
note2_pressed = False
note3_pressed = False
note4_pressed = False
note5_pressed = False
note6_pressed = False
note7_pressed = False
note8_pressed = False
note9_pressed = False
note10_pressed = False
note11_pressed = False
note12_pressed = False
note13_pressed = False
note14_pressed = False
note15_pressed = False
#  array of note states
note_states = [note0_pressed, note1_pressed, note2_pressed, note3_pressed,
               note4_pressed, note5_pressed, note6_pressed, note7_pressed,
               note8_pressed, note9_pressed, note10_pressed, note11_pressed,
               note12_pressed, note13_pressed, note14_pressed, note15_pressed]
#  pins for 5-way switch
select = digitalio.DigitalInOut(board.GP6)
up = digitalio.DigitalInOut(board.GP5)
down = digitalio.DigitalInOut(board.GP4)
left = digitalio.DigitalInOut(board.GP3)
right = digitalio.DigitalInOut(board.GP2)
#  array for 5-way switch
joystick = [select, up, down, left, right]

for joy in joystick:
    joy.direction = digitalio.Direction.INPUT
    joy.pull = digitalio.Pull.UP
#  states for 5-way switch
select_state = None
up_state = None
down_state = None
left_state = None
right_state = None
midi_state = None

#  coordinates for navigating main GUI
select_x = [0, 32, 64, 96]
select_y = [0, 32, 64, 96]

#  y coordinate for 5-way switch navigation
y_pos = 0
#  x coordinate for 5-way switch navigation
x_pos = 0
sub_state = False
#  default midi number
midi_num = 60
#  default MIDI button
button_num = 0
#  default MIDI button position
button_pos = 0
#  check for blinking LED
led_check = None
#  time.monotonic() device
clock = time.monotonic()

#  coordinates for tracking location of 5-way switch
up_scroll = 0
down_scroll = 0
left_scroll = 0
right_scroll = 0
switch_coordinates = [(0, 0), (1, 0), (2, 0), (3, 0),
                      (0, 1), (1, 1), (2, 1), (3, 1),
                      (0, 2), (1, 2), (2, 2), (3, 2),
                      (0, 3), (1, 3), (2, 3), (3, 3)]

#  array of default MIDI notes
midi_notes = [60, 61, 62, 63, 64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75]

#  show main display GUI
display.root_group = splash

while True:

    #  debouncing for 5-way switch positions
    if up.value and up_state == "pressed":
        print("Button pressed.")
        up_state = None
    if down.value and down_state == "pressed":
        print("Button pressed.")
        down_state = None
    if left.value and left_state == "pressed":
        print("Button pressed.")
        left_state = None
    if right.value and right_state == "pressed":
        print("Button pressed.")
        right_state = None
    if select.value and select_state == "pressed":
        print("Button pressed.")
        select_state = None

    #  MIDI input
    for i in range(16):
        buttons = note_buttons[i]
        #  if button is pressed...
        if not buttons.value and note_states[i] is False:
            #  send the MIDI note and light up the LED
            midi.send(NoteOn(midi_notes[i], 120))
            note_states[i] = True
            leds[i].value = True
        #  if the button is released...
        if buttons.value and note_states[i] is True:
            #  stop sending the MIDI note and turn off the LED
            midi.send(NoteOff(midi_notes[i], 120))
            note_states[i] = False
            leds[i].value = False

    #  if we're on the main GUI page
    if not sub_state:
        #  if you press up on the 5-way switch...
        if not up.value and up_state is None:
            up_state = "pressed"
            #  track the switch's position
            up_scroll -= 1
            if up_scroll < 0:
                up_scroll = 3
            y_pos = up_scroll
            down_scroll = up_scroll
        #  if you press down on the 5-way switch...
        if not down.value and down_state is None:
            down_state = "pressed"
            #  track the switch's position
            down_scroll += 1
            if down_scroll > 3:
                down_scroll = 0
            y_pos = down_scroll
            up_scroll = down_scroll
        #  if you press left on the 5-way switch...
        if not left.value and left_state is None:
            # print("scroll", down_scroll)
            left_state = "pressed"
            #  track the switch's position
            left_scroll -= 1
            if left_scroll < 0:
                left_scroll = 3
            x_pos = left_scroll
            right_scroll = left_scroll
        #  if you press right on the 5-way switch...
        if not right.value and right_state is None:
            # print("scroll", down_scroll)
            right_state = "pressed"
            #  track the switch's position
            right_scroll += 1
            if right_scroll > 3:
                right_scroll = 0
            x_pos = right_scroll
            left_scroll = right_scroll

        #  update square's position on the GUI
        rect.y = select_y[y_pos]
        rect.x = select_x[x_pos]

        #  update the currently highlighted button on the GUI
        for coords in switch_coordinates:
            if x_pos == coords[0] and y_pos == coords[1]:
                button_pos = switch_coordinates.index(coords)
                #  print(button_pos)
        button_num = text_labels[button_pos].text

        #  if you press select on the 5-way switch...
        if not select.value and select_state is None:
            select_state = "pressed"
            #  grab the selected button's MIDI note
            midi_num = int(button_num)
            #  change into the secondary GUI menu
            sub_state = True

    #  if an arcade button is selected to change the MIDI note...
    if sub_state:
        #  display the secondary GUI menu
        display.root_group = big_splash
        #  display the selected button's MIDI note
        big_text.text = str(midi_num)

        #  blink the selected button's LED without pausing the loop
        if (time.monotonic() > (clock + 1)) and led_check is None:
            leds[button_pos].value = True
            led_check = True
            clock = time.monotonic()
        if (time.monotonic() > (clock + 1)) and led_check is True:
            leds[button_pos].value = False
            led_check = None
            clock = time.monotonic()

        #  blocks the MIDI number from being set above 128
        if midi_num >= 128:
            midi_num = 128
        #  blocks the MIDI number from being set below 0
        if midi_num <= 0:
            midi_num = 0

        #  if you press right on the 5-way switch...
        if not right.value and right_state is None:
            #  increase the MIDI number
            midi_num += 1
            right_state = "pressed"
        #  if you press up on the 5-way switch...
        if not up.value and up_state is None:
            #  increase the MIDI number
            midi_num += 1
            up_state = "pressed"
        #  if you press left on the 5-way switch...
        if not left.value and left_state is None:
            #  decrease the MIDI number
            midi_num -= 1
            left_state = "pressed"
        #  if you press down on the 5-way switch...
        if not down.value and down_state is None:
            #  decrease the MIDI number
            midi_num -= 1
            down_state = "pressed"

        #  update arcade button's MIDI note
        #  allows you to check note while you're adjusting it
        midi_notes[button_pos] = midi_num

        #  if you press select on the 5-way switch...
        if not select.value and select_state is None:
            select_state = "pressed"
            #  change back to main menu mode
            sub_state = False
            #  update new MIDI number text label
            text_labels[button_pos].text = str(midi_num)
            #  show main GUI display
            display.root_group = splash
            #  turn off blinking LED
            leds[button_pos].value = False

View on GitHub

Review

Make sure you've followed these steps:‎

  • Loaded all the required library files and directories into the CIRCUITPY /lib directory

  • Copied code.py to the main (root) directory of the CIRCUITPY drive

Your Raspberry Pi Pico CIRCUITPY drive should look like this after you load the libraries ‎and code.py file:‎

review_10

CircuitPython Code Walkthrough

Import the Libraries

First, the CircuitPython libraries are imported.‎

Download File

Copy Code
import time
import board
import displayio
import i2cdisplaybus
import terminalio
import adafruit_aw9523
import busio
import adafruit_ssd1327
import digitalio
from adafruit_display_text import label
from adafruit_display_shapes.circle import Circle
from adafruit_display_shapes.rect import Rect
import usb_midi
import adafruit_midi
from adafruit_midi.note_on          import NoteOn
from adafruit_midi.note_off         import NoteOff

I2C and MIDI Setup

I2C is setup to use the Pico's GP0 and GP1 pins. You have two I2C devices in this project: ‎the Grayscale 1.5" 128x128 OLED Display and the AW9523 GPIO Expander and LED Driver. ‎

midi is also setup to act as a USB MIDI output device. midi_out sends notes out from the ‎device.‎

Download File

Copy Code
# i2c setup, higher frequency for display refresh
i2c = busio.I2C(board.GP1, board.GP0, frequency=1000000)
#  i2c display setup
display_bus = i2cdisplaybus.I2CDisplayBus(i2c, device_address=0x3D)
#  i2c AW9523 GPIO expander setup
aw = adafruit_aw9523.AW9523(i2c)
#  MIDI setup as MIDI out device
midi = adafruit_midi.MIDI(midi_out=usb_midi.ports[1], out_channel=0)

‎Display Setup

This project utilizes a graphical user interface (GUI) to let you change the MIDI note ‎numbers assigned to each of the arcade buttons. Each button is represented on the display ‎as a circle. The code uses the Circle object from the adafruit_display_shapes library to ‎easily draw circles on the display without having to import a bitmap.‎

spots hold the list of coordinates for each of the circles and the for statement creates each ‎circle and assigns them to the correct coordinate.‎

A rectangle is also created using the Rect object from the adafruit_display_shapes library. ‎This rectangle is used to highlight the currently selected circle on the display.‎

‎Download File

Copy Code
# display dimensions
WIDTH = 128
HEIGHT = 128
#  display setup
display = adafruit_ssd1327.SSD1327(display_bus, width=WIDTH, height=HEIGHT, brightness = 0.01)

#  main display group, shows default GUI menu
splash = displayio.Group()
#  group for circle icons
circle_group = displayio.Group()
#  group for text labels on circles
text_group = displayio.Group()

#  list of circle positions
spots = (
    (16, 16),
    (48, 16),
    (80, 16),
    (112, 16),
    (16, 48),
    (48, 48),
    (80, 48),
    (112, 48),
    (16, 80),
    (48, 80),
    (80, 80),
    (112, 80),
    (16, 112),
    (48, 112),
    (80, 112),
    (112, 112),
    )

#  creating the circles & pulling in positions from spots
for spot in spots:
    circle = Circle(x0=spot[0], y0=spot[1], r=14, fill=0x888888)
	#  adding circles to their display group
    circle_group.append(circle)
#  square to show position on menu
rect = Rect(0, 0, 33, 33, fill=None, outline=0x00FF00, stroke = 3)

splash.append(circle_group)
splash.append(rect)

‎MIDI Note Labels

Each circle has text that shows the currently assigned MIDI note number for each arcade ‎button. This information is stored in texts along with the coordinates for each string's ‎location. The for statement creates each text object, pulling this information from texts, and ‎stores them in the text_labels array.‎

Download File

Copy Code
#  strings and positions for the MIDI note text labels
texts = [
    {'num': "60", 'pos': (12, 16)},
    {'num': "61", 'pos': (44, 16)},
    {'num': "62", 'pos': (76, 16)},
    {'num': "63", 'pos': (108, 16)},
    {'num': "64", 'pos': (12, 48)},
    {'num': "65", 'pos': (44, 48)},
    {'num': "66", 'pos': (76, 48)},
    {'num': "67", 'pos': (108, 48)},
    {'num': "68", 'pos': (12, 80)},
    {'num': "69", 'pos': (44, 80)},
    {'num': "70", 'pos': (76, 80)},
    {'num': "71", 'pos': (108, 80)},
    {'num': "72", 'pos': (12, 112)},
    {'num': "73", 'pos': (44, 112)},
    {'num': "74", 'pos': (76, 112)},
    {'num': "75", 'pos': (108, 112)},
    ]
text_labels = []

for text in texts:
    text_area = label.Label(terminalio.FONT, text=text['num'], color=0xFFFFFF)
    text_area.x = text['pos'][0]
    text_area.y = text['pos'][1]
    text_labels.append(text_area)
    text_group.append(text_area)
splash.append(text_group)

‎Secondary GUI Menu

In addition to the main GUI, there is a secondary GUI. When you select an arcade button's ‎MIDI note to edit, the display shows a large circle with large text showing the MIDI note ‎number that you're editing. This secondary GUI is stored in big_splash.‎

‎Download File

Copy Code
#  secondary display group, shows large circle when button is selected
big_splash = displayio.Group()
#  large circle to fill display
big_circle = Circle(x0=64, y0=64, r=62, fill=0x888888)
big_splash.append(big_circle)
#  large text to fill circle
big_text = label.Label(terminalio.FONT, text='   ', color=0xFFFFFF)
big_text.x = 43
big_text.y = 62
big_text.scale = 4
big_splash.append(big_text)

LEDs with the AW9523‎

The arcade button's LEDs are controlled with the AW9523 GPIO expander. The I/O of the ‎AW9523 is accessed with aw.get_pin(pin_number). The pin numbers are stored in ‎the led_pins array and the for statement sets up the pins to be outputs.‎

‎Download File

Copy Code
#  array for LEDs on AW9523
leds = []
led_pins = [0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15]
#  setup to create the AW9523 outputs for LEDs
for led in led_pins:
    led_pin = aw.get_pin(led)
    led_pin.direction = digitalio.Direction.OUTPUT
    leds.append(led_pin)

Arcade Button Pins

The pins used for the arcade buttons are stored in the note_pins array. They are setup to be ‎digital inputs in the for statement and are then stored in the note_buttons array. ‎

Each arcade button has a state setup for debouncing. These states are stored in ‎the note_states array.‎

Download File

Copy Code
#  button pins, all pins in order skipping GP15
note_pins = [board.GP7, board.GP8, board.GP9, board.GP10, board.GP11,
             board.GP12, board.GP13, board.GP14, board.GP16, board.GP17,
             board.GP18, board.GP19, board.GP20, board.GP21, board.GP22, board.GP26]

note_buttons = []

for pin in note_pins:
    note_pin = digitalio.DigitalInOut(pin)
    note_pin.direction = digitalio.Direction.INPUT
    note_pin.pull = digitalio.Pull.UP
    note_buttons.append(note_pin)

#  note states
note0_pressed = False
note1_pressed = False
note2_pressed = False
note3_pressed = False
note4_pressed = False
note5_pressed = False
note6_pressed = False
note7_pressed = False
note8_pressed = False
note9_pressed = False
note10_pressed = False
note11_pressed = False
note12_pressed = False
note13_pressed = False
note14_pressed = False
note15_pressed = False
#  array of note states
note_states = [note0_pressed, note1_pressed, note2_pressed, note3_pressed,
               note4_pressed, note5_pressed, note6_pressed, note7_pressed,
               note8_pressed, note9_pressed, note10_pressed, note11_pressed,
               note12_pressed, note13_pressed, note14_pressed, note15_pressed]

‎‎5-Way Navigation Switch

The GUI is navigated with a 5-way switch. This allows you to move in all directions around ‎the screen and select the arcade button that you want to edit. The digital pins for the 5-way ‎switch are stored in the joystick array and are setup as inputs in the for statement.‎

Download File

Copy Code
#  pins for 5-way switch
select = digitalio.DigitalInOut(board.GP6)
up = digitalio.DigitalInOut(board.GP5)
down = digitalio.DigitalInOut(board.GP4)
left = digitalio.DigitalInOut(board.GP3)
right = digitalio.DigitalInOut(board.GP2)
#  array for 5-way switch
joystick = [select, up, down, left, right]

for joy in joystick:
    joy.direction = digitalio.Direction.INPUT
    joy.pull = digitalio.Pull.UP

State Machines

There are a few state machines used in the code. Each pin for the 5-way switch has a state ‎for debouncing. The other states' functionality is commented below.‎

Download File

Copy Code
#  states for 5-way switch
select_state = None
up_state = None
down_state = None
left_state = None
right_state = None
midi_state = None

#  coordinates for navigating main GUI
select_x = [0, 32, 64, 96]
select_y = [0, 32, 64, 96]

#  y coordinate for 5-way switch navigation
y_pos = 0
#  x coordinate for 5-way switch navigation
x_pos = 0
sub_state = False
#  default midi number
midi_num = 60
#  default MIDI button
button_num = 0
#  default MIDI button position
button_pos = 0
#  check for blinking LED
led_check = None
#  time.monotonic() device
clock = time.monotonic()

GUI Navigation Setup

The navigation for the GUI works by counting the number of times each directional input ‎from the 5-way switch is pressed. The combinations of these counts are stored in ‎the switch_coordinates array to act as x and y coordinates on the GUI. It's helpful to think of ‎the arcade buttons as a 4x4 grid.‎

Download File

Copy Code
#  coordinates for tracking location of 5-way switch
up_scroll = 0
down_scroll = 0
left_scroll = 0
right_scroll = 0
switch_coordinates = [(0, 0), (1, 0), (2, 0), (3, 0), (0, 1), (1, 1), (2, 1), (3, 1), (0, 2),
            (1, 2), (2, 2), (3, 2), (0, 3), (1, 3), (2, 3), (3, 3)]

MIDI Note Array

The midi_notes array holds the default MIDI notes that are assigned to the arcade buttons. ‎If you want to change the MIDI notes that are loaded after powering the MIDI Fighter, you'll ‎want to edit this array.‎

Download File

Copy Code
#  array of default MIDI notes
midi_notes = [60, 61, 62, 63, 64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75]

The Loop

Switch Debouncing

The loop begins by debouncing the five inputs of the 5-way switch.‎

Download File

Copy Code
while True:

    #  debouncing for 5-way switch positions
    if up.value and up_state == "pressed":
        print("Button pressed.")
        up_state = None
    if down.value and down_state == "pressed":
        print("Button pressed.")
        down_state = None
    if left.value and left_state == "pressed":
        print("Button pressed.")
        left_state = None
    if right.value and right_state == "pressed":
        print("Button pressed.")
        right_state = None
    if select.value and select_state == "pressed":
        print("Button pressed.")
        select_state = None

MIDI Input

The arcade buttons send their assigned MIDI note number out with a ‎MIDI NoteOn message when they are pressed. Additionally, when you press an arcade ‎button, its LED lights up with the AW9523. When the arcade button is released, ‎a NoteOff message is sent, and the LED is turned off.‎

Download File

Copy Code
#  MIDI input
    for i in range(16):
        buttons = note_buttons[i]
        #  if button is pressed...
        if not buttons.value and note_states[i] is False:
            #  send the MIDI note and light up the LED
            midi.send(NoteOn(midi_notes[i], 120))
            note_states[i] = True
            leds[i].value = True
        #  if the button is released...
        if buttons.value and note_states[i] is True:
            #  stop sending the MIDI note and turn off the LED
            midi.send(NoteOff(midi_notes[i], 120))
            note_states[i] = False
            leds[i].value = False

Main GUI Navigation

The main GUI is navigated using the 5-way switch. Every time you press up, down, left or ‎right, the values of up_scroll, down_scroll, left_scroll or right_scroll are updated with a ‎count between 0 and 3. These values are used as coordinates to track where you are on the ‎GUI. ‎

y_pos and x_pos also hold these values and are used as array indexes to update the ‎highlighting square's position on the GUI.‎

‎Download File

Copy Code
#  if we're on the main GUI page
    if not sub_state:
        #  if you press up on the 5-way switch...
        if not up.value and up_state is None:
            up_state = "pressed"
            #  track the switch's position
            up_scroll -= 1
            if up_scroll < 0:
                up_scroll = 3
            y_pos = up_scroll
            down_scroll = up_scroll
        #  if you press down on the 5-way switch...
        if not down.value and down_state is None:
            down_state = "pressed"
            #  track the switch's position
            down_scroll += 1
            if down_scroll > 3:
                down_scroll = 0
            y_pos = down_scroll
            up_scroll = down_scroll
        #  if you press left on the 5-way switch...
        if not left.value and left_state is None:
            # print("scroll", down_scroll)
            left_state = "pressed"
            #  track the switch's position
            left_scroll -= 1
            if left_scroll < 0:
                left_scroll = 3
            x_pos = left_scroll
            right_scroll = left_scroll
        #  if you press right on the 5-way switch...
        if not right.value and right_state is None:
            # print("scroll", down_scroll)
            right_state = "pressed"
            #  track the switch's position
            right_scroll += 1
            if right_scroll > 3:
                right_scroll = 0
            x_pos = right_scroll
            left_scroll = right_scroll

        #  update square's position on the GUI
        rect.y = select_y[y_pos]
        rect.x = select_x[x_pos]

Track the Button

In order to keep track of which button on the GUI is highlighted, the x_pos and y_pos values ‎are compared to the switch_coordinates array to track which button is highlighted on the ‎screen. This is how that button's value can then be affected in the secondary GUI.‎

button_num is used to track the MIDI note number for the currently selected button.‎

Download File

Copy Code
#  update the currently highlighted button on the GUI
        for coords in switch_coordinates:
            if x_pos == coords[0] and y_pos == coords[1]:
                button_pos = switch_coordinates.index(coords)
                #  print(button_pos)
        button_num = text_labels[button_pos].text

Selecting a Button to Edit

When you have navigated to your chosen arcade button's position, you can press select on ‎the 5-way switch to enter the editing mode for that button. midi_num grabs the highlighted ‎button's MIDI note number so that you'll be able to edit and update that number.‎

Download File

Copy Code
#  if you press select on the 5-way switch...
        if not select.value and select_state is None:
            select_state = "pressed"
            #  grab the selected button's MIDI note
            midi_num = int(button_num)
            #  change into the secondary GUI menu
            sub_state = True

Secondary GUI: Edit the Arcade Button's MIDI Note Number

When you enter the editing mode, the secondary GUI is displayed. Your selected button's ‎LED will also blink on and off until you exit this mode. The blinking is done ‎using time.monotonic() so that it doesn't interrupt anything else happening in the loop.‎

Download File

Copy Code
#  if an arcade button is selected to change the MIDI note...
    if sub_state:
        #  display the secondary GUI menu
        display.root_group = big_splash
        #  display the selected button's MIDI note
        big_text.text = midi_num

        #  blink the selected button's LED without pausing the loop
        if (time.monotonic() > (clock + 1)) and led_check is None:
            leds[button_pos].value = True
            led_check = True
            clock = time.monotonic()
        if (time.monotonic() > (clock + 1)) and led_check is True:
            leds[button_pos].value = False
            led_check = None
            clock = time.monotonic()

MIDI Note Number Range

A MIDI note range is setup so that you don't go below 0 or above 128.‎

Download File

Copy Code
#  blocks the MIDI number from being set above 128
        if midi_num >= 128:
            midi_num = 128
        #  blocks the MIDI number from being set below 0
        if midi_num <= 0:
            midi_num = 0

Adjusting the MIDI Note

The MIDI note number can be increased by pressing up or right with the 5-way switch and ‎decreased by pressing down or left with the 5-way switch. The value of midi_num is either ‎increased or decreased by 1 depending on the input.‎

Download File

Copy Code
#  if you press right on the 5-way switch...
        if not right.value and right_state is None:
            #  increase the MIDI number
            midi_num += 1
            right_state = "pressed"
        #  if you press up on the 5-way switch...
        if not up.value and up_state is None:
            #  increase the MIDI number
            midi_num += 1
            up_state = "pressed"
        #  if you press left on the 5-way switch...
        if not left.value and left_state is None:
            #  decrease the MIDI number
            midi_num -= 1
            left_state = "pressed"
        #  if you press down on the 5-way switch...
        if not down.value and down_state is None:
            #  decrease the MIDI number
            midi_num -= 1
            down_state = "pressed"

Update the MIDI Note

The value of the selected arcade button's MIDI note is adjusted in real time. This allows you ‎to play the note while you're adjusting to make sure it's the correct note.‎

‎Download File

Copy Code
#  update arcade button's MIDI note
        #  allows you to check note while you're adjusting it
        midi_notes[button_pos] = midi_num

Save the New MIDI Note

After deciding on your MIDI note, you can press select again on the 5-way switch to save ‎your choice. This updates the text label on the main GUI, stops the LED from blinking and ‎brings you back to the main GUI on the display.‎

Download File

Copy Code
#  if you press select on the 5-way switch...
        if not select.value and select_state is None:
            select_state = "pressed"
            #  change back to main menu mode
            sub_state = False
            #  update new MIDI number text label
            text_labels[button_pos].text = midi_num
            #  show main GUI display
            display.root_group = splash
            #  turn off blinking LED
            leds[button_pos].value = False

‎Circuit Diagram

diagram_11

The diagram below provides a visual reference for wiring of the components. This diagram ‎was created using the software package Fritzing.‎

Adafruit Library for Fritzing

Use Adafruit's Fritzing parts library to create circuit diagrams for your projects. Download ‎the library or just grab individual parts. Get the library and parts from GitHub - Adafruit ‎Fritzing Parts.‎

STEMMA QT Connections

The following components are connected via STEMMA QT cables.‎

  • Raspberry Pi Pico – 1.5" OLED‎

  • ‎1.5" OLED – AW9523 LED Driver

5-way navigation switch

The 5-way navigation switch is connected to the following pins on the Raspberry Pi Pico.‎

  • Ground – Ground

  • Select – GP6‎

  • Up – GP2‎

  • Down – GP3‎

  • Left – GP4‎

  • Right – GP5‎

Button Switches

The switches from the buttons are connected to the following pins on the Raspberry Pi Pico.‎

  • Button 1 – GP7‎

  • Button 2 – GP8‎

  • Button 3 – GP9‎

  • Button 4 – GP10‎

  • Button 5 – GP11‎

  • Button 6 – GP12‎

  • Button 7 – GP13‎

  • Button 8 – GP14‎

  • Button 9 – GP16‎

  • Button 10 – GP17‎

  • Button 11 – GP18‎

  • Button 12 – GP19‎

  • Button 13 – GP20‎

  • Button 14 – GP21‎

  • Button 15 – GP22‎

  • Button 16 – GP26‎

Button LEDs

The LEDs from the buttons are connected to the following pins on the AW9523 LED Driver.‎

  • Button 1 – Pin 0‎

  • Button 2 – Pin 1‎

  • Button 3 – Pin 2‎

  • Button 4 – Pin 3‎

  • Button 5 – Pin 4‎

  • Button 6 – Pin 5‎

  • Button 7 – Pin 6‎

  • Button 8 – Pin 7‎

  • Button 9 – Pin 8‎

  • Button 10 – Pin 9‎

  • Button 11 – Pin 10‎

  • Button 12 – Pin 11‎

  • Button 13 – Pin 12‎

  • Button 14 – Pin 13‎

  • Button 15 – Pin 14‎

  • Button 16 – Pin 15‎

3D Printing

CAD Files

STL files for 3D printing are oriented to print "as-is" on FDM style machines. Parts are ‎designed to 3D print without any support material. Original design source may be ‎downloaded using the links below.‎

files_12

CAD Parts List

List of the 3D printed parts.‎

  • case-top.stl

  • case-frame.stl

  • case-bottom.stl

  • case-handle.stl

  • PCB-mount.stl

  • ‎5way-switch-pcb.stl

  • window-print-blank.stl

  • window-printed-midi-logo.stl

  • case-bottom-window.stl

Opens in the web browser to preview 3D models. More download options available in the ‎preview page.‎

Fusion 360 Share Link

Includes a STEP and Fusion 360 Archive.‎

Download CAD Source

Grab just the STL files for 3D printing.‎

Download STL Files

Window Options

The top cover is designed to have a window. This allows you to peek through and see the ‎Raspberry Pi Pico. The window can be 3D printed using transparent filament.‎

Have fun with this! Add your own text, logo, or stickers / vinyl decals. Personalize it, make it ‎yours.‎

Optionally, the window can be made from acrylic using a laser cutter or CNC mill.‎

window_13

Install Window

The window features a lip to prevent it from being pressed all the way through the cut out in ‎the top cover.‎

The window is installed through the bottom side of the top cover. It should have a tight fit.‎

Optionally glue in place to permanently secure to the top cover.‎

install_14

install_15

Install Handle to Frame

Use the following hardware to secure the handle to the frame.‎

  • ‎4x M3 x 10mm screws‎

  • ‎4x M3 locknuts‎

hardware_16

Handle Kickstand

The handle features an angled surface for propping up the case. Reference the image for ‎the correct placement of the handle. Use the USB opening on the side of the frame as an ‎indicator for the correct orientation.‎

handle_17

Secure Handle to Frame

Insert the M3 screws through the mounting holes in the hinges. Then, insert the screws ‎through the holes on the side of the frame. Install and fasten the locknuts onto the screws. ‎Use pliers to tightly secure the screw and nuts.‎

secure_18

Install Bottom Cover to Frame

The bottom cover snap fits onto the frame. The bottom cover features snap fit clips that are ‎designed to lock onto the edges inside the frame.‎

Reference the image for the correct orientation.‎

cover_19

cover_20

 

Fusion 360 CAD Tutorial

Taking a look at designing a hinged handle that can be 3d printed in place with no supports. ‎The design features a handle that can rotate 180 degrees. This handle is a part of the ‎enclosure for a MIDI controller. Driven with user parameters, the handle can be customized ‎to fit any project.‎

PCB Mount Assembly

Hardware for PCB Mount

Use the following hardware for assembling the PCB mount.‎

  • ‎4x M3 x 12mm long FF standoffs‎

  • ‎4 x M2.5mm x 8mm long FF standoffs‎

  • ‎4x M2 x 6mm long FF standoffs‎

  • ‎8x M3 x 6mm screws‎

  • ‎8x M2 x 4mm screws‎

  • ‎8x M2.5 x 4mm screws‎

screws_21

Install M3 hardware

Insert M3 screws through the mounting holes on the outer perimeter of the PCB mount. ‎Fasten the M3 standoffs onto the thread of the screw. ‎

m3_22

Install M2 Hardware

Insert M2 screws through the mounting holes that are near the M3 standoffs. Fasten the M2 ‎standoffs onto the threads of the screws. ‎

m2_23

Install M2.5 Hardware

Flip the PCB over and insert the M2.5 screws through the remaining mounting holes. Fasten ‎the M2.5 standoffs onto the threads of the screws. The M2.5 standoffs should be facing the ‎opposite side. Reference the image for correct placement.‎

flip_24

Assembled PCB Mount

Double check the standoffs are tightly fastened and installed in the correct mounting holes. ‎Reference the images, click the thumbnail to enlarge.‎

mount_25

mount_26

Wiring the 5-Way Navigation Switch

Wires for 5-Way Nav Switch

Choose the method to switch you'd like to wire the 5-way navigation switch. Provided is an ‎STL to 3D print the PCB or you can optionally send the PCB to a fab service.‎

Use a 6-wire ribbon cable, 114mm long.‎

wiring_27

Download 5-Way Navigation Switch PCB files

Install 5-Way Switch to PCB

Line up the pins of the switch with the holes in the PCB. Fit the 5-way navigation switch onto ‎the PCB.‎

lineup_28

lineup_29

5-Way Navigation Switch Schematic

Reference the schematic to get the correct connections for the pins. ‎

The common ground and center pins are good indicators for wiring. Up, down, left and right ‎are subject to change depending on the switch’s orientation.‎

The full data sheet is available, and a PDF can be downloaded from here.‎

5way_30

Solder Wires to 5-Way Nav Switch PCB

If you're using the PCB, solder the pins of the switch to the PCB. Then, solder the 6-wires ‎from the ribbon cable to the breakout pins on the PCB.‎

If you're using the 3D printed PCB, solder the wires to the exposed pins from the bottom. Be ‎careful not to melt the plastic.‎

solder_31

Soldering 5-Way Switch to Pico

Get ready to solder the 6-wires from the navigation switch to the Raspberry Pi Pico.‎

solder_32

If using the 3D printed pcb, double check the wires are soldered to the correct pins of the 5-‎way switch.‎

Solder Wires to 5-Way Switch

Solder the 6-wires from the navigation switch to the bottom of the Raspberry Pi Pico PCB. ‎Reference the pins below.‎

  • Ground – Ground

  • Select – GP6‎

  • Up – GP5‎

  • Down – GP4‎

  • Left – GP3‎

  • Right – GP2‎

solder_33

Soldered 5-Way Switch

Double check all of the wires have been properly soldered.‎

solder_34

Wiring STEMMA for Pico

STEMMA Wire

Use the STEMMA QT JST SH-4 cable for the Raspberry Pi Pico. This will plug into the OLED ‎display.‎

Remove the male header pins by cutting them off leaving the cable about 150mm in length.‎

Use wire strippers to remove a bit of insulation from the tips of each wire. Tin the exposed ‎strands of wire by adding a bit of solder.‎

stemma_35

Solder STEMMA to Raspberry Pi Pico

Attach the four wires from the STEMMA cable to the bottom of the Raspberry Pi Pico.‎

  • Blue wire – GP0‎

  • Yellow Wire – GP1‎

  • Red Wire – 3V3‎

  • Black Wire – GND

stemma_36

Soldered Pico STEMMA cable

Double check the four wires have been properly soldered to the pins on the Raspberry Pi ‎Pico.‎

stemma_37

Install Buttons

Installing Buttons

Get the 16 buttons ready to panel mount to the top cover. Remove the hex nuts by ‎unscrewing them from the body of each button.‎

buttons_38

Panel Mount Buttons

Start by installing one button. Insert the body of the button through the hole. While holding ‎it in place, fasten the hex nut onto the button.‎

To make the wiring easier, ensure all sixteen buttons are orientated the same. This will help ‎keep the wiring tidy as well.‎

Tightly fasten the hex nuts to secure the buttons to the top cover.‎

panel_39

panel_40

Numbering Buttons for Wiring

Each button will need to wired to the Raspberry Pi Pico and LED Driver. The numbering of ‎the buttons is important and should be planned before wiring.‎

Take a moment to review the numbering scheme of the buttons. This will help you ensure ‎the buttons are soldered to the correct pins.‎

numbering_41

Installed Buttons

The first button starts from the top right. The numbering scheme appears reversed because ‎we'll be soldering from the back view of the top cover.‎

Reference the image for the assigned button numbers.‎

installed_42

Wiring Grounds

Ground Wires

All of the switches and LEDs from the buttons will share common ground. In order to do ‎this, we'll need to create several short wires.

Use silicone ribbon wire to create 32 short wires that are approximately 70mm(2.76in) in ‎length. ‎

Use wire strippers to remove a bit of insulation from both ends of each wire. Tin the ‎exposed wire with a bit of solder.‎

ground_43

Tinning Pins

Apply a bit of solder to all of the pins on each button. This will make attaching the wires to ‎the pins easier.‎

tinning_44

Be careful not to melt the buttons with the soldering iron!

First Ground Wires

Attach two wires to the ground pin of the first switch. Reference the markings on the ‎buttons (if they have them).‎

The pins inside the gray box are the pins for the switch.

The pins outside the gray box are the ‎pins for the LEDs.‎

first_45

Sharing Ground

Each ground connect will need to jump to the next button in the arrangement. Using ‎tweezers can help hold two wires in place while soldering.

sharing_46

Wiring Grounds

Starting with the first button from the top right, proceed to wire from right to left to complete ‎the first row of four buttons.‎

On the four button, jump to the next row with button #8 and proceed to jump from left to ‎right.‎

On the fifth button, jump to the next row with button #9 and proceed to share ground from ‎right to left.‎

On the twelfth button, jump to the last row with button #16. Proceed to share ground from ‎left to right. ‎

grounds_47

grounds_48

grounds_49

grounds_50

Button Switches Shared Ground

Take a moment to double check the wiring and ensure all of the solder joints are solid. ‎Lightly tug on the wires to check if they're secured.

check_51

LED and Switch Shared Ground

On button #13 in last row, connect the second ground wire to the ground pin on the LED. Proceed to share ground to all of the button LEDs.

led_52

Button LED Ground Wiring

Complete the last row, Button #13 to #16 and connect each going right to left.‎

Proceed to connect Button #16 to Button #12 going from left to right.‎

Proceed to connect Button #9 to Button #5 going from right to left.‎

Proceed to connect Button #8 to Button #4 going from left to right.‎

The last ground wire connects Button #2 to Button #1.‎

Once complete, take a moment to review all of the wires.‎

groundwiring_53

groundwiring_54

groundwiring_55

groundwiring_56

Wiring Button Switches

Wire Planning

Start planning to wire the switches from all sixteen buttons to the Raspberry Pi Pico. The ‎wires will be soldered to the bottom of the PCB.‎

Place the Raspberry Pi Pico over the opening in the top cover to reference how long the wires ‎will need to be in order to reach the PCB.‎

wire_57

Wires for Switches

Each wire will most likely have a different length of wire. To help keep them organized, use ‎heat shrink tubing, tape or similar to keep sets of wire bundled together.‎

Here I've created four sets of wires, each set having four wires.‎

wires_58

Wiring Buttons 1-4‎

Solder the wires to buttons 1-4.‎

buttons1-4_59

Wiring Buttons 5-8‎

Solder the next set of wires to Buttons 5-8‎

buttons5-8_60

Wiring Buttons 9-12‎

Solder the next set of wires to Buttons 9-12.‎

buttons9-12_61

Wiring Buttons 13-16‎

Solder the last set of wires to Buttons 13-16.‎

Once complete, take a moment to review each wire.‎

buttons13-16_62

Wiring Button LEDs

Wires for LEDs

Time to make wires for connecting the Button LEDs. Create four sets of wire, each set ‎containing four wires.

wires_63

Wiring LEDs 1-4‎

Proceed to wire up the LEDs in the first row.‎

wiring1-4_64

Wiring LEDs 5-8‎

Proceed to wire up the second row, Buttons 5-8.‎

wiring5-8_65

Wiring LEDs 9-12‎

Proceed to wire up the third row, buttons 9-12.‎

wiring9-12_66

Wiring LEDs 13-16‎

Proceed to wire up the last row, buttons 13-16.‎

Once complete, review.‎

wiring13-16_67

Wiring Button Switches to Pico

Wiring Button LEDs and Switches to Pico

Get ready to solder all of the wires to the bottom of the Raspberry Pi Pico PCB.‎

switches_68

Solder Button Switches 1-4‎

Use a PCB vise or third helping hands to keep the Raspberry Pi Pico PCB secured while ‎soldering.‎

Solder the switch wires from Button 1-4 to GP7-10.‎

  • Button 1 – GP7‎

  • Button 2 – GP8‎

  • Button 3 – GP9‎

  • Button 4 – GP10‎

switches_69

Solder Button Switches 5-8‎

Proceed to wire up the second row of button switches to the Raspberry Pi Pico.‎

  • Button 5 – GP11‎

  • Button 6 – GP12‎

  • Button 7 – GP13‎

  • Button 8 – GP14‎

switches_70

Do not use GP15 – It's used as the boot select button and should be avoided.‎

Solder Button Switches to 9-12‎

Proceed to wire up the third row of button switches to the Raspberry Pi Pico.‎

  • Button 9 – GP16‎

  • Button 10 – GP17‎

  • Button 11 – GP18‎

  • Button 12 – GP19‎

switches_71

Solder Button Switches 13-16

Proceed to wire up the last row of button switches to the Raspberry Pi Pico.‎

  • Button 13 – GP20‎

  • Button 14 – GP21‎

  • Button 15 – GP22‎

  • Button 16 – GP26‎

switches_72

Install OLED

Solder Ground to OLED

Secure the OLED to a panavise, PCB vise or third helping hands. Solder the remaining ground wire to the ground pin on the OLED breakout.

switches_73

Connect STEMMA Cables to OLED

Plug in the STEMMA QT cable from the Raspberry Pi Pico to the left port on the side of the ‎OLED.‎

Plug in the STEMMA QT / Qwiic JST SH 4-Pin Cable to the right port on the other side of the ‎OLED.‎

switches_74

Hardware for OLED

Use the following hardware to secure the OLED to the top cover.‎

  • ‎4x M2.5 x 12mm screws‎

  • ‎4x M2.5 hex nuts‎

switches_75

Install OLED to Top Cover

Place the OLED face down into the top cover. Line up the mounting tabs with the mounting ‎holes in the top cover.‎

Insert the screws through the holes in the top cover and push them through the mounting ‎holes on the OLED.‎

cover_76

Secure OLED

While holding screw in place, insert and fasten an M2.5 hex nut onto the thread of the ‎screw. Only finger tightly the hex nuts to secure the screen. Proceed to install the remaining ‎screws. ‎

secure_77

The OLED screen is very fragile so be gentle when tightening screws!‎

Install 5-Way Nav Switch

Install Rubber Nub for 5-Way Nav Switch

Before panel mounting the 5-way navigation switch, install the rubber nubbin for the ‎Joystick (if you'd like, it's optional). It is press fitted over the stem of the joystick and has a ‎snug fit. ‎

rubber_78

Screws for 5-Way Nav Switch

Install the 5-way navigation switch into the top cover. Line up the mounting tabs with the ‎built-in standoffs on the top cover. Use the following screws to secure the 5-way navigation ‎switch.‎

  • ‎2x M3 x 4mm screws‎

screws_79

Secure 5-Way Nav Switch

Insert and fasten the two M3 x 4mm screws through the mounting tabs on the PCBs.‎

fasten_80

Install PCB Mount

Installing PCB Mount

Get the PCB mount ready to secure the Raspberry Pi Pico. Use the following screws.‎

  • ‎4x M2 x 4mm long screws‎

securepico_81

Secure Pico to PCB Mount

Carefully place the Raspberry Pi Pico over the M2 standoffs that are secured to the PCB ‎mount. Use the 4x M2 x 4mm long screws to secure the Raspberry Pi Pico to the four M2 ‎standoffs.‎

carefully_82

Connect USB Extension Cable to Pico

Grab the USB extension cable and connect it to the microUSB port on the Raspberry Pi Pico. ‎It's important to connect these together before securing the PCB mount to the top cover.

extension_83

Screws for Securing PCB mount to Top Cover

Use the following screws to secure the PCB mount to the top cover.‎

  • ‎4x M3 x 4mm long screws‎

screws_84

Secure PCB Mount to Top Cover

Position the PCB mount in place and line up the M3 standoffs with the mounting holes in ‎the top cover.‎

While holding in place, insert and fasten the 4x M3x4mm long screws to secure the PCB ‎mount to the top cover.‎

position_85

Secured PCB Mount

Check the PCB mount is properly secured to the top cover.‎

secured_86

secured_87

Install and Wire LED Driver

Screws for LED Driver

Use the following hardware to secure the LED driver to the PCB mount.‎

  • ‎4x M2.5 x 4mm long screws‎

driver_88

Secure LED Driver to PCB Mount

Place the LED driver over the remaining M2.5 standoffs.‎

Insert and fasten 4x M2.5x4mm long screws to secure the LED driver to the PCB mount.‎

secure_89

Wire Button LEDs 1-4 to LED Driver‎

Get ready to solder the LED wires to the LED driver. Make the following connections.‎

  • Button 1 – Pin #0‎

  • Button 2 – Pin #1‎

  • Button 3 – Pin #2‎

  • Button 4 – Pin #3‎

wirebutton_90

Note: Be careful not to miss Pin 0 – It's on the other side of the board.‎

Wire Button LEDs 5-8 to LED Driver‎

Make the following connections.‎

  • Button 5 – Pin #4‎

  • Button 6 – Pin #5‎

  • Button 7 – Pin #6‎

  • Button 8 – Pin #7‎

wirebutton_91

Wire Button LEDs 9-12 to LED Driver‎

Make the following connections.‎

  • Button 9 – Pin #8‎

  • Button 10 – Pin #9‎

  • Button 11 – Pin #10‎

  • Button 12 – Pin #11‎

wirebutton_92

Pins #8-11 are on the other side of the board.‎

Wire Button LEDs 13-16 to LED Driver‎

Make the following connections

  • Button 13 – Pin #12‎

  • Button 14 – Pin #13‎

  • Button 15 – Pin #14‎

  • Button 16 – Pin #15‎

connections_93

Connect STEMMA Cable to LED Driver

Lastly, connect the STEMMA cable from the OLED to the STEMMA port on the LED driver.‎

It just plugs in, isn't STEMMA QT awesome?‎

connect_94

Wiring Complete

YES! Congratulations, you've completed the wiring. Take a moment to bask in the glory.‎

complete_95

Final Assembly

Secure USB Extension Cable

The USB extension cable is panel mounted to the side of the frame. Use the screws ‎included or use your own (mine are coated in black paint).‎

  • M3 x 10mm long screws

Hold the USB extension port in place with your desired orientation. Insert and fasten the two ‎M3 screws while holding the USB port in place.‎

The stock length of the USB extension cable is just the right length we need – No need to cut ‎or extend, yay!‎

length_96

length_97

Close Case

The top cover snap fits onto the frame. Bring the two together and line up the clips with the ‎edges of the frame. Firmly press them together to snap fit the case shut.‎

close_98

Final Build

And there you have it! Your DIY MIDI Controller is assembled and ready for jamming. ‎Congratulations!‎

final_99

Jam Out

With your Raspberry Pi Pico MIDI controller all assembled, you're ready to jam! You can use ‎it with any software that allows MIDI input. Most commonly, you'll use a MIDI controller ‎with music production software such as Reason, Garage Band, FL Studio, Ableton Live, ‎etc.‎

You could use the MIDI device for recording your own music with MIDI or for playing live. ‎With the MIDI mapping, you can create unique arrangements on the fly without having to go ‎back and forth between software and the device. In a live situation, the added control of the ‎quick mapping opens up a world of possibilities. ‎

 

מק"ט יצרן # 4886
STEMMA QT GPIO EXPANDER AW9523
Adafruit Industries LLC
מק"ט יצרן # 4741
GRAPHIC DISPLAY OLED - 1.5"
Adafruit Industries LLC
מק"ט יצרן # 3491
SWITCH PUSH SPST-NO WHT 10MA 5V
Adafruit Industries LLC
מק"ט יצרן # 4210
JST SH 4-PIN CABLE - QWIIC COMPA
Adafruit Industries LLC
מק"ט יצרן # 4697
BLACK RUBBER JOYSTICK NUBBIN CAP
Adafruit Industries LLC
מק"ט יצרן # 3258
CBL USB2.0 MCR B RCPT-MCR B PLUG
Adafruit Industries LLC
מק"ט יצרן # 3299
BLACK NYLON SCREW AND STAND-OFF
Adafruit Industries LLC
מק"ט יצרן # 3890
CBL RIBN 10COND FLAT BLACK 3.28'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.