Maker.io main logo

Lighting LED Nets with WLED and xLights

1,332

2025-04-14 | By Adafruit Industries

License: See Original Project Addressable LEDs Hand Tools LED Matrix Solder / Desoldering Wifi Wireless

Courtesy of Adafruit

Guide by Erin St Blaine

Overview

Add hundreds of lights to your home or yard with these fantastic Pebble Pixel Nets. Adafruit ‎carries them in a variety of sizes, from 1x1m to 1x6m large, and they are chainable and ‎expandable, so no vision is too big.‎

These nets use 12v power, which can be easily handled by the Adafruit Sparkle ‎Motion microcontroller. It has 4 powered LED outputs, a power manager so you can run 12v ‎or 5v lights, and an onboard I2S microphone, which makes sound-reactive projects a ‎snap. ‎

The build is fairly easy, with no soldering required (though adding connectors can make ‎your life easier). This gives you time to focus on making beautiful sequences and enjoying ‎your pretty lights.

lights_1

WLED and xLights

Both WLED and xLights are open-source control software for LEDs. The Sparkle Motion ‎board works great with both. What's the difference?‎

WLED is a fast and easy way to get your lights doing beautiful things. It's easy to install and ‎configure, and you can be up and running within just a few minutes. WLED's software lives ‎on the microcontroller and works over your local WiFi network to talk to each controller. It's ‎easy to sync your projects together and use the preset animations and customize them to a ‎certain extent. I use WLED when I want to "set it and forget it" -- the controller boots up ‎when I power it on and then the animations just run automatically.‎

xLights is a more advanced option, and its biggest strength is sequencing. This program is ‎used by industry professionals and also by homeowners who want a crazy mad holiday ‎display in their front yard, with animated trees, windows, roof lines, arches, and matrices. ‎xLights makes it possible to run animations across all your different lights at once. It's free ‎to download and use, and there are online communities where people share and sell their ‎favorite sequences. xLights really shines when it's showtime: sequence all your different ‎lights to a piece of music and impress the heck out of your neighbors.‎

To run xLights you first need to install and configure WLED, so work through that section ‎first.‎

Parts

These nets require 12v power. For just 1-2m of net, this 5a power supply is just fine. If you're ‎using the bigger nets or chaining multiple nets together, or if you're doing an outdoor ‎installation, look for a beefier power supply.‎

This net will also run on battery power. Our 8 x AA battery holder supplies 12v and will run a ‎‎1-2m net for several hours. It's insufficient for larger projects, but sometimes a few hours is ‎all you need.‎

Connectors & Wire

Using connectors allow you to remove your Sparkle Motion controller from your project, ‎which is especially helpful when it's a larger scale project that's hard to move. Adding 3-pin ‎JST connectors is a bit more work during setup but can save you a lot of time down the road. ‎They're pretty weatherproof and hold up to wind and rain. I like these color-coded ones.‎

Get some heat-shrink tubing too!‎

For a Large Install

Bigger (800+ pixel) installations will require thicker wire connections and more power. Here ‎are a couple suggestions to get you started.‎

Standard JST connectors won't work in this case: the wires inside those little connectors ‎just aren't rated to carry that much current. Solder your wires together or use a 12v rated ‎connector like these. ‎

Wiring Diagram

diagram_2

diagram_3

These nets are 20 pixels wide with 5mm spacing. A 1m net is a 20x20 square and contains ‎‎400 pixels.‎

The Sparkle Motion board has 4 outputs: 3 in the screw terminal and another using the pins ‎just to the left of it. WLED prefers no more than 800 pixels per output (though it will work ‎with more, just not as smoothly) and xLights sets a hard limit of 1000 pixels per output. ‎

Keep this in mind when you're setting up your project. For the larger nets with 1200-1800 ‎pixels, you may want to add a second data line that connects into the net after the first 800 ‎pixels, for best performance. ‎

It's also a good idea to connect another power line at the far end of the net -- the ‎manufacturers have broken out power injection wires every 800 pixels on the bigger nets to ‎make this easy. If you're getting flickering or voltage, drop across the pixels, try adding ‎another power injection point.‎

The Sparkle Motion is built to power LEDs, but for very large projects with larger power ‎draws, it's a good idea to run the power directly to the lights instead of pulling it all through ‎the board.‎

How many LEDs Can I Connect?‎

The Sparkle Motion board has four outputs for LED strips: 3 in the screw terminal and one ‎more using the GPIO pins next to the screw terminal. It has a "Classic" ESP32 chip ‎onboard.‎

Driving Pixels with WLED

From the WLED Knowledge base:‎

For perfect performance, it is recommended to use 512 LEDs/pin with 4 outputs for a total ‎of 2048 LEDs.

For very good performance, it is recommended to use 800 LEDs/pin with 4 outputs for a ‎total of 3200 LEDs.

For good performance, you can use 1000 LEDs/pin with 4 outputs for a total of 4000 LEDs.

For okay performance, you can use 1000 LEDs/pin with 5 outputs for a total of 5000 LEDs.

For okay performance, you can use 800 LEDs/pin with 6 outputs for a total of 4800 LEDs.

ESP32 can calculate about 65k-85k LEDs per second (that means 1000 LEDs @~70fps, ‎‎2000 LEDs @~35fps, 4000 LEDs @~18fps)

‎4 outputs seem to be the sweet spot.‎

How Do I Power It?‎

For Adafruit's 1x1 meter net, these power supplies will work great.‎

For larger projects (more than 800 pixels), or projects that will be placed outdoors, try this ‎power supply (or similar):‎

For wearable or portable projects, you can use this 8xAA battery pack for 12v pixels. But if ‎you're making a wearable project, you might also want to check out the Sparkle Motion ‎Mini board. It's not quite as powerful and won't drive 12v pixels but can power up to 4A at 5v ‎and that's plenty for most costume pieces. Check out our 5v Pebble Pixels to go along with ‎it.‎

Assembly - Small Projects

Adafruit LED nets have a couple different wires coming off them. Look for the wire labeled ‎‎"input". Each of the 3 wires has a label too! Handy.‎

I like to wire a 3 pin JST connector between the net and the Sparkle Motion board. This is not ‎necessary: it's totally possible to wire the net directly to the Sparkle Motion board's screw ‎terminal.‎

If you're not using JST connectors, then go ahead and insert the 3 input wires into the screw ‎terminal on the Sparkle Motion Board: 12v to +, DI to 19, and G to G. Otherwise, solder the ‎female side of your JST connector to the input wires on the net. I like to use red for +12v, ‎green for data, and black for G.‎

The 2-strand wire on the net is for power injection. The larger nets have this attached in the ‎middle to make your life easy. You can also inject power at the far end. A good rule of thumb ‎is to inject power every 800 pixels or so.‎

wires_4

assembly_5

Use a tiny precision flat head screwdriver to carefully and gently open the ports on the screw ‎terminal. These are pretty easy to break so be gentle. Look carefully at the openings as you ‎turn the screws. When you see a square opening appear, stop turning.‎

Strip about 1/8" of wire from the 3 net or connector wires and insert carefully into the screw ‎terminals. Gently tighten the screw until it's snug: about 5 turns -- it shouldn't turn freely, if it ‎does, you've got the wire in the wrong part of the hole so pull it out and try again.‎

terminal_6

terminal_7

The wires should not come out easily when you tug. But, as we know, these controllers get ‎tugged on all the time! After testing to be sure of my connections, I added a zip tie around ‎the back of the controller to create strain relief on the connectors. ‎

connections_8

connections_9

LED strips often come with these connectors already attached, but there seems to be no ‎standard for whether the factories attach the male or the female connector on the "in" end. ‎For my own peace of mind, I try to be consistent and always use the male side of the ‎connectors on the microcontrollers, and the female on the "in" end of my LED strip. Data is ‎flowing "out" from the microcontroller and "in" to the strip, so the male/female metaphor ‎makes good sense in this arrangement. ‎

There is also no standard as to which way the color coding is wired on these connectors. ‎Some have a red wire on the left side, some on the right side. Some have no color coding at ‎all.‎

Hooking your strips up "backwards" (accidentally connecting a red wire to a black ‎wire) can damage your board and your LEDs, so it's important to be really careful when ‎you're setting up your connectors.‎

Be as consistent as possible with color coding and throw away any connectors you've got in ‎the drawer that are wired "backwards" from the rest.

connect_10

Connect the net to the controller and plug the controller in with at 12v power supply. These ‎boards come pre-loaded with a rainbow animation on pin 19, so if your lights come on, ‎you've got it right and you're good to go.‎

Troubleshooting

No lights? Here are a few things to try:‎

  • Check your wire connections. These screw terminals can be tricky to manage, and ‎they break pretty easily. Try using a different set of holes if you think your ‎connections might be the problem

  • Get WLED installed and running on your microcontroller

  • Be sure you're connecting to the "input" end of the net and not the "output" end. ‎These nets are directional and will only work if you connect to "in"

  • If your lights are on but are super dim or flickering, you may have a powering issue. ‎Try power injection or try using a screw terminal to power the lights directly instead ‎of through the board

Assembly - Big Projects

For larger projects with more than 800 pixels or so, the wiring gets a little bit more ‎complicated. It's not a good idea to pull too much power through the Sparkle Motion board, ‎and bigger LED installations can draw a fair amount of power. ‎

You'll also want to start a new data line every 800 pixels or so if you're planning to run WLED ‎or xLights on your Sparkle Motion Board. ‎

Find the input end of your net. It should be labeled by the manufacturer. ‎

Solder a 3-pin JST connector to the 3 wires, and at the same time, splice in a beefy (16-18g) ‎power and ground wire. I'm using 16-gauge lamp cord here, but there are lots of options ‎available with different form factors.

solder_11

This higher current power supply is a bit too much for most of the standard JST connectors. ‎They use very skinny wire inside and can burn up pretty quickly.‎

For the very best power transfer, hard-wire the 16-gauge power wires to your power supply. If ‎you want a removable power supply, try using these 2-pin wire joints to connect the wires. ‎They can handle the 12v current.‎

current_12

Data Outputs

If you're running WLED or X-lights, these controllers work best at around 800-1000 pixels ‎per output. Adafruit 4-meter nets have 1600 lights. So, for these nets, for best performance, ‎it's a good idea to run a data line to the middle of the net and connect it up right after pixel ‎‎800. ‎

On the 4m net there's a power injection wire soldered on at this point, so it's easy enough to ‎find. It's the unbroken wire along the bottom that we want. Carefully separate it from the ‎other wires and cut it carefully in the middle. Solder a long wire to the "in" for the second ‎half of the net. ‎

I wove this wire and the power injection wire through the plastic connectors at the top of the ‎net to keep them from getting pulled or hanging down.‎

outputs_13

Connect the data wire and the two power injection wires to a female JST connector and then ‎to your Sparkle Motion board.‎

Splice the power wires coming from the power supply to the power injection lines as well. ‎This will work best if power is flowing directly from the power supply to the lights for each ‎power injection point.

splice_14

It's possible to use the 3rd and 4th input on the board to control more nets and lights. With ‎xLights or WLED you can also sync multiple controllers together, so expansion is pretty ‎easy. ‎

WLED Setup

This section will show how to install and set up WLED on your Sparkle Motion board and ‎set up a 2-dimensional matrix so you can run mapped, 2D animations on your net.‎

The Sparkle Motion board has a lot more features we're not covering in this guide. It has an ‎onboard I2S microphone, for instant audio-reactive projects. It has an IR sensor so anyone ‎can control your project with a simple infrared remote. There are a lot of settings and ‎features that can really make your project shine.‎

Check out the Sparkle Motion Guide for information on how to use these features and ‎more.‎

guide_15

Adafruit Sparkle Motion

By Erin St Blaine

WLED Setup

View Guide

config_16

WLED Software

Board Choices

WLED runs on several different boards in Adafruit's collection. There are different benefits ‎to each, but the installation process is largely the same. This page contains instructions for ‎multiple boards -- be sure to use the pinouts and installation instructions for the one you're ‎using.

Sparkle Motion

This is our flagship ESP32 board, designed with WLED and Xlights in mind. It has 4 outputs ‎and is set up to drive either 5v, 12v or 24v pixels. It's a workhorse of a board and for larger ‎projects it's the clear winner. It has an onboard microphone for instant sound-reactive ‎support, and an IR sensor built in, to make it easy to control your project with an infrared ‎remote. It also has a couple stemma ports so you can add your own sensors or peripherals.‎

Sparkle Motion Mini

The Sparkle Motion Mini is a smaller version of the Sparkle Motion board. It has two LED ‎outputs, a microphone, and two stemma ports that make it easy to add an IR sensor or ‎other peripherals. It's got an onboard NeoPixel and a small footprint, making it perfect for ‎wearables or smaller projects. It will power a whole lot of pixels through the onboard USB ‎port: it's safe to draw up to 4A through this port, giving you plenty of power for most ‎wearable projects.‎

At this time, the Sparkle Motion Mini works best with WLED 0.15.1 -- the extra GPIO for ‎the microphone pins are not supported in WLED 0.15.0. This should be fixed with the ‎release of version 16.‎

To get mic support now, the following combined .bin file can be used. Get it by downloading ‎this zip file:‎

esp32_bootloader_v4_WLED_0.16.0-alpha_ESP32.zip

To install, extract the .bin file from the zip and then follow the same ESB Web Flasher ‎process used for installing CircuitPython. At the "Programming the Board" step, choose ‎the .bin file and leave offset as 0x0.‎

QT Py Pico ESP32‎

The QT Py Pico is small and affordable, so usually my go-to for smaller costumes or ‎wearables. It also has a range of BFF add-on boards that add functionality. Here's a guide ‎with more QT Py info. The QT Py will drive up to around 30 pixels through the onboard USB ‎port, so if you have more LEDs than that you may want to consider the Sparkle Motion Mini ‎instead, or you can power the board through the +5v pin.‎

Note: WLED works on the QT Py Pico but NOT on the S2 or S3 versions, at the time of writing.‎

Feather Huzzah ESP32 ‎

The Feather Huzzah ESP32 the top of the line. It's a great choice for projects where you want ‎to add sensors, interaction, or drive a whole lot of LEDs. It's the most reliable as well -- I've ‎run these for two months straight with no power cycling and they just keep on truckin. ‎Adafruit has a very wide selection of Feather Wing boards that connect to the Feather ‎microcontroller line. The sky is the limit with these boards.‎

It also comes in a version with a high-powered WiFi range extender! If you're trying to sync ‎multiple instances across distance, check this one out. Feather Huzzah ESP32 V2 w.FL ‎Antenna.

Feather Huzzah ESP8266

The Feather Huzzah ESP8266 will run WLED as well but won't drive as many pixels: the ‎ESP32 limit on WLED is around 1000 pixels per input, but the ESP8266 tops out at around ‎‎500. It's about $5 cheaper though, so for smaller projects it's a great way to save a little ‎money and still have access to all the Featherwing options in the Adafruit store.‎

Driver Update

Some versions of our controllers have a new serial chip which needs a driver installed ‎before we can install WLED. Head over to our How to Install Drivers for WCH USB to Serial ‎Chips tutorial and download and install the new driver.‎

If you have an older QT Py with CP2102 USB-to-Serial bridge, use SiLabs’ driver instead.‎

Install WLED

These next steps require a Web Serial-compatible browser. As of this writing, that ‎means Google Chrome, Microsoft Edge or Opera “desktop” browsers. Other browsers ‎‎(Safari, Firefox, Explorer and anything mobile) won’t work.‎

Visit https://install.wled.me/‎

Plug your microcontroller into your computer with a known good USB cable. Click "Install" ‎and select the port for your board.‎

Depending on the USB-to-serial bridge chip on the board, you might see one or two serial ‎ports. On Mac, for instance, there might be both ‎‎“/dev/cu.usbmodem[number]” and “/dev/cu.wchusbserial[number]”. Use the ‎‎“wchusbserial” one.‎

install_17

After successful installation, enter your WiFi network name and password when prompted. ‎This must be a 2.4 GHz WiFi network; ESP32 does not support 5 GHz networks. If it can’t ‎connect, then as a fallback WLED will create its own 2.4 GHz WiFi access point.‎

after_18

If you don't see the "Connect to Wi-Fi" prompt, you'll need to set up your WiFi network using ‎AP (access point) mode. Open up your WiFi settings and look for a WiFi network ‎called WLED-AP. Connect to this network using the default password wled1234. The WLED ‎interface will pop up in its own browser.‎

From here, go into Config/Wifi Settings and enter your WiFi credentials near the top. Give ‎your project a name in the mDNS field a little further down the page. Now you can type in ‎‎"projectname.local" (where "projectname" is your mDNS name) into any web browser on ‎the same wifi network to access your microcontroller.‎

You can also scan the QR code below to open access point mode. ‎

For more help and troubleshooting tips visit the Getting Started page on the WLED ‎knowledge base.‎

page_19

page_20

scan_21

Setup & Preferences

WiFi Setup

Head to the WiFi Setup screen under Config and create a good URL so you can control your ‎project from any web-enabled device. Call it something you'll remember, that's easy to type ‎into any web browser on your WiFi network in order to connect to your project.‎

In Safari or Chrome on your phone or computer, type in this web address to access the ‎WLED interface: http://projectname.local (where "projectname" is whatever you put into ‎this field).‎

Check out the Additional Settings page for more info on accessing your project. WLED has ‎an "access point mode" that doesn't require a WiFi network for when you're out on the go. ‎It's also helpful to download one of the WLED apps to help manage and organize your ‎projects.‎

setup_22

setup_23

LED Preferences

Next, head to the LED Preferences tab under the Config menu.‎

Scroll down to Hardware Setup. Put your total number of LEDs into the "Length" field and ‎change GPIO to the pin number associated with the pin you soldered to. Check the pinout ‎diagram for the board you're using (it's the number in yellow).‎

preferences_24

Use It

use_25

Now you can use any computer or handheld device to control your LEDs. ‎

Make sure your device is on the same WiFi network as your board. Navigate to your custom ‎URL (projectname.local/ ) in a web browser. You'll see a color picker above a whole bunch of ‎color palette choices.‎

Choose a color, choose an effect, and watch your lights animate and glow!‎

Save your favorite combinations as presets, create playlists, control the speed and intensity ‎of the animations, and lots more. This web app is incredibly intuitive and easy to use.‎

Head over to the WLED wiki at https://kno.wled.ge/ to delve into all the particulars.‎

WLED Config

Next, we'll tell WLED about our physical setup. We'll give our project a name and easy-to-‎remember URL and tell the software how many LEDs we have set up on each pin.‎

WiFi Setup

Head to the WiFi Setup screen under Config. This is where your network credentials live, so ‎you can change them if needed. Scroll down to the mDNS field and create a good URL so ‎you can control your project from any web-enabled device. Call it something you'll ‎remember, that's easy to type into any web browser on your WiFi network in order to connect ‎to your project. ‎

In this example, I'd go to my web browser on my phone, iPad, or computer, and type in ‎‎"http://projectname.local" to open up the WLED interface on my screen. Your device must ‎be on the same WiFi network as your board.‎

config_26

config_27

LED Preferences

Next, head to the LED Preferences tab under the Config menu.‎

Scroll down to Hardware Setup. The Sparkle Motion board has 4 spots to attach LED ‎strips: the screw terminal uses GPIO 19, 22, and 21 and the through-hole solder pads to ‎the left of the screw terminal is GPIO 23.‎

WLED allows up to 4 strips to be connected at once. The strips can be of different types, ‎lengths, and color order. Select your LED type, length, and GPIO pin. If you have multiple ‎strips connected, click the + button and enter the additional strips in the same way.

tab_28

tab_29

Click "save" and if you've done everything correctly, your light strands should come on in a ‎warm, cheerful yellow color. Success! Time to start making pretty light animations. ‎

Troubleshooting

If your lights didn't come on, here are a few things to try:‎

  1. ‎Head back to WLED and check your pinout configuration under LED Preferences. Be ‎sure the pin number is the correct GPIO for the attachment point you used.‎

  2. Check your wiring! Be sure you connected to the IN end of the LED strip. These strips ‎can be inconsistent, so this is a pretty common problem. Use an alligator clip to try ‎connecting the data wire on the other end (the power and ground wires should work ‎from either end).‎

  3. Try re-uploading the WLED software. ‎

  4. If the lights come on but you can't control them: i.e., you type in "projectname.local" ‎into your browser and it won't connect, make sure you're on the correct WiFi network. ‎If you're on a different network than the one you set up the sofware on, you won't see ‎the WLED connection.‎

  5. If your lights came on in blue or green instead of yellow, your color order is wrong. ‎See below to fix.‎

  6. If only half your lights came on, be sure you've got the correct number in the "length" ‎field under LED preferences.‎

  7. If your lights came on in a variety of weird colors and looking like a 1950s diner ‎interior, you may have the wrong LED strip type selected. RGBW strips and RGB ‎strips are not the same, so be sure you've got the correct strip type, or you'll get very ‎odd behavior.‎

  8. If your microcontroller hangs or keeps rebooting, or gets really hot, you may have the ‎power and ground lines switched. Unplug right away and check: this is a fast way to ‎brick your controller.‎

Color Order

If your lights have come on in any color other than a warm yellow, there's one more setting ‎to change. LED strips and pixels are not all standardized, and sometimes the red, green, ‎and blue LEDs inside are connected in a different order. ‎

In the main interface window, choose "solid" as your effect and red as your color from the ‎color picker. ‎

If your lights come on in any color other than red, your color order is set incorrectly. This is ‎an easy fix. Head back to the LED settings tab and find the Hardware Setup section (this is ‎where you set up your pin number earlier). Choose BRG from the dropdown, click save, and ‎see if your pixel colors match your color picker now. If not, try another combo until the lights ‎look correct.‎

color_30

color_31

WLED 2d Matrix

If you're planning to set up xLights on this board once you're done installing WLED: STOP. ‎The 2-d setup can make xLights setup go haywire. Set up your xLights matrix models first, ‎then come back and set up the 2-d matrix in WLED. ‎

If you're using a 2-d matrix such as an LED curtain or net, WLED has a handy 2d-matrix ‎setup feature that will take care of the mapping for you. Head to Config and choose the 2D ‎Configuration tab.‎

Check out these tutorials for more about 2d mapping with WLED:‎

Change the dropdown to read 2d Matrix, and additional options will appear. If you want to ‎sync more than one panel, you can do it here. ‎

Set up your layout numbers to match the number of rows and columns in your project. ‎These nets have 20 pixels in a row and 20 pixels per meter.‎

You can also change orientation here - my pixels start in the lower left corner and finish in ‎the upper right.‎

dropdown_32

dropdown_33

Matrix Effects

WLED has a hefty number of matrix effects that appear in the list when you've got your 2d ‎matrix set up. Many of them can be customized with speed and intensity sliders, or ‎different color palettes. Go wild!

effects_34

xLights Setup

To get xLights installed, head over to the xLights Quick Start Guide. This will walk you ‎through downloading and installing the software. Be sure to install the Vamp Plugins as ‎well.‎

Once the software is installed, head to the Controllers tab to set up your Sparkle Motion ‎board.‎

Controller Setup

controller_35

Be sure your Sparkle Motion board is set up with WLED and plugged in to power. It doesn't ‎need to be plugged into your computer, just running on the same WiFi network. ‎

Click "Add Ethernet" and set up your board as shown. Mine is called Butterfly1 in WLED so I ‎kept the same name in xLights. Choose WLED as the vendor and model, and Generic ‎ESP32 as the variant. Change the protocol to DDP. Click save.‎

Model Setup

model_36

Next head to the Layout tab. Click the Matrix tool and draw a box in the black area - don't ‎worry about the size or shape yet just get it onto the field.‎

Click one of the dots on the matrix to select it. In the lower left, set up the parameters as ‎shown. Give it a name and click the "Don't Zig Zag" box since our matrix is not serpentine.‎

  • Under # Strings, enter 1. This means there's one data line feeding all the LEDs‎

  • Nodes/String: total number of pixels on this data line. Enter 400 for a 1-meter net or ‎‎800 for a 2-meter net

  • Strands/String: Total number of rows in your net. 20 for a 1m net or 40 for a 2m net

  • Starting Location: Change this so it matches your net's orientation

If you have a 4-meter net, or two smaller nets you'd like to "merge" into one, add a second ‎matrix and set it up the same way. For my setup. I'm using one 4m net and I have attached a ‎second data line at the 801st pixel. Drag it into place under the first matrix to line it up.‎

If you have multiple models, you can create a Group. I've grouped my two net sections into ‎one group called Net1. When I run animations on the Group, the whole net will act as one ‎continuous matrix instead of two separate pieces.‎

Save your models once you're happy with the layout.‎

Connect Ports

ports_37

Head back to the Controllers tab and select "Visualize". Drag your model(s) to the ports ‎you've connected to on the Sparkle Motion board. The screw terminal ports are 1, 2, and 3 ‎and the pin pad is 4.‎

Close the port window and click "Save". Then click the "Upload Output" button to send the ‎configuration to the controller.‎

window_38

save_39

Create a Sequence

Let's create a test sequence and see if we can get our lights responding. In the "Sequence" ‎tab in xLights, go to File > New Sequence. ‎

For now, just to keep things simple, choose Animation and 20 FPS (frames per second). ‎This will create a sequence that's populated with your models and ready to test your lights. ‎

sequence_40

sequence_41

Select the "Butterfly Effect" animation and drag it to your timeline, on the line that has your ‎matrix model or group. Drag the handle out so the effect takes up a good chunk of the ‎timeline, and press "play". You should see the animation appear on the onscreen model in ‎the lower left of the screen.‎

To send your sequence to the LED net, click the light bulb button in the top center of the ‎screen.‎

send_42

Troubleshooting

If your net doesn't respond, here are a few things to try:‎

  • Check your settings in WLED. Be sure the board is working and showing animations ‎on the net before setting up your controller in xLights

  • If you've set up a 2D matrix in WLED, try setting it back to 1D strip before configuring ‎xLights. Having two different matrix definitions can confuse things

  • Be sure you've saved your controller settings and clicked "Upload Output" ‎

  • If your matrix is trying to join 20 ports on the controller, change the "string" number ‎to 1‎

  • Be sure your computer and the controller are on the same WiFi network

  • Did you click the light bulb icon? That's what turns the show on and off / starts and ‎stops sending data to the lights

  • If it's just not working, try deleting all your models and controllers and start again

More Resources

xLights is a pro-level program with lots of functions and settings. It can be a little ‎overwhelming at first, but the possibilities are grand. Here are a few links with tutorials and ‎inspiration to get you started.‎

There are dozens of tutorials available on YouTube and even online courses available for ‎learning this massively deep program. Go wild.

מק"ט יצרן # 6159
NEOPIXEL LED OUTDOOR NETTING - 2
Adafruit Industries LLC
מק"ט יצרן # 6165
NEOPIXEL LED OUTDOOR NETTING - 8
Adafruit Industries LLC
₪ 1,229.58
הצגת עוד Details
מק"ט יצרן # 875
BATTERY HOLDER AA 8 CELL LEADS
Adafruit Industries LLC
מק"ט יצרן # 6024
ADAFRUIT NEOPIXEL PEBBLE / SEED
Adafruit Industries LLC
מק"ט יצרן # 2632
1/4 TO 1/4 SCREW ADAPTER - FOR C
Adafruit Industries LLC
PANEL MOUNT 1K POTENTIOMETER (BR
מק"ט יצרן # 1789
PANEL MOUNT 1K POTENTIOMETER (BR
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.