Maker.io main logo

Low-Cost Data Acquisition (DAQ) with Arduino and Binho for ML

2,012

2020-03-16 | By ShawnHymel

License: Attribution Arduino

Data Acquisition (DAQ) is the process of collecting information from one or more sensors for processing on a computer. Most DAQ devices act as a converter to read from one or more sensors and convert the reading to a raw measurement value. Many DAQ devices can be scripted to read at various intervals, at particular data rates, etc.

DAQ diagram

Many professional DAQ devices are easily a few hundred to thousands of dollars. If you only need to collect simple data, like from an accelerometer or temperature sensor, we can create our own DAQ device from an Arduino. Additionally, we can step up to the professional Binho Nova host adapter to act as a DAQ as well.

With both of these devices, we can rely on community-written libraries to avoid having to write driver code to communicate with the sensors, which saves us a good amount of time (and staring at datasheets). While we do need to write some code to read from the sensors and DAQ devices, it can prove to be a more economical solution than relying on a professional DAQ.

Collecting sensor data can be extremely important to many machine learning tasks, as you will often need to collect hundreds or thousands of samples. Scripting the collection of these can make the collection process much easier.

You can see how to work with the Arduino and Binho Nova to read from a sensor in video form here:

 

Arduino DAQ

Arduino has made writing firmware for microcontrollers extremely easy and accessible for many people. While the abstraction layers might be less efficient as writing strict C tailored for your target process, it can make creating a DAQ quick and (relatively) painless. You have access to several different sensor interfaces, including analog-to-digital converters (ADC), I2C, and SPI. Additionally, community-written libraries mean you can spend less time writing low-level firmware drivers.

To start, we’ll write a quick Arduino sketch that reads from an MSA301 accelerometer and prints out the X, Y, and Z acceleration measurements over Serial whenever an ‘r’ character is received. This lets our computer control the sampling rate. You’ll want to note the sampling rate of the accelerometer, so there is a little bit of datasheet reading that’s needed. If we’re using the Adafruit library, the sensor updates its internal values at a rate of 500 Hz by default (which can be changed up to 1000 Hz). So, you’ll need the computer to sample no faster than 500 Hz.

Connect the MSA301 accelerometer board to the Arduino via I2C port:

 

Copy Code
Arduino --> MSA301
   5V   -->  VIN
  GND   -->  GND
  SCL   -->  SCL
  SDA   -->  SDA

 

 

Wiring Arduino to MSA301

In a new Arduino sketch, install the Adafruit MSA301 library, the Adafruit BusIO library, and the Adafruit unified sensor library (as per this tutorial). Enter the following code:

 

Copy Code
#include <Wire.h>
#include <Adafruit_MSA301.h>
#include <Adafruit_Sensor.h>

Adafruit_MSA301 msa;

void setup() {

  // Open serial port
  Serial.begin(250000);

  // Initialize MSA301
  if (!msa.begin()) {
    Serial.println("Error: Could not find MSA301 chip");
    while (1);
  }
}

void loop() {

  char c;

  // Wait until we get an 'r' on the serial line
  if (Serial.available()) {
    c = Serial.read();
    if (c == 'r') {
      
      // Get new MSA reading
      msa.read();
    
      // Print out results
      Serial.print(msa.x_g);
      Serial.print('\t');
      Serial.print(msa.y_g);
      Serial.print('\t');
      Serial.println(msa.z_g);
    }
  }
}

 

 

Upload that to your Arduino. I’m using an Arduino UNO in this example, but you’re welcome to use almost any Arduino board (assuming you have an I2C port). Open the Serial monitor. At the top, enter an ‘r’ character and press “Send.” You should see 3 values printed out, corresponding to X, Y, and Z acceleration measurements from the MSA301. Note that the units are g-force.

Read from Arduino DAQ with Python

Since we’re doing this for use in machine learning (ML), I’m going to show the example in Jupyter Notebook. However, you’re welcome to use regular Python as well.

First, we need to install the pyserial package. In a new cell, enter:

 

Copy Code
!python -m pip install pyserial

 

 

When that’s done, import a few packages in the next cell:

 

Copy Code
import serial
import numpy as np
import matplotlib.pyplot as plt
import time

 

 

We then need to set some parameters. You’ll want to change the serial port to match your Arduino (which you can find in the Arduino IDE):

 

Copy Code
# Settings
serial_port = 'COM19'
baud_rate = 250000
label_name = 'circle'
num_class_samples = 10   # Number of samples to collect for this label category
time_per_sample = 2.0    # Seconds
accel_sample_rate = 100  # Times per second (Hz) to read from acceleromater
num_accel_samples = int(time_per_sample * accel_sample_rate)

 

 

As a test, we’ll want to open the serial port and attempt to read from the Arduino.

 

Copy Code
# Test Serial port (open, wait for Arduino to reset, read line, close)
ser = serial.Serial(serial_port, baud_rate, timeout=1)
time.sleep(2)
ser.write('r'.encode('ascii'))
line = ser.readline()
ser.close()
print(line)

 

 

Seeing how this works, we can create a function that reads a number of measurements from the Arduino equal to the sample time we set:

 

Copy Code
# Open serial port and read lines
def capture_accel(ser, nsamples):
    samples = np.zeros((nsamples, 3))
    for i in range(nsamples):
        
        # Use timer to determine when to take measurement next
        start = time.time()
        
        # Transmit 'r' to have Arduino respond with X, Y, and Z acceleration
        ser.write('r'.encode('ascii'))
        line = ser.readline()
        parsed = line.decode().rstrip().split('\t')
        sample = np.array([float(axis) for axis in parsed])
        samples[i] = sample
        
        # Wait before reading again
        while (time.time() - start) < (1. / accel_sample_rate):
            pass
        
    return samples

 

 

Finally, we create a script that calls the previous function to read a number of samples. In this example, let’s say we’re making a “magic wand” that responds to gestures in the air made with the accelerometer. So, we would have the user press the ‘enter’ key when they’re ready and then have 2 seconds to make the gesture.

In normal deep learning implementations, we would need hundreds or thousands of examples to get a robust model. To keep things simple in this example, I’ll only capture 10 samples of each gesture.

In the next cell, run the following code:

 

Copy Code
# Capture sample set
accel_data = np.zeros((num_class_samples, num_accel_samples, 3))
ser = serial.Serial(serial_port, baud_rate, timeout=1)
print('Waiting for Arduino to reset...')
time.sleep(2)
i = 0
while i < num_class_samples:
    input('Press enter and draw shape with board')
    try:
      
      # Get sample from Arduino
      samples = capture_accel(ser, num_accel_samples)
      accel_data[i] = np.array(samples)
      print('Sample', i, 'captured with shape:', accel_data[i].shape)
      i += 1
      
    except:
      print('Error parsing samples. Try again.')
      pass
ser.close()

 

 

Now that we have all of our samples captured, we can use Matplotlib to plot a few of them to see if everything looks right:

 

Copy Code
# Plot a few
for sample_idx in range(5):
    fig = plt.figure(figsize=(14,2))
    ax = fig.add_subplot(111)
    ax.plot(accel_data[sample_idx, :, 0], label='x')
    ax.plot(accel_data[sample_idx, :, 1], label='y')
    ax.plot(accel_data[sample_idx, :, 2], label='z')
    plt.legend(loc='upper left')
plt.show()

 

 

With the above code, you should get 5 plots that look something like the following:

Plot from circle gesture

Finally, save the raw data in a file:

 

Copy Code
# Save raw accelerometer data
np.save(label_name, accel_data)

 

 

Just as a test, we can read and print out the raw readings:

 

Copy Code
# Test: load array
test_data = np.load(label_name + '.npy')
print(test_data)

 

 

The full code for this example can be found here: https://gist.github.com/ShawnHymel/4d2ed5b5e8f6b516d1c5f7e52d40bf68#file-read_msa301_arduino-ipynb

Binho Nova DAQ with Python

The Binho Nova is a host adapter, which is a useful device for communicating with various sensors and analog/digital devices from your computer. Normally, host adapters are used to debug problems with devices that rely on digital communications, like SPI and I2C. They are also useful for configuring chips, such as flash or EEPROM, prior to assembly during manufacturing.

That being said, they can also be used as an alternative to a DAQ device. The Binho Nova is an inexpensive host adapter that works with CircuitPython. As a result, we can use many of the Adafruit (and community) CircuitPython libraries with the Binho Nova to communicate with various sensors.

Please note that at this time, I2C writes with CircuitPython seem to be somewhat slow with the Binho Nova. I found that it took about 40 ms between I2C reads/writes. Raw communication with the Binho Nova is much faster, if you don’t mind writing your own driver (using raw reads/writes in Python). Hopefully, this will speed up in the future, as being able to use community libraries with a host adapter makes development much easier.

To begin, you’ll need to install the Blinka and Binho Python libraries found on this tutorial.

If you’re using Jupyter Notebook, you’ll need to set an environment variable prior to launching Jupyter Notebook. For example, if you’re using Anaconda, you’ll want to enter one of the following into the Anaconda prompt.

Windows:

 

Copy Code
set BLINKA_NOVA=1

 

 

Mac/Ubuntu (in the command prompt before launching Jupyter Notebook):

 

Copy Code
export BLINKA_NOVA=1

 

 

After, you can launch Jupyter Notebook:

 

Copy Code
jupyter notebook

 

 

In the first cell, if you haven’t already, install the following libraries:

 

Copy Code
!python -m pip install binho-host-adapter
!python -m pip install adafruit-blinka
!python -m pip install adafruit-circuitpython-msa301

 

 

Next, import the necessary packages:

 

Copy Code
import board
import busio
import adafruit_msa301
import numpy as np
import matplotlib.pyplot as plt
import time

 

 

Then, create some settings like last time:

 

Copy Code
# Settings
label_name = 'down_up'
num_class_samples = 10    # Number of samples to collect for this label category
time_per_sample = 2.0     # Seconds
accel_sample_rate = 25    # Times per second (Hz) to read from accelerometer
num_accel_samples = int(time_per_sample * accel_sample_rate)

 

 

We can initialize communication with the MSA301 sensor through the Binho Nova with the following:

 

Copy Code
# Create library object using Bus I2C port
i2c = busio.I2C(board.SCL, board.SDA)
msa = adafruit_msa301.MSA301(i2c)

 

 

We’ll want to test communication with the sensor with:

 

Copy Code
# Test reading from sensor
start = time.time()
print(msa.acceleration)
print(time.time() - start)

 

 

Just like in the Arduino example, we’ll want to write a function that reads from the sensor for 2 seconds:

 

Copy Code
# Connect to Binho Nova and read samples
def capture_accel(nsamples):
    samples = np.zeros((nsamples, 3))
    for i in range(nsamples):
        
        # Use timer to determine when to take measurement next
        start = time.time()
        
        # Read X, Y, and Z acceleration over I2C and convert to g-force
        accel = msa.acceleration
        sample = np.array([axis / 9.80665 for axis in accel])
        samples[i] = sample
        
        # Wait before reading again
        while (time.time() - start) < (1. / accel_sample_rate):
            pass
        
    return samples

 

 

We then create a script that captures 10 (or however many you want) samples:

 

Copy Code
# Capture sample set
accel_data = np.zeros((num_class_samples, num_accel_samples, 3))
i = 0
while i < num_class_samples:
    input('Press enter and draw shape with board')
    try:
        
        # Get sample from Binho Nova
        samples = capture_accel(num_accel_samples)
        accel_data[i] = np.array(samples)
        print('Sample', i, 'captured with shape:', accel_data[i].shape)
        i += 1
        
    except:
        print('Error parsing samples. Try again.')
        pass

 

 

When you run this cell, follow the prompts to press the 'enter' key and perform the gesture in the air with the sensor.

When that’s done, we can plot a few samples with the following:

 

Copy Code
# Plot a few
for sample_idx in range(5):
    fig = plt.figure(figsize=(14,2))
    ax = fig.add_subplot(111)
    ax.plot(accel_data[sample_idx, :, 0], label='x')
    ax.plot(accel_data[sample_idx, :, 1], label='y')
    ax.plot(accel_data[sample_idx, :, 2], label='z')
    plt.legend(loc='upper left')
plt.show()

 

 

You should get 5 plots that look something like the following:

Plot for down-up gesture

Finally, we save the samples as a Numpy array with:

 

Copy Code
# Save raw accelerometer data
np.save(label_name, accel_data)

 

If we want to test loading the array, we can do that with:

Copy Code
# Test: load array
test_data = np.load(label_name + '.npy')
print(test_data)

 

The full code can be found here: https://gist.github.com/ShawnHymel/8e2e57e76d30939a899b743330df5f10

Going Further

Hopefully, these examples have helped give you some ideas on how you can capture sensor data inexpensively by creating your own DAQ device out of an Arduino or host adapter. While the process might involve a little more code writing than other DAQ options, you can rely on community libraries to simplify the whole process.

The Binho Nova has a number of adapters (e.g. QWIIC) to make interfacing to various sensor boards much easier, some of which can be found here.

Binho Qwiic connection

Here are some other resources to help you in your journey:

מק"ט יצרן # 4344
MSA301 TRIPLE AXIS ACCELEROMETER
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.