Maker.io main logo

PyLeap BLE Controlled NeoPixels with CLUE

77

2023-12-26 | By Adafruit Industries

License: See Original Project LED Strips

Courtesy of Adafruit

Guide By Liz Clark

Overview

 

One of the CLUE's many features is BLE connectivity, which opens ‎up possibilities for utilizing wireless communication. In this project, ‎you'll use the PyLeap app to wirelessly load the project code onto ‎your CLUE. Then, you'll connect to the CLUE with the Adafruit ‎Bluefruit Connect app to change the colors and animations of a strip ‎of NeoPixels over BLE.‎

projects_colorHero

Original Project

This project was originally created by Erin St. Blaine and Kattni ‎Rambor with CircuitPython and a Circuit Playground Bluefruit. The ‎code has been adapted for the CLUE to make use of the CLUE's ‎screen to display animation and RGB color information. You can ‎check out the original Learn Guide for more information on how the ‎code works.‎

Easy No-Soldering Bluetooth Controlled Room Lights Learn Guide

Parts

Connect the NeoPixels to the CLUE

connect_1

To wire up the strip of NeoPixels to the CLUE, you'll clip the NeoPixel ‎strip's alligator clips to the CLUE's pads located at the bottom of the ‎board. The alligator clips are color coded so that you can tell which ‎connection goes where.‎

Wiring Diagram

wiring_2

  • NeoPixel Data In to CLUE pad 0 (white wire)‎
  • NeoPixel Power to CLUE 3V pad (red wire)‎
  • NeoPixel Ground to CLUE GND pad (black wire)‎

Assembly

First, make sure that your CLUE is disconnected from power. Then, ‎clip the NeoPixel strip's white alligator clip to the CLUE's pad 0. ‎This is the data input for the NeoPixel strip.‎

first_3

Next, clip the NeoPixel strip's red alligator clip to the CLUE's 3V pad. ‎This is the power input for the NeoPixel strip.‎

next_4

Finally, clip the NeoPixel strip's black alligator clip to the CLUE's ‎GND pad. This is the ground connection for the NeoPixel strip.‎

finally_5

Now your NeoPixel strip is connected to your CLUE!

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY flash drive to iterate.‎

The following instructions will show you how to install CircuitPython. ‎If you've already installed CircuitPython but are looking to update it ‎or reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for CLUE from ‎circuitpython.org

Click the link above to download the latest version of ‎CircuitPython for the CLUE.‎

Download and save it to your desktop (or wherever is handy).‎

click_6

Plug your CLUE into your computer using a known-good USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So, make sure you have a USB cable you know is good ‎for data sync.‎

Double-click the Reset button on the top (magenta arrow) on your ‎board, and you will see the NeoPixel RGB LED (green arrow) turn ‎green. If it turns red, check the USB cable, try another USB port, ‎etc. Note: The little red LED next to the USB connector will pulse red. ‎That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

plug_7

You will see a new disk drive appear called CLUEBOOT.‎

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.‎

drag_8

drag_9

The LED will flash. Then, the CLUEBOOT drive will disappear, and a ‎new disk drive called CIRCUITPY will appear.‎

If this is the first time, you're installing CircuitPython or you're doing ‎a completely fresh install after erasing the filesystem, you will have ‎two files - boot_out.txt, and code.py, and one folder - lib on ‎your CIRCUITPY drive.‎

If CircuitPython was already installed, the files present before ‎reloading CircuitPython should still be present on ‎your CIRCUITPY drive. Loading CircuitPython will not create new ‎files if there was already a CircuitPython filesystem present.‎

That's it, you're done! :)

flash_10

Pairing

Now that you're done uploading the correct ‎firmware, disconnect your device from your computer and power it ‎via LiPoly or AAA battery pack.‎

Pairing device to PyLeap

Once powered, press the small Reset button in the center of the ‎board (Circuit Playground Bluefruit) or on the top right of the board ‎‎(CLUE). When the blue light flashes, press the Reset button again.‎

circuit_playground_ezgif22

Circuit Playground Bluefruit with a small Reset button in the center of the board

reset_12

Adafruit CLUE Reset Button (Highlighted on the upper right)‎

When done correctly, the LEDs will flash yellow followed by solid ‎blue. Once this occurs, the board will continuously be in discovery ‎mode.‎

Scan & Connect

When your Circuit Playground Bluefruit or Adafruit CLUE is in ‎discovery mode, hold it very closely to your iPhone or iPadOS to pair. ‎

circuitpython_ezgifcom-gif-maker

Below the spinning Blinka, you'll notice a status indicator that will let ‎you know your current pairing status.‎

Once you've found your device and received the Bluetooth Pairing ‎Request message, press Pair to pair your board to your iPhone or ‎iPadOS.‎

message_14

If your Circuit Playground Bluefruit doesn't ‎appear:‎

  1. ‎Check to see if your Circuit Playground Bluefruit is powered on. ‎Verify that the green On light is lit.
  2. Make sure your Circuit Playground Bluefruit is running the ‎correct firmware. See the CircuitPython page in this guide.‎‎
  3. Try resetting the Circuit Playground Bluefruit by pressing the ‎small Reset button near the center of the board.‎

BLE Controlled NeoPixels Code

ble_15

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 Kattni Rembor for Adafruit Industries
# SPDX-FileCopyrightText: 2020 Erin St Blaine for Adafruit Industries
#
# SPDX-FileCopyrightText: 2022 Liz Clark for Adafruit Industries (Adapted for CLUE)
#
# SPDX-License-Identifier: MIT

# pylint: disable=attribute-defined-outside-init
# pylint: disable=too-few-public-methods

import board
import neopixel
import displayio
import terminalio
from adafruit_display_text import label
from rainbowio import colorwheel
from adafruit_display_shapes.rect import Rect
from adafruit_led_animation.animation.solid import Solid
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.rainbow import Rainbow
from adafruit_led_animation.animation.rainbowcomet import RainbowComet
from adafruit_led_animation.animation.sparkle import Sparkle
from adafruit_led_animation.animation.sparklepulse import SparklePulse
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation.group import AnimationGroup
from adafruit_led_animation.animation import Animation
from adafruit_led_animation.sequence import AnimateOnce
from adafruit_led_animation.color import (
AMBER,
ORANGE,
WHITE,
RED,
BLACK
)

from adafruit_ble import BLERadio
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.nordic import UARTService

from adafruit_bluefruit_connect.packet import Packet
from adafruit_bluefruit_connect.button_packet import ButtonPacket
from adafruit_bluefruit_connect.color_packet import ColorPacket

NUM_LEDS = 60 # change to reflect your LED strip
NEOPIXEL_PIN = board.D0 # change to reflect your wiring

# Declare a NeoPixel object on NEOPIXEL_PIN with NUM_LEDS pixels,
# no auto-write.
# Set brightness to max, we'll control it later in the code
pixels = neopixel.NeoPixel(NEOPIXEL_PIN, NUM_LEDS, brightness=1.0,
auto_write=False,
)

ble = BLERadio()
uart_service = UARTService()
advertisement = ProvideServicesAdvertisement(uart_service)

display = board.DISPLAY
clue_group = displayio.Group()

rect = Rect(0, 0, 240, 240, fill=0x0)
clue_group.append(rect)

text_area = label.Label(terminalio.FONT, text="CONNECT TO BLE", color=WHITE)
text_area.anchor_point = (0.5, 0.5)
text_area.anchored_position = (240 / 2, 240 / 2)
text_area.scale = 2
clue_group.append(text_area)

display.root_group = clue_group

class RainbowFade(Animation):
''' fades the entire strip through the whole spectrum '''
_color_index = 150 # choose start color (0-255)
def __init__(self, pixel_object, speed, name): # define animation
super().__init__(pixel_object, speed=speed, color=WHITE, name=name)

def draw(self): # draw the animation
''' fades the entire strip through the whole spectrum '''
self.color = colorwheel(self._color_index + 1)
self._color_index = (self._color_index + 1) % 256
self.fill(self.color)

# ANIMATION DEFINITIONS --
# create as many animations as you'd like and define their attributes here.
# They can be a single line or a group of animations - the groups will play
# at the same time, overlaid on top of each other.


readingLight = Solid(pixels, color=0xFF7D13, name="reading light") #warm white color HEX code
brightWhite = Solid(pixels, color=(150, 150, 150), name="bright white")
rainbow = Rainbow(pixels, speed=0.1, period=10, step=0.5, name="rainbow")
rainbowfade = RainbowFade(pixels, speed=0.4, name="rainbowfade")
powerup = RainbowComet(pixels, speed=0, tail_length=50, bounce=False, name="rainbow comet")
off = Solid(pixels, color=BLACK, name="off")

#startup animation will play just once
startup = AnimateOnce(powerup)

#starrynight and fire are animation groups with layered effects.
starrynight = AnimationGroup(
SparklePulse(pixels, speed=0.01, color=(0, 0, 150), period=1),
Comet(pixels, speed=0, tail_length=8, color=(150, 150, 150), bounce=False),
name = "starrynight")

fire = AnimationGroup(
Comet(pixels, speed=0.1, tail_length=1, color=BLACK),
Sparkle(pixels, speed=0.1, num_sparkles=10, color=AMBER),
Sparkle(pixels, speed=0.1, num_sparkles=10, color=RED),
Sparkle(pixels, speed=0.1, num_sparkles=20, color=ORANGE),
Sparkle(pixels, speed=0.1, num_sparkles=5, color=0xFF7D13),
Sparkle(pixels, speed=0.1, num_sparkles=10, color=BLACK),
name = "fire"
)

# Here is the animation playlist where you set the order of modes

animations = AnimationSequence(
readingLight,
fire,
rainbow,
starrynight,
rainbowfade,
brightWhite,
auto_clear=True,
)


current_color = BLACK
MODE = 0

while True:
if MODE == 0: # If currently off...
startup.animate()
while startup.animate():
pass
MODE = 3
# Advertise when not connected

elif MODE >= 1: # If not OFF MODE...
ble.start_advertising(advertisement)
while not ble.connected:
text_area.text = "CONNECT TO BLE"
if MODE == 2:
pass
elif MODE == 1:
animations.animate()
# Now we're connected

while ble.connected:
if uart_service.in_waiting:
packet = Packet.from_stream(uart_service)
# Color Picker Functionality
if isinstance(packet, ColorPacket):
MODE = 2
# Set all the pixels to one color and stay there.
pixels.fill(packet.color)
pixels.show()
text_area.text = str(packet.color)
# Control Pad Functionality
elif isinstance(packet, ButtonPacket):
if packet.pressed:
if packet.button == ButtonPacket.BUTTON_1:
MODE = 1
animations.activate(1)
elif packet.button == ButtonPacket.BUTTON_2:
MODE = 1
animations.activate(2)
elif packet.button == ButtonPacket.BUTTON_3:
MODE = 1
animations.activate(3)
elif packet.button == ButtonPacket.BUTTON_4:
MODE = 1
animations.activate(4)
# change the mode with right arrow
elif packet.button == ButtonPacket.RIGHT:
MODE = 1
animations.next()
elif packet.button == ButtonPacket.LEFT:
MODE = 4
off.animate()
#change the brightness with up and down arrows
elif packet.button == ButtonPacket.UP:
pixels.brightness = pixels.brightness + 0.1
pixels.show()
if pixels.brightness > 1:
pixels.brightness = 1
elif packet.button == ButtonPacket.DOWN:
pixels.brightness = pixels.brightness - 0.1
pixels.show()
if pixels.brightness < 0.1:
pixels.brightness = 0.1
if MODE == 1:
text_area.text = str(animations.current_animation.name)
if MODE == 4:
text_area.text = str(off.name)
if MODE == 1:
animations.animate()
if MODE == 3:
text_area.text = "CONNECTED"
if MODE == 4:
animations.freeze()

 

View on GitHub

Bluefruit Connect App

app_16

After loading the project onto your CLUE with PyLeap, close out of ‎the PyLeap app. This disconnects the CLUE from PyLeap.‎

Now, your CLUE display will show "CONNECT TO BLE", signaling that ‎it's ready to connect to the Bluefruit Connect App. Follow along with ‎the next two pages to download and install the app and then ‎connect to the CLUE with it.‎

You need to close out of PyLeap before connecting to the Bluefruit ‎Connect App. The CLUE can only be connected to one app at a time.‎

Installation and Setup

install_17

The Bluefruit LE Connect app provides iOS & Android devices with a ‎variety of tools to communicate with Bluefruit LE devices. These ‎tools cover basic communication and info reporting as well as more ‎project specific uses such as Arduino Pin Control and a Color Picker.‎

The iOS app is a free download from Apple's App Store. It requires ‎iOS 11.3 or later and works on iPhones, iPads, and iPod Touches.‎

The Android app is a free download from the Google Play Store. It ‎requires Android 4.4 or later.‎

The app is compatible with these BLE devices from Adafruit, and ‎possibly more:‎

First off - install the app from one of the App stores listed above if ‎you haven't already.‎

Enable Bluetooth

If Bluetooth is disabled on your device, enable it by going ‎to Settings->Bluetooth on your iOS device, or the analogous setting ‎on your Android device.‎

enable_18

Enable Location Services

If you plan to use the app to send location/GPS data to Bluefruit LE, ‎enable Location Services. Enable it on iOS using Settings->Privacy-‎‎>Location Services.‎

services_19

Scan for Devices

On launch, the app will automatically begin to scan for ‎nearby Bluetooth LE devices. Devices are presented in a table ‎view in the order in which they were discovered.‎

Don't forget to turn on Bluetooth on your device! Airplane Mode ‎turns off BLE.‎

iPhone

The following images depict the app when used on the iPhone. The ‎Android app looks similar.‎

iphone_20

The device list will display all BLE devices discovered by the app (not ‎just Bluefruit hardware) - so you may see a quite a few "" or ‎‎<Unknown> entries for devices that don't advertise their name, as ‎seen above.‎

  • To refresh the list and start a new scan, simply swipe down on ‎the current list
  • Each device's signal strength is displayed in the left side of its ‎row.‎

If you tap on the device entry (not on Connect), you'll see more detail ‎about a particular device:‎

tap_21

iPad

The following images depict the app when used on the iPad.‎

ipad_22

Tap the middle of a device's table row to reveal its relevant ‎advertisement data.‎

  • Any device listed with a "Connect" button at the right can be ‎accessed in Info mode
  • Any device listed as "UART Capable" can be used with all ‎modes - Info, UART, Pin I/O, & Controller.‎

To use the Bluefruit Connect app with your device it must be "UART ‎capable"! All Adafruit BLE devices implement the UART interface, ‎but other devices may not.

Multiple UART Mode

multiple_23

The Multiple UART feature allows to monitor incoming data from and ‎send data to multiple devices simultaneously.‎

To use it:‎

  • Activate the Multiple UART Mode switch
  • Tap Connect next to each device you'd like to include
  • Tap the Start button below the Multiple UART mode to begin

Once connected, you can choose UART or Plotter module to view ‎incoming data from all connected peripherals. In the UART module, ‎you can send data to one or all connected devices at once.‎

Connect

Tap the Connect button on the UART capable list entry you wish to ‎use and choose a connection mode from the menu that appears.‎

button_24

Troubleshooting

trouble_25

If you’re having trouble finding your Bluefruit device in the scanned ‎peripherals list, ensure the board is powered and not paired with ‎any other BLE devices. If the problem persists, it could be due ‎to caching issues in the iOS or Android operating system. For a fix, ‎try the following:‎

  • Cycle Bluetooth - Turn your mobile device’s Bluetooth radio off ‎and on again in the Settings app
  • Relaunch App - Quit the Bluetooth LE Connect app and restart ‎it. (instructions for iOS & Android)
  • Cycle Power - Restart your mobile device by powering it off ‎and restarting.‎

Doing one or both of the above solves most peripheral scanning ‎issues. If you're still having trouble, try searching the Adafruit ‎Support forum for your issue.‎

Usage

After connecting your CLUE to the Bluefruit app, your CLUE display ‎will show "CONNECTED". Now you can start controlling the NeoPixel ‎strip's animations and colors with the app.‎

display_26

In the app, select the Controller module. Then select the Control ‎Pad on the next screen.‎

projects_appController_1

You can press the different onscreen number buttons to select the ‎NeoPixel animations. The CLUE screen will display the name of the ‎animation.‎

  • 1 - Fire animation
  • ‎2 - Rainbow animation
  • 3 - Starry night animation
  • 4 - Rainbow fade animation

projects_modeSelect

The arrow buttons can also affect the NeoPixels.‎

  • Up - increase brightness
  • Down - decrease brightness
  • Right - advance through the animations in order
  • Left - turn the NeoPixels off

projects_brightness

Go back to the main Controller module page and select the Color ‎Picker.‎

projects_colorWheel_1

Select your color in the color wheel and then press Send selected ‎color to change the color of the NeoPixels. The CLUE screen will ‎display the RGB color code.‎

projects_colorPicker

You can change the saturation of the color by moving the ‎slider under the color wheel.‎

projects_saturationSlider

מק"ט יצרן # 3811
ADDRESS LED STRIP SERIAL RGB
Adafruit Industries LLC
מק"ט יצרן # 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
מק"ט יצרן # 3287
BATTERY HOLDER AA 3 CELL LEADS
Adafruit Industries LLC
מק"ט יצרן # 727
BATTERY HOLDER AAA 3 CELL LEADS
Adafruit Industries LLC
מק"ט יצרן # 2487
MOD FLORA WEARABLE BLUEFRUIT LE
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.