Maker.io main logo

How to Fuse Motion Sensor Data into AHRS Orientation (Euler/Quaternions)

440

2024-03-11 | By Adafruit Industries

License: See Original Project Arduino

Courtesy of Adafruit

Guide by Lady Ada

Overview

 

AHRS is an acronym for Attitude and Heading Reference System, a ‎system generally used for aircraft of any sort to determine heading, ‎pitch, roll, altitude etc.

A basic IMU (Intertial Measurement Unit) generally provides raw sensor ‎data, whereas an AHRS takes this data one step further, converting it ‎into heading or direction in degrees. ‎

To help you get started designing your own AHRS system, or just to ‎help convert raw sensor data into useful numbers that you can relate ‎to the real world, we've created an Arduino library that lets you 'fuse' a ‎range of common accelerometer/gyroscope/magnetometer sensor sets ‎using a few different algorithms such ‎as Mahony, Madgwick, and NXP Sensor Fusion.‎

We recommend a Cortex M0 or faster/greater chipset - there's a lot of ‎math and memory required so 4KB+ or RAM and 32 MHz+ speed helps ‎for the fancier algorithms. That said, you can do some basic fusion ‎with an ATmega328p (Arduino UNO compatible). The data is output on ‎the serial port for easy integration.‎‎

  1. We'll start by verifying you can store calibrations on your chipset, ‎and then calibrating your sensors.‎‎
  2. Then we'll compile the AHRS library for your desired sensors and ‎algorithm/
  3. Finally, we'll visualize the motion using a Web Serial API 3D model.‎

sensors_Rabbit10DOF

Storing Calibrations

Every sensor will vary and need calibration. Some sensors have a 'range' ‎for their error output, which helps us know if the sensor is functioning ‎‎- but we still need to calibrate every sensor/board. One of the ‎challenges with per-device-calibration is how to store that calibration.‎

We could put the calibrations at the top of the Arduino sketch, but we ‎would have to re-compile it for each device, and it’s also easy to forget ‎or lose the calibration.‎

So, instead, we try to store the calibration in non-volatile memory - ‎that means either EEPROM or external FLASH. We try to use external ‎flash not internal flash, because internal flash can be erased and ‎overwritten when we upload new code.‎

There's lots of different ways you could save calibrations - but to make ‎things easiest we're going to stick to those two techniques. However, ‎that means our board has to have some sort of NVM available! Here's ‎what you can expect:‎

EEPROM Memory (either real or ‎simulated)‎

Some chips have EEPROM memory, this is a tiny amount of memory, ‎which is separate from FLASH, where you can tuck maybe 256 bytes of ‎data. There's two kinds of EEPROM, 'real' and 'simulated'. Real is, well, ‎real! There's literally a chunk of memory inside the chip itself, and ‎you'll see it mentioned in the datasheet as EEPROM.‎

The ATmega328 datasheet indicates that you can get up to 1KB of ‎EEPROM (depends on which model of the chip you buy.)

features_1

‎It’s not terribly common to see EEPROM in chips as you get to the ‎more expensive models. Partially that's because they tend to have SPI ‎Flash chips, but also cause they aren't that useful with larger chips. ‎Either way, simulated EEPROM is when some internal SPI flash or ‎external memory storage is dual used as EEPROM. For example, the ‎ESP8266 uses the very end of the SPI flash chip that holds the program memory ‎for EEPROM.

Some chips with real EEPROM:‎

  • ATmega328 (Arduino Uno/Metro/compatibles)
  • ATmega32u4 (Arduino Leonardo/compatibles)
  • ATmega2560 (Arduino Mega/compatibles)‎

Some chips with simulated EEPROM:‎

External SPI or QSPI memory

This is a separate chip used to store files, code, audio, graphics, etc. A ‎lot of Adafruit products have SPI/QSPI memory in order to support ‎CircuitPython. For example:‎

  • All Adafruit nRF52840 boards
  • All Adafruit SAMD51 ("M4") boards
  • Many SAMD21 ("M0") boards (they'll often have Express in the ‎name)‎

The reason we prefer external memory is that you can edit the file ‎using any text editor, when CircuitPython (or another mass-storage ‎enabled sketch) is loaded. Also, many of the above do not have ‎EEPROM, so there's often not a choice.‎

The Feather M0 Express has an 8-SOIC SPI Flash chip highlighted to ‎the left.‎

feather_2

The only thing to watch out for is that the SPI FLASH must ‎be formatted with a filesystem - much like an SD card (altho, these ‎days, SD cards come pre-formatted). A blank SPI Flash chip doesn't ‎have anything on it.‎

Manually Setting in Code

The least desirable, but sometimes necessary, option is to simply set ‎the calibration at the top of your sketch/code. It's not something we ‎like to do because it’s easy to lose the calibration, but it's always an ‎option!‎

Calibration Pre-Check

OK before we continue, we have to check that we are able to store ‎calibration either in the EEPROM (ATmega328, 'm32u4, 'm2560, ‎ESP8266, ESP32) or (Q)SPI Flash (most Adafruit M0, M4, nRF52840 ‎boards.)‎

Library Installation

You'll need a few libraries, install them through the library manager!‎

library_3

Search for and install Adafruit Sensor Calibration.

library_4

We strongly recommend using Arduino IDE 1.8.10+ because it will ‎automatically install any dependency libraries. If you have to install ‎manually, grab SdFat - Adafruit Fork, ArduinoJson, Adafruit ‎SPIFlash, Adafruit Unified Sensor as well (see all dependencies here.)‎

Compilation & Upload Check

Load sensor_calibration_read example - yes even though there is no ‎calibration yet, this will let us verify the basics!‎

load_5

EEPROM Storage

First, we'll try loading it into a chip with EEPROM (an ATmega328-‎based Metro mini!)‎

loading_6

Here's what you should look for:‎

  • At the top you'll see that Has EEPROM is 1 - indicating we're ‎using the internal EEPROM
  • It's OK to see No calibration loaded/found (it’s a fresh chip!)
  • The hex block after the **WARNING** is the raw calibration data ‎stored. It's normal to see all 0x00 or 0xFF's if this is the first time ‎running the program.
  • Finally, you'll see Calibrations found:‎
    • Magnetic Hard Offset should default to 0, 0, 0 (no offset)‎
    • Magnetic Soft Offset should default to 1, 0, 0, 0, 1, 0, 0, ‎‎0, 1 - note that isn't all zeros! It's a 3x3 identity matrix.
    • Gyro Zero Rate Offset should default to 0, 0, 0 (no offset)‎
    • Accel Zero Rate Offset should default to 0, 0, 0 (no offset)‎

If you got this far, you're good! Go to the next page where we try to ‎write calibrations.‎

Flash Storage

Here's what you can expect if you're using a chip with built in SPI/QSPI ‎storage!‎

storage_7

Here's what you should look for:‎

  • At the top you'll see that Has FLASH is 1 - indicating we're using ‎the external SPI Flash storage and that it successfully Mounted ‎Filesystem!
  • It's OK to see Failed to read file/No calibration ‎loaded/found (we haven't made one yet!)
  • Finally, you'll see Calibrations found:
    • Magnetic Hard Offset should default to 0, 0, 0 (no offset)
    • Magnetic Soft Offset should default to 1, 0, 0, 0, 1, 0, 0, ‎‎0, 1 - note that isn't all zeros! It's a 3x3 identity matrix.‎
    • Gyro Zero Rate Offset should default to 0, 0, 0 (no offset)‎
    • Accel Zero Rate Offset should default to 0, 0, 0 (no offset)‎

If you got this far, you're good! Go to the next page where we try to ‎write calibrations.‎

Flash Unformatted Error

There's a chance, if you have a totally fresh board, that the flash is ‎unformatted. In this case, when you upload the calibration reader, ‎you'll get that the JEDEC Chip ID was read (it may vary), and that the ‎flash size was detected - but failed to mount newly formatted filesystem!‎

flash_8

If that happens, you have two ways to format the filesystem.‎

  1. Easiest way (we think) is to install CircuitPython - that's because you ‎don't have to compile anything - simply enter the bootloader by ‎click/double-clicking and dragging over a UF2 file which will ‎format the disk for you.‎‎
  2. Or you can load the SdFat formatter example in the Adafruit ‎SPIFlash library:‎

filesystem_9

Compile, upload and check the serial monitor for instructions.‎

compile_10

Now re-upload/re-try the sensor calibration reading demo.‎

Calibration Write Check

OK now that we have our calibration storage worked out, let’s try ‎writing a calibration to disk!‎

Load up the other example, sensor_calibration_write

You'll see that we first load any existing calibration from non-volatile ‎storage with cal.loadCalibration(). Then we set the calibrations we want to ‎save with:‎

Download File

Copy Code
// in uTesla
cal.mag_hardiron[0] = -3.35;
cal.mag_hardiron[1] = -0.74;
cal.mag_hardiron[2] = -40.79;

// in uTesla
cal.mag_softiron[0] = 0.965;
cal.mag_softiron[1] = 0.018;
cal.mag_softiron[2] = 0.010;
cal.mag_softiron[3] = 0.018;
cal.mag_softiron[4] = 0.960;
cal.mag_softiron[5] = 0.003;
cal.mag_softiron[6] = 0.010;
cal.mag_softiron[7] = 0.003;
cal.mag_softiron[8] = 1.080;

// in Radians/s
cal.gyro_zerorate[0] = 0.05;
cal.gyro_zerorate[1] = -0.01;
cal.gyro_zerorate[2] = -0.01;

which only changes the calibrations in temporary memory. Finally, we ‎run cal.saveCalibration() to write the calibration to permanent storage.‎

Upload this to your board.‎

EEPROM Example

If you use a chip with EEPROM, you'll see similar output from the ‎previous page, this time you will get to see the HEX data stored in ‎EEPROM. We use the same format as PJRC's NXPMotionSense library so ‎you will see 0x75, 0x54 as the first two bytes of the data chunk.‎

eeprom_11

External FLASH example

If you use a chip with external flash, you should see similar output ‎from the previous pre-check, but now it will write the calibration and ‎also print out calibration file for you. You can see that it's stored in ‎JSON format for easy parsing in Python or Arduino!‎

external_12

Reading back calibration

OK no matter which way you calibrated, now you can load the ‎calibration read example to see the saved values loaded up and printed ‎out!‎

For EEPROM:‎

sensors_14

For external FLASH:‎

reading_13

Magnetic Calibration with MotionCal

Calibrating the magnetometer is required to get good orientation data!‎

Before running this example - make sure you have done the calibration ‎pre-check and write check!‎

Paul Stoffregen of PJRC wrote a really awesome cross-platform calibration ‎helper that is great for doing both soft and hard iron magnetometer ‎calibration. What's nice about it is you get a 3D visualization of the ‎magnetometer output, and it also tosses outliers and tells you how ‎much spherical coverage you got!‎

Step 1 - Download MotionCal ‎Software

MotionCal is available for Mac, Windows and Linux, you can download it ‎from clicking here.‎

Look for this section on the website:‎

section_15

And click the one that matches your computer the best.‎

Step 2 - Configure & Upload the ‎AHRS calibration Example

Next, we have to tell the microcontroller board to send the ‎magnetometer (and, if there is one, accelerometer and gyroscope) data ‎out over serial in the right format.‎

Open up the Adafruit_AHRS->calibration example.‎

open_16

At the top of the sketch, you'll see a section where you can #include ‎different sensor sets. Not every sensor-set is defined, but our most ‎popular ones are! (You'll need sensors that are Adafruit_Sensor ‎compatible.)‎

Uncomment whichever kit you are using, and comment out the rest.‎

kit_17

Select your desired board & port from the Tools menu then ‎click Upload.‎

tools_18

Open up the serial console and check that the EEPROM/Filesystem was ‎found. There may already be an existing calibration from prior ‎experiments.

experiments_19

You'll then see a stream of data that looks like:

Raw:-58,-815,8362,76,-121,-95,-375,-159,-24

Uni:-0.07,-0.98,10.00,0.0832,-0.1327,-0.1046,-37.50,-15.93,-2.50‎

The first three numbers are accelerometer data - if you don't have an ‎accelerometer, they will be 0.‎

The middle three numbers are gyroscope data - if you don't have a ‎gyroscope, they will be 0.‎

The last three numbers are magnetometer, they should definitely not ‎be zeros!‎

Step 3 - Run MotionCal

Close the serial port, and launch MotionCal.‎

close_20

Select the same COM/Serial port you used in Arduino.‎

com_21

Twist the board/sensor around. Make sure it’s not near any strong ‎magnets (unless that's part of the installation.)

twist_22

Keep twisting until you get a complete 'sphere' of red dots. At this ‎point you are calibrated!‎

twist_23

In the top right you'll see the hard magnetic offsets at the top, the soft ‎offsets in the middle and the field strength at the bottom.‎

In this case, the hard iron offsets are [-31.25, 35.67, -116.44]

Take a screenshot of this display, so you can refer to these ‎numbers later!‎

MotionCal does not calibrate the accelerometer or gyroscope (yet) - so ‎those offsets will be zero.‎

motion_24

Eventually you'll have enough datapoints that the Send Cal button will ‎activate (its grayed out by default.)

Once you can click the button, try clicking it (we had to try a few ‎times?)‎

click_25

You'll see a large green checkmark once the calibration is saved and ‎verified!

checkmark_26

Step 4 - Verify Calibration

Re-load the sensor_calibration_read sketch to verify the calibration ‎was saved!‎

26a

Sensor Fusion Algorithms

There's 3 algorithms available for sensor fusion. In general, the ‎better the output desired, the more time and memory the ‎fusion takes!‎

Note that no algorithm is perfect - you'll always get some drift and ‎wiggle because these sensors are not that great, but you should be ‎able to get basic orientation data.‎

In order of complexity, they are:‎

Mahony

This basic but effective algorithm will run on smaller chips like the ‎‎'328p which makes it a great one for any platform.‎

The original paper is available here

Madgwick

This algorithm is very popular when you have faster Cortex M0, M3, ‎M4 or faster chips. It isn't going to run on an atmega328p.‎

The original paper is available here

NXP Sensor Fusion

This really nice fusion algorithm was designed by NXP and requires a ‎bit of RAM (so it isn’t for a '328p Arduino) but it has great output ‎results.‎

As described by NXP:

Sensor fusion is a process by which data from several different sensors ‎are fused to compute something more than could be determined by ‎any one sensor alone. An example is computing the orientation of a ‎device in three-dimensional space. That orientation is then used to ‎alter the perspective presented by a 3D GUI or game. ‎

The NXP Sensor Fusion Library for Kinetis MCUs (also referred to as ‎Fusion Library or development kit) provides advanced functions for ‎computation of device orientation, linear acceleration, gyro offset, and ‎magnetic interference based on the outputs of NXP inertial and ‎magnetic sensors.

Version 7.00 of the development kit has the following features:‎

  • Full source code for the sensor fusion libraries
  • IDE-independent software based upon the NXP Kinetis Software ‎Development (KSDK).
  • The Fusion Library no longer requires Processor Expert for ‎component configuration.‎
  • Supports both bare-metal and RTOS-based project development. ‎Library code is now RTOS agnostic.
  • Optional standby mode powers down power-hungry sensors ‎when no motion is detected.‎
  • ‎9-axis Kalman filters require significantly less MIPS to execute
  • All options require significantly less memory than those in the ‎Version 5.xx library.‎
  • Full documentation including user manual and fusion data sheet

The fusion library is supplied under a liberal BSD open-source license, ‎which allows the user to employ this software with NXP MCUs and ‎sensors, or those of our competitors. Support for issues relating to the ‎default distribution running on NXP reference hardware is available via ‎standard NXP support channels. Support for nonstandard platforms ‎and applications is available at ‎https://community.nxp.com/community/sensors/sensorfusion.‎

Let's fuse!‎

OK now that the sensors are calibrated, and you know what the ‎options are for filters - it’s time to FUSE THOSE SENSORS! That's what ‎we're here for, right?‎

Install the Adafruit AHRS library from the library manager. We strongly ‎recommend using Arduino IDE 1.8.10+ because it will automatically ‎install any dependency libraries. See all dependencies here.

install_27

Open up the calibrated_orientation sketch.‎

open_28

At the top of the sketch, you'll see a section where you ‎can #include different sensor sets. Not every sensor-set is defined, but ‎our most popular ones are! (You'll need sensors that ‎are Adafruit_Sensor compatible.)

‎Uncomment whichever kit you are using and comment out the rest.‎

Download File

Copy Code
// uncomment one combo 9-DoF!
#include "LSM6DS_LIS3MDL.h" // can adjust to LSM6DS33, LSM6DS3U, LSM6DSOX...
//#include "LSM9DS.h" // LSM9DS1 or LSM9DS0
//#include "NXP_FXOS_FXAS.h" // NXP 9-DoF breakout

Next, you can select which fusion algorithm you want to try:‎

Download File

Copy Code
// pick your filter! slower == better quality output
//Adafruit_NXPSensorFusion filter; // slowest
Adafruit_Madgwick filter; // faster than NXP
//Adafruit_Mahony filter; // fastest/smalleset

By default, we'll be performing a calculation every 10 ms (100Hz) and ‎printing out 1 out of 10 calculations, however you can adjust those ‎numbers up or down in this section as well as adding debug output‎.

Download File

Copy Code
#define FILTER_UPDATE_RATE_HZ 100
#define PRINT_EVERY_N_UPDATES 10
//#define AHRS_DEBUG_OUTPUT

OK now compile & upload!‎

Open the serial console and you'll see the sensors detected and then ‎text like this.‎

Orientation: 180.82 -1.65 2.48‎

These are the Euler angle outputs from the fusion algorithm.‎

You'll also see text like

Quaternion: 0.7545, 0.2937, 0.5858, -0.0356‎

These are the quaternion outputs.‎

serial_29

Euler Angles

Euler angles describe orientation (in degrees) around a single reference ‎point in three-dimensional space. ‎

Various names are employed for the three angles, but the most ‎common terminology with aircraft is Roll (x), Pitch (y) and Yaw (z). ‎

The illustration below from the Wikipedia article on Euler angles should ‎illustrate the concept clearly. You normally have both positive and ‎negative angles (-180° to 180°) depending on the direction the airplane ‎is tilted, with 0° in every direction corresponding to the airplane being ‎perfectly aligned with each axis:‎

airplane_30

The printout of data is in Yaw (Z) Pitch (Y) Roll (X) order, so if you get

Orientation: 163.00 -4.90 33.56‎

The yaw is 163 degrees, pitch is -4.90 degrees and roll isare about ‎‎33.56 degrees. The sketch will keep updating itself with the latest ‎values at whatever speed we've set in the example sketch.‎

Try twisting the sensor along each axis as printed on the sensor ‎breakout/PCB to see the numbers change from -180~180 for each axis.‎

sensor_31

WebSerial Visualizer

sensors_99

Those three numbers are fine and good, but we want to see what they ‎mean in 3D space, right? Traditionally, a Processing sketch would be ‎used to read the serial data and convert it to a 3D rotation - but thanks ‎to Web Serial API we can use any Chrome browser - a lot easier than installing ‎Processing!‎

Step 1 - Install Chrome

Start by installing the Chrome browser if you haven't yet.‎

Step 2 - Enable Web Serial API if necessary

As of Chrome 89, Web Serial is enabled by default.‎

At the time of this tutorial, you'll need to enable the Serial API, which is ‎really easy.‎

Visit chrome://flags from within Chrome. Find and enable ‎the experimental web platform features.‎

chrome_32

Restart Chrome

Step 3 - Visit the Adafruit 3D Model viewer

In Chrome, ‎visit https://adafruit.github.io/Adafruit_WebSerial_3DModelViewer/‎

Verify you have 115200 Baud selected (it only really matters for non-‎native-serial devices but might as well make sure it’s right.)‎

Click Connect

click_33

When the security window pops up, pick the matching Serial/COM port ‎for your board running the AHRS sketches. Make sure the serial port ‎isn't open in Arduino or something.‎

window_34

You'll see the serial port monitor on the bottom and a 3D bunny on the ‎top. Try rotating and twisting the sensor to see it move!‎

monitor_35

מק"ט יצרן # 5543
ADAFRUIT LSM6DS3TR-C + LIS3MDL -
Adafruit Industries LLC
מק"ט יצרן # 4517
LSM6DSOX + LIS3MDL 9 DOF IMU
Adafruit Industries LLC
מק"ט יצרן # 3387
LSM9DS1 ACCEL/MAG/GYRO/TEMP BRD
Adafruit Industries LLC
מק"ט יצרן # 4438
LSM6DSOX 6 DOF STEMMA QWIIC
Adafruit Industries LLC
מק"ט יצרן # 4479
STEMMA QT MAGNETOMETER LIS3MDL
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.