Maker.io main logo

CLUE BLE MIDI Glove

52

2024-04-19 | By Adafruit Industries

License: See Original Project Displays LCD / TFT Wearables

Courtesy of Adafruit

Guide by John Park

Overview

 

Send wireless MIDI continuous controller (CC) messages over the air ‎to your favorite BLE synthesizer or synth app on iOS or mac os! This ‎project uses the CLUE's built-in accelerometer and proximity sensor ‎to send three different CC signals as you tilt and roll your hand.‎

Use the CLUE's TFT screen, buttons, and touch pads to select ‎different CC numbers, and even pause/restart sending data while ‎maintaining the BLE MIDI connection.‎

You can also change the sound of your synth entirely at the tap of a ‎CLUE touchpad by sending Bank/Preset Program Change messages.‎

Parts

Other Materials

In addition to the parts above you'll also need:‎

  • Glove/mitten/fingerless glove or wrist strap
  • Velcro or other material to adhere the CLUE to the glove/strap

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY flash drive to iterate.‎

The following instructions will show you how to install CircuitPython. ‎If you've already installed CircuitPython but are looking to update it ‎or reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for CLUE from ‎circuitpython.org

Click the link above to download the latest version of ‎CircuitPython for the CLUE.‎

Download and save it to your desktop (or wherever is handy.)‎

download_1

Plug your CLUE into your computer using a known-good USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So, make sure you have a USB cable you know is good ‎for data sync.‎

Double-click the Reset button on the top (magenta arrow) on your ‎board, and you will see the NeoPixel RGB LED (green arrow) turn ‎green. If it turns red, check the USB cable, try another USB port, ‎etc. Note: The little red LED next to the USB connector will pulse red. That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

plug_2

You will see a new disk drive appear called CLUEBOOT.‎

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.‎

drive_3

drive_4

The LED will flash. Then, the CLUEBOOT drive will disappear, and a ‎new disk drive called CIRCUITPY will appear.‎

If this is the first time, you're installing CircuitPython or you're doing ‎a completely fresh install after erasing the filesystem, you will have ‎two files - boot_out.txt, and code.py, and one folder - lib on ‎your CIRCUITPY drive.‎

If CircuitPython was already installed, the files present before ‎reloading CircuitPython should still be present on ‎your CIRCUITPY drive. Loading CircuitPython will not create new ‎files if there was already a CircuitPython filesystem present.‎

That's it, you're done! :)‎

circuitpy_5

Make the CLUE MIDI Glove

Text Editor

Adafruit recommends using the Mu editor for editing your ‎CircuitPython code. You can get more info in this guide.‎

Alternatively, you can use any text editor that saves files.‎

Installing Project Code

To use with CircuitPython, you need to first install a few libraries, into ‎the lib folder on your CIRCUITPY drive. Then you need to ‎update code.py with the example script.‎

Thankfully, we can do this in one go. In the example below, click ‎the Download Project Bundle button below to download the ‎necessary libraries and the code.py file in a zip file. Extract the ‎contents of the zip file, open the ‎directory MIDI_CLUE_BLE_Glove/ and then click on the directory ‎that matches the version of CircuitPython you're using and copy the ‎contents of that directory to your CIRCUITPY drive.‎

Your CIRCUITPY drive should now look similar to the following ‎image:‎

image_6

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

"""
CLUE BLE MIDI
Sends MIDI CC values based on accelerometer x & y and proximity sensor
Touch #0 switches Bank/Preset patches
Touch #1 picks among the three CC lines w A&B buttons adjusting CC numbers
Touch #2 starts/stops sending CC messages (still allows Program Change)
"""
import time
from adafruit_clue import clue
import adafruit_ble
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
import adafruit_ble_midi
import adafruit_midi
from adafruit_midi.control_change import ControlChange
from adafruit_midi.program_change import ProgramChange

# from adafruit_midi.note_on import NoteOn
# from adafruit_midi.pitch_bend import PitchBend
import simpleio
import displayio
import terminalio
from adafruit_display_text import label
from adafruit_display_shapes.rect import Rect

# --- Pick your midi out channel here ---
midi_channel = 1
# --- Pick your MIDI CC numbers here ---
cc_x_num = 71
cc_y_num = 72
cc_prox_num = 73
# --- Pick Bank & Preset pairs here ---
touch_patch = [ # first number is the Bank, second is the Preset
(4, 16), # minimoog: Leads > Original MINI
(5, 8), # Pads > Intergalactic Pass
(0, 13), # Bass > Kraft Bass
(6, 9), # Percussion > Space Hat
]

patch_count = len(touch_patch)
patch_index = (
patch_count - 1
) # start on the last one so first time it is pressed it goes to first

cc_x = 0
cc_y = 0
cc_prox = 0

# Use default HID descriptor
midi_service = adafruit_ble_midi.MIDIService()
advertisement = ProvideServicesAdvertisement(midi_service)

ble = adafruit_ble.BLERadio()
if ble.connected:
for c in ble.connections:
c.disconnect()

midi = adafruit_midi.MIDI(midi_out=midi_service, out_channel=midi_channel - 1)

print("advertising")
ble.name = "CLUE BLE MIDI"
ble.start_advertising(advertisement)

clue.display.brightness = 1.0
clue.pixel.brightness = 0.2
screen = displayio.Group()

ORANGE = 0xCE6136
GRAY = 0x080808
BLACK = 0x121212
BLUE = 0x668190
SILVER = 0xAAAAAA
BROWN = 0x805D40

# --- Setup screen ---
# BG
color_bitmap = displayio.Bitmap(240, 240, 1)
color_palette = displayio.Palette(1)
color_palette[0] = GRAY
bg_sprite = displayio.TileGrid(color_bitmap, x=0, y=0, pixel_shader=color_palette)
screen.append(bg_sprite)
column_a = 20
column_b = 168
# positions that are distributed relative to cc_x and cc_prox y positions
row_a = 80
row_c = 170
row_b = int(row_a + ((row_c - row_a) / 2))
line_row_a = int(row_a + ((row_b - row_a) / 2))
line_row_b = int(row_b + ((row_c - row_b) / 2))
picker_box_row = [row_a, row_b, row_c]

# trim
top_trim_box = Rect(0, 0, 240, 8, fill=BROWN, outline=None)
screen.append(top_trim_box)
bottom_trim_box = Rect(0, 232, 240, 8, fill=BROWN, outline=None)
screen.append(bottom_trim_box)

# title text
title_label = label.Label(terminalio.FONT, text="MIDI CLUE", scale=4, color=SILVER)
title_label.x = 14
title_label.y = 27
screen.append(title_label)

# title box
title_box = Rect(0, 54, 240, 8, fill=BROWN, outline=None)
screen.append(title_box)

# cc x num
cc_x_num_label = label.Label(
terminalio.FONT,
text=("CC {}".format(cc_x_num)),
scale=3,
color=ORANGE,
)
cc_x_num_label.x = column_a
cc_x_num_label.y = row_a
screen.append(cc_x_num_label)

# cc x value
cc_x_label = label.Label(terminalio.FONT, text=str(cc_x), scale=3, color=ORANGE)
cc_x_label.x = column_b
cc_x_label.y = row_a
screen.append(cc_x_label)

# picker box
picker_box = Rect(3, row_a, 6, 6, fill=ORANGE, outline=None)
screen.append(picker_box)

# mid line
mid_line_a = Rect(0, line_row_a, 240, 2, fill=SILVER, outline=None)
screen.append(mid_line_a)

# cc y num
cc_y_num_label = label.Label(
terminalio.FONT, text=("CC {}".format(cc_y_num)), scale=3, color=BLUE
)
cc_y_num_label.x = column_a
cc_y_num_label.y = row_b
screen.append(cc_y_num_label)

# cc y value text
cc_y_label = label.Label(terminalio.FONT, text=str(cc_y), scale=3, color=BLUE)
cc_y_label.x = column_b
cc_y_label.y = row_b
screen.append(cc_y_label)

# mid line
mid_line_b = Rect(0, line_row_b, 240, 2, fill=SILVER, outline=None)
screen.append(mid_line_b)

# cc prox num text
cc_prox_num_label = label.Label(
terminalio.FONT,
text=("CC {}".format(cc_prox_num)),
scale=3,
color=SILVER,
)
cc_prox_num_label.x = column_a
cc_prox_num_label.y = row_c
screen.append(cc_prox_num_label)

# cc prox value text
cc_prox_label = label.Label(terminalio.FONT, text=str(cc_prox), scale=3, color=SILVER)
cc_prox_label.x = column_b
cc_prox_label.y = row_c
screen.append(cc_prox_label)

# footer line
footer_line = Rect(0, 192, 240, 2, fill=SILVER, outline=None)
screen.append(footer_line)


# patch label
patch_label = label.Label(terminalio.FONT, text="Patch _", scale=2, color=BLUE)
patch_label.x = 4
patch_label.y = 216
screen.append(patch_label)

# footer label
footer_label = label.Label(terminalio.FONT, text="connect BLE", scale=2, color=ORANGE)
footer_label.x = 102
footer_label.y = 216
screen.append(footer_label)

# show the screen
clue.display.root_group = screen

cc_num_pick_toggle = 0 # which cc to adjust w buttons
cc_send_toggle = True # to start and stop sending cc

debug = False # set debug mode True to test raw values, set False to run BLE MIDI

while True:
if debug:
accel_data = clue.acceleration # get accelerometer reading
accel_x = accel_data[0]
accel_y = accel_data[1]
prox_data = clue.proximity
print("x:{} y:{}".format(accel_x, accel_y,))
print("proximity: {}".format(clue.proximity))
time.sleep(0.2)

else:
print("Waiting for connection")
while not ble.connected:
pass
print("Connected")
footer_label.x = 80
footer_label.color = BLUE
footer_label.text = "BLE Connected"
time.sleep(2)
footer_label.x = 110
footer_label.color = SILVER
footer_label.text = "sending CC"

while ble.connected:
# Clue sensor readings to CC
accel_data = clue.acceleration # get accelerometer reading
accel_x = accel_data[0]
accel_y = accel_data[1]
prox_data = clue.proximity

# Remap analog readings to cc range
cc_x = int(simpleio.map_range(accel_x, -9, 9, 0, 127))
cc_y = int(simpleio.map_range(accel_y, 0, 9, 0, 127))
cc_prox = int(simpleio.map_range(prox_data, 0, 255, 0, 127))

# send all the midi messages in a list
if cc_send_toggle:
midi.send(
[
ControlChange(cc_x_num, cc_x),
ControlChange(cc_y_num, cc_y),
ControlChange(cc_prox_num, cc_prox),
]
)
cc_x_label.text = str(cc_x)
cc_y_label.text = str(cc_y)
cc_prox_label.text = str(cc_prox)

# If you want to send NoteOn or Pitch Bend, here are examples:
# midi.send(NoteOn(44, 1column_a)) # G sharp 2nd octave
# a_pitch_bend = PitchBend(random.randint(0, 16383))
# midi.send(a_pitch_bend)

if clue.button_a:
if cc_num_pick_toggle == 0:
cc_x_num = cc_x_num - 1
cc_x_num_label.text = "CC {}".format(cc_x_num)
time.sleep(0.05) # Debounce
elif cc_num_pick_toggle == 1:
cc_y_num = cc_y_num - 1
cc_y_num_label.text = "CC {}".format(cc_y_num)
time.sleep(0.05)
else:
cc_prox_num = cc_prox_num - 1
cc_prox_num_label.text = "CC {}".format(cc_prox_num)
time.sleep(0.05)

if clue.button_b:
if cc_num_pick_toggle == 0:
cc_x_num = cc_x_num + 1
cc_x_num_label.text = "CC {}".format(cc_x_num)
time.sleep(0.05)
elif cc_num_pick_toggle == 1:
cc_y_num = cc_y_num + 1
cc_y_num_label.text = "CC {}".format(cc_y_num)
time.sleep(0.05)
else:
cc_prox_num = cc_prox_num + 1
cc_prox_num_label.text = "CC {}".format(cc_prox_num)
time.sleep(0.05)

if clue.touch_0:
patch_index = (patch_index + 1) % patch_count
midi.send( # Bank select
[
ControlChange(0, 0), # MSB
ControlChange(32, touch_patch[patch_index][0]), # LSB
]
)
midi.send(ProgramChange(touch_patch[patch_index][1])) # Program Change
patch_label.text = "Patch {}".format(patch_index + 1)
time.sleep(0.2)

if clue.touch_1:
cc_num_pick_toggle = (cc_num_pick_toggle + 1) % 3
picker_box.y = picker_box_row[cc_num_pick_toggle]
time.sleep(0.1)

if clue.touch_2:
cc_send_toggle = not cc_send_toggle
if cc_send_toggle:
footer_label.x = 110
footer_label.color = SILVER
footer_label.text = "sending CC"
else:
footer_label.x = 114
footer_label.color = ORANGE
footer_label.text = "CC paused"
time.sleep(0.1)

print("Disconnected")
print()
ble.start_advertising(advertisement)

View on GitHub

How It Works

The code does a few key things at startup:‎

  • Import necessary libraries, including ‎the adafruit_ble_midi and adafruit_midi libraries
  • Creates variables to store:‎
    • output MIDI channel (can be set to 1-16)
    • three CC numbers (e.g., CC#1 = modulation)
    • list of MIDI Band/Preset pairs for changing patches
  • Advertises the CLUE BLE MIDI peripheral over BLE so devices ‎can connect to it
  • Uses displayio to lay out the screen text and dividers
  • Checks the two buttons and three touch pads to make any ‎adjustments to variables and UI
  • Waits for a BLE connection

Sending Data

Once a connection has been established between the CLUE and a ‎BLE MIDI device, here's what takes place:‎

  • CLUE accelerometer readings on x- and y-axis are read and ‎remapped using simpleio.map_range() command. Each axis ‎reading ranges from -9 to 9 and needs to re-map to ‎MIDI CC ranges which is 0-127. Depending on how you want to ‎tilt your hand, you can pick and subset of the accelerometer's ‎range per axis
  • CLUE proximity sensor is remapped from 0-255 to 0-127
  • The remapped sensor data is sent as CC data over MIDI
  • Similarly, when the CLUE's touch sensor #0 is pressed, a MIDI ‎message is sent to toggle among the pre-‎selected Bank/Patch pairs. Note, the Bank choice is sent ‎via CC0 and/or CC32 (Most Significant Bit and/or Least ‎Significant Bit for Bank select varies by MIDI device ‎manufacturer). The Patch choice is sent via ProgramChange

CLUE UI

The CLUE's buttons and touch pads act as user inputs to adjust ‎these things:‎

  • Touch #0 toggles between Bank/Preset patches
  • Touch #1 selects between the three CC lines on the screen ‎‎(look for the small dot next to the selected line) to enable ‎adjusting the CC numbers over which to send the sensor data
  • Buttons A and B decrease and increase the MIDI CC number of ‎the selected CC line
  • Touch #2 toggles on/off the sending of CC data (to give your ‎arm a rest!)‎

Build the Glove

Now that the CLUE is coded, you'll want to attach it to a glove back. ‎You can use some double-stick foam tape or adhesive Velcro to ‎attach it, or even a few stitches of strong thread.‎

You can also attach the battery pack the same way, or simply hold it ‎in your hand during use.‎

Use the MIDI Glove

To use the Power Glove MIDI controller with a mac os ‎machine, follow these setup instructions.‎

On iOS devices, you can use the MIDI Wrench app to create and test ‎the BLE MIDI connection, and then use it to "port" the MIDI ‎messages to other apps, such as AudioKit Synth One and Moog ‎Minimoog which you can see in action below:‎

 

Most of these software synths will provide a way to map CC values to ‎any function you like, often with a "MIDI learn" mode as well as ‎explicit number entry.‎

You can also use BLE MIDI with some hardware synthesizers, as well ‎as with BLE MIDI add-on dongles, such as this one from ‎Yamaha which adds BLE MIDI to synths with classic DIN-5 MIDI.‎

מק"ט יצרן # 727
BATTERY HOLDER AAA 3 CELL LEADS
Adafruit Industries LLC
מק"ט יצרן # 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.