Maker.io main logo

Remote Control XRP Robot Through the Internet

1,698

2025-02-14 | By Aswin S Babu

License: Apache License, Version 2.0 Robot Kits Raspberry Pi MCU Raspberry Pi SBC

In the first part of this blog series, XRP Meets Raspberry Pi: Simplifying Robot Control with Flask Server, we explored how to wirelessly control an XRP using a Raspberry Pi powered web server. But why stop at local networks when we can take it global?

In this sequel, we will see how we can use a similar setup to control XRP through the internet remotely. The difference is that this time, we are using a cloud-based (Google Cloud Platform (GCP)) Ubuntu Virtual Machine (VM) to host our Flask web server. This upgrade helps us control the XRP from anywhere around the globe, unlike the previous setup, where the Raspberry Pi's website and thus the XRP itself were only accessible inside the local network. 

What is XRP?

XRP is an open-source robotics platform for students who wish to learn the basics of robot programming. Learning is simpler and effortless on an XRP as it includes access to a free open curriculum developed by Worcester Polytechnic Institute (WPI).


XRP robot

XRP Robot

How does the new approach work?

Here we are using MQTT (Message Queuing Telemetry Transport) to communicate to the Raspberry Pi which is connected to the XRP via USB. The Raspberry Pi connects with the flask webserver using MQTT via a cloud MQTT broker such as hiveMQ. So, when you send a command via the joystick interface on the webserver you created, it first sends an MQTT message to the Raspberry Pi. The RPi then sends these commands to the XRP through the USB interface. Now let's dive deep into the setup.

Prerequisites

Hardware:

- XRP robot

- Raspberry Pi (model 3B+ or newer)

- USB cable for XRP-RPi connection

Software:

- Google Cloud Platform account

- HiveMQ broker account

- Thonny and Geany IDE installed on Raspberry Pi

Now that we have a clear idea of the requirements, let’s get started! First, we’ll configure an MQTT cloud broker, followed by setting up an Ubuntu Virtual Machine (VM) on GCP.


Step 1: Setting up cloud MQTT broker

MQTT is a lightweight Publish-Subscribe (Pub-Sub) protocol developed by IBM. It allows communication over a topic name. Any device that needs to send a message can Publish it over a topic name and whichever device wishes to listen to that message can subscribe to that particular topic.

1.1 Create a hive MQ account using the following URL

HiveMQ

1.11 Click on Start free

HiveMQ account creation page


1.12 Click on Sign Up Free Now

Hivemq account creation page.

1.13 Create an account and choose the serverless option

Hivemq account creation page.

1.14 Configuring the login credentials

Click on Manage cluster > Access management to set up login credentials.

Hivemq configuration page.

   

Hivemq configuration page.

   

1.141 Setup username and password

Grant publish and subscribe permissions, then click Save. The publish permission allows sending messages to a specified topic, while the subscribe permission enables receiving messages from that topic.

Hivemq configuration page.

   

1.15 Copy the connection details

Take note of the connection details such as URL, port, username and password you set above for future use.

Step 2: Setting up VM on Google Cloud

2.1 Creating a Virtual Machine (VM instance)

We need to create an Ubuntu virtual machine, where we will be running the flask server. Use the Google cloud platform to create an Ubuntu virtual machine. At the website follow the following steps to reach the VM creation window.

Click on VM instances> enable compute engine API > enable billing> create billing account > manage billing account > create account.


Then continue with VM creation.

2.11 Specify an instance name and region

Google Cloud VM configuration page.

2.12 Under the general-purpose option choose the E2 series

Google Cloud VM configuration page.

2.13 Choose the Ubuntu OS

Google Cloud VM configuration page.


Google Cloud VM configuration page.

2.14 Enable HTTP and HTTPS

Go with the default setup elsewhere but enable HTTP and HTTPS under the firewall option.

Then press the create button to finish the VM creation.

Google Cloud VM configuration page.

2.2 Access VM 

Press the SSH button and then press Authorize, this will lead you to the Command Line interface of the Ubuntu instance created. Log into the instance using the credentials specified before.

VM access page

VM command line interface


Step 3:  Setting Up Flask server on google cloud

Now that we have SSH access to the Ubuntu VM we can install the MQTT library for communications. Here we are using the paho mqtt library on the Google Cloud. Additionally, we also need to install the Flask web framework.

3.1 Installing various libraries

We require Python and Python package manager (pip) libraries for this project. Run the following commands on the VM to install them.

3.11 Commands to install Python and Pip

Enter the following commands to install Python and then pip. pip is the standard package manager for Python. We can use pip to install various Python libraries as shown below.

Copy Code
sudo apt-get update

sudo apt install python3 python3-pip -y

3.12 Commands to install MQTT and Flask

Enter the following commands to install MQTT and Flask libraries

Copy Code
pip install paho-mqtt

sudo pip3 install flask

3.2 Flask server code

3.21 Create a Python file

Create a file with some name, say flaskServer.py

Copy Code
nano flaskServer.py

Copy the below code to the file you created and then save it (press Ctrl+X )

Github code link

3.22 Update the MQTT credentials in the code

Modify the following MQTT credentials in the code by looking at the hiveMQ connection you set up in step 1

MQTT credentials that need to be modified in the code.

 Step 4: Programming the XRP and Raspberry Pi

Similar to our previous project on the XRP, we are using USB communication, again in this project as well. So, we need to program both the XRP robot as well as the Raspberry Pi which is connected to the XRP via USB. Raspberry Pi receives the control commands from the user via the Flask website and MQTT broker. 

Control commands are published under a topic name from the flask server and the Raspberry Pi is subscribed to that topic. Thus, it receives the commands and then sends them to the XRP (RPi Pico) through the USB interface between them.

4.1 Raspberry Pi programming

Follow step 3 of the first part of this project to see how you can set up the Raspberry Pi and access its Graphical User Interface (GUI ) using a VNC tool like MobaXterm. Once you have logged into the Pi by using Mobaxterm or any other VNC tool, use any programming IDE such as 'Geany' to create a Python file say ‘RPi.py’ and then then copy the below code and save the file.

Github code link

Let’s look at the RPi side code.

The code is intended to:

  1. Receive MQTT messages from a broker.

  2. Forward commands via USB serial to the connected Raspberry Pi Pico.

  3. Provide a bridge between an MQTT communication channel and a serially connected microcontroller (XRP).

4.2 XRP Programming

Now we need to program our XRP. You can follow this link for assistance. You may use any method to program your XRP. Here we are using Thonny IDE to program XRP. Follow the link for more details. Programming XRP Robot Using Thonny. Let's create a file named XRP.py and copy the following code.

Github code link

The code is designed to:

  1. Control the movement of an XRP robot based on incoming commands (F, B, L, R).

  2. Read commands from the RPi.

  3. Execute robot motions by setting appropriate drive efforts for forward, backward, left, and right movements.

XRP Robot connected to Raspberry Pi via USB

XRP Robot connected to Raspberry Pi via USB

4.3 Running the programs.

As we have finished with the programming part, we can run the programs one by one.

4.31 Running Flask server code

Let's begin by running the flask server code on the Ubuntu VM. Follow step 2.2 to access the Ubuntu virtual machine and run the flask server code (flaskServer.py) we created in step 3.21. In order to do this, run the following command on the same path as the code file.

Copy Code
sudo python3 flaskServer.py

Note: To verify the folder path, you can type 'pwd' (print working directory) on the command line interface. Also 'ls' will list all the files in the current path.

To access the created web server, use the external IP address mentioned on the Google VM instance page.

Note: Try to use http instead of https. For instance, here it will be http://34.95.x.x/

VM instance page on Google Cloud Platform

VM instance selection page on Google Cloud Platform.

If everything is ok, you should be seeing a joystick interface as below.

XRP joystick image

Joystick interface created.

4.32 Running XRP code

After making sure that the XRP is connected to the RPi, use Thonny IDE to run the XRP.py file we created in step 4.2.

4.33 Running Raspberry Pi code

Connect the XRP to the RPI and run the RPI.py file we created using the Geany IDE. You should be able to see messages indicating a USB connection with XRP.

5 Controlling the XRP robot over the internet

We came to the final step in the project here. Now we can control our XRP from anywhere around the globe via the internet. Have fun playing with the joystick to remotely control your XRP. Happy Coding!

מק"ט יצרן # 22296
XRP ROBOTICS PLATFORM KIT BETA (
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.