Maker.io main logo

RGB LCD Shield

157

2025-02-04 | By Adafruit Industries

License: See Original Project LCD / TFT Arduino

Courtesy of Adafruit

Guide by Lady Ada

Overview

adafruit_products_arduino_compatibles_715-04

This new Adafruit shield makes it easy to use a 16x2 Character LCD. ‎We really like the range of LCDs we stock in the shop, such as our ‎classic blue & white as well as the fancy RGB negative and RGB ‎positive.‎

Unfortunately, these LCDs do require quite a few digital pins, 6 to ‎control the LCD and then perhaps another 3 to control the RGB ‎backlight for a total of 9 pins. That's half of the pins available on a ‎classic Arduino!‎

arduino_1

With this in mind, we wanted to make it easier for people to get ‎these LCD into their projects. So, we devised a shield that lets you ‎control a 16x2 Character LCD, up to 3 backlight pins AND 5 keypad ‎pins using only the two I2C pins on the Arduino! The best part is ‎you don't really lose those two pins either, since you can use I2C-‎based sensors, real-time clocks, etc. and have them share the I2C ‎bus. This is a super slick way to add a display without all the wiring ‎hassle.‎

shield_2

This shield is perfect for when you want to build a stand-alone ‎project with its own user interface. The 4 directional buttons plus ‎select button allows basic control without having to attach a bulky ‎computer.‎

shield_3

The shield is designed for 'classic' Arduino-shaped boards such as ‎the Uno, Metro, etc. But it will also fit "Mega" sized boards because ‎the I2C pins are labeled SCL/SDA.‎

This used to come as a kit but now comes as an assembled SMT ‎design, so much less soldering is required.‎

assembled_3

Revision History:‎

  • As of May 29, 2024 – The PCB's design has been updated. Now ‎it comes with the buttons, chips and other components ‎already soldered into place. You will still need to solder on the ‎shield headers and the LCD, but it's a lot easier.‎

Text editor powered by tinymce.‎

Parts List

As of May 29, 2024 – The PCB's design has been updated. Now it ‎comes with the buttons, chips and other components already ‎soldered into place. You will still need to solder on the shield headers ‎and the LCD, but it's a lot easier.‎

Rev B:‎

The shield comes with the board and headers. All other parts are ‎already soldered on for your convenience!‎

revB_4

Rev A:‎

Check to make sure your kit comes with all the parts. Sometimes we ‎make mistakes so double check everything and ‎email support@adafruit.com if you need replacements!‎

revA_5

‎1) Resistors‎

There is a total of 5 resistors in this kit. For resistors labeled R1 and R2 ‎on the PCB, they are 1/4W 5% 4.7K resistors (Yellow, Violet Red, Gold). ‎For resistors labeled RED and BLUE on the PCB, they are 1/4W 5% ‎‎220-ohm resistors (Red, Red, Brown, Gold). For the resistor labeled ‎GREEN on the PCB, it is a 1/4W 5% 330-ohm resistor (Orange Orange ‎Brown Gold).‎

‎2) Potentiometer‎

There is one 10k trim potentiometer. This part will go in the spot ‎labeled Contrast, near the RESET button. Note: The pot may be blue ‎instead of orange.‎

‎3) Pushbuttons‎

There is a total of 6, 6mm tactile switch pushbuttons. These will be ‎used in the UP, DOWN, LEFT, RIGHT, SELECT, and RESET locations on ‎the PCB.‎

‎4) i2c Port Expander Chip‎

There is one of these MCP23017 i2c (16 input/output) port expander ‎chips in the kit. This is how we are able to only use 2 Arduino pins to ‎run the entire LCD and buttons. Click here for more info on this chip.‎

‎5) Male Header Pins‎

There are two strips of 36 male header pins in the kit. These will be ‎used to attach the shield to the Arduino, as well as attach the LCD to ‎the PCB.‎

‎6) Printed Circuit Board‎

There will be one PCB in the kit as shown above.‎

printed_6

Additional

You'll want an LCD to place into the shield. This isn't included by ‎default since a lot of people already have LCDs they may want to use. ‎‎(We do sell these in packs however, so chances are you did get an ‎LCD with your order.)‎

You can also use 16x2 LCDs or even OLEDs that are the same size ‎that do not have an RGB backlight or have no backlight at all.‎

We carry Negative type or Positive type LCDs.‎

Text editor powered by tinymce.‎

Assembly

As of May 29, 2024, the shield comes with the buttons, chips and ‎other components already soldered into place. You can skip ahead to ‎the Headers section if you have this new version.‎

Check the kit against the parts list to verify you have all the parts ‎necessary.

kit_7

Put the printed circuit board into a vise or board holder, heat up your ‎soldering iron and make sure you are ready to go!‎

board_8

Resistors

We'll start with the first resistor R1 - which has yellow, violet, red, gold ‎bands on it. This resistor is part of the interface between the Arduino ‎and the 'port expander' that controls the LCD.

‎Bend the resistor into a 'staple' and slide it into the slot marked R1 on ‎the PCB. Resistors do not have a direction so you can put it in 'either ‎way' and it'll work fine.‎

bend_9

Bend the 'legs' of the resistor out so it sits flat against the PCB and ‎flip it over.‎

This way the resistor won't fall out while soldering.‎

fall_10

With your soldering iron heated up and ready, solder in both leads of ‎the resistor. To do this, heat up the round ring pad and the wire lead ‎at the same time for 2 or 3 seconds, then dip the end of the solder ‎into the heated joint to melt it in.‎

Then remove the solder and the soldering iron.‎

soldering_11

soldering_12

Once the soldering is complete, we can clean up by clipping the ‎leads of the resistor. This keeps them from shorting to something ‎else. Use diagonal or flush cutters to clip the wires right above where ‎the solder joint ends.‎

joint_13

Since you did so great with the first resistor, we'll place all of the rest ‎now at the same time. R2 is a 4.7K resistor just like R1 (Yellow, Violet, ‎Red Gold) so place that one first.

Next you can do the two 220-ohm resistors RED and BLUE - named ‎because they are the backlight series resistors for the RGB ‎backlights on the LCDs. These resistors are colored Red Red Brown ‎Gold. They look very similar to the 330-ohm resistor so check ‎carefully that you have the red-band ones. Use a multimeter if you ‎can to verify the resistance!‎

Finally, place the remaining 330-ohm resistor (Orange, Orange, ‎Brown, Gold) into the GREEN spot. The green LED is might brighter ‎than the red or blue in the RGB backlight, so a larger resistor is ‎required to balance it out.‎

place_14

Make sure the resistors all sit nice and flat against the PCB.‎

resistors_15

Solder the resistors just like you did with the first one.‎

solder_16

Clip all the leads.

clip_17

clip_18

Buttons

Next up we will place the buttons. These buttons are useful to send a ‎signal to the Arduino (say if you have a basic menu system). We ‎have a 4-way 'direction pad' for up/down/left/right input and a ‎button to the right called SELECT. These 5 buttons should be able to ‎make 'talking' back to your project easy. These are connected to the ‎I2C port expander chip, so they require no extra pins on the Arduino, ‎our library does the work of reading whether they are pressed.‎

The button all the way to the right is the RESET button, for when you ‎want to reset the entire system.‎

All the buttons are the same, and they should snap nicely into place. ‎Press down onto each button until it snaps in and sits flat against ‎the PCB.‎

buttons_19

buttons_20

Flip over the PCB and check that all the legs for the buttons are ‎sticking out.‎

flip_21

Solder each leg, taking care not to accidentally 'short' two button ‎legs together. The ones for the directional pads are very close!‎

leg_22

leg_23

MCP23017 and Potentiometer

We're nearly done! Now we will place the I2C port expander chip. ‎Double check that it has the MCP23017-E/SP marking on it. This is a ‎‎16-pin expander chip, which uses the i2c bus. That means you can ‎send it commands using the i2c pins on an Arduino and control 16 ‎more digital pins! 5 of those pins go to the buttons, 6 go to the LCD ‎control and 3 are used for the backlight (the remaining 2 are unused).‎

Unlike buttons or resistors, chips do have a direction and the must ‎be put in the right way! First, use a flat table to carefully bend the ‎legs of the chip so they are parallel. Then slip it into the silkscreened ‎outline so that the notch at the end of the chip is on the right. Click ‎the image to the left to make absolutely sure you've got it in the ‎right way. Once you are sure, press the chip into place.‎

Next, place the 10K potentiometer (the orange-faced thing with ‎three legs) into the spot above the RESET button. It will only fit one ‎way. This is the contrast potentiometer which will adjust how dark ‎the characters appear. All displays are slightly different, so you'll ‎adjust this once the display is soldered in.‎

The kit may come with two potentiometers - a big blue one for ‎breadboarding the LCD and a smaller orange one for the shield kit. ‎You can throw away or recycle the blue one, use only the orange ‎one here!‎

shield_24

shield_25

Flip over the PCB and solder in the three legs of the potentiometer ‎and then all 28 pins of the port expander.‎

flip_26

flip_27

flip_28

Headers

The steps here on out apply both to the older kit shield and the ‎newest shield.‎

Take a stick of 36 pin header and break off a 10-pin piece, an 8 pin ‎piece and two 6 pin pieces.‎

headers_29

Place the header onto your Arduino, if you have an R2 or earlier ‎Arduino, there will be two pins that 'hang over' past the AREF ‎breakout. These two extra pins are used for R3 and later Arduino ‎classics and Mega's to make connecting to the I2C pins easier. We ‎suggest keeping those two pins in case you ever upgrade your ‎‎'duino.‎

pins_30

Place the shield right on top. It should fit perfectly where all the short ‎ends of the header fit into the holes of the shield.‎

To make it sit flat, you may need to clip the legs of the buttons down ‎‎- they will interfere with the DC jack, lifting the shield a bit.‎

flat_31

flat_32

Solder all of the header pins. Even though they aren't used for ‎passing signals, they will make the mechanical connection to the ‎Arduino strong.‎

connection_33

connection_34

connection_35

RGB LCD

Next, check if you have an RGB LCD (with 18 pins) or a Monochrome ‎display (not RGB, with 16 pins).‎

If you have a RGB 18 pin display break off an 18-pin strip of header ‎and place it with the long ends down into the LCD placement slot.‎

If you have a Monochrome 16 pin display break off a 16-pin strip of ‎header and place it with the long ends down into the LCD ‎placement slot so that the two right-most pins are empty.‎

empty_36

Now you can take the 16x2 LCD of your choosing and place it on top. ‎For the RGB LCDs we stock, there are two connection rows, just ‎make sure it matches the outline silkscreen on the shield and you ‎should be good to go.‎

If your LCD does not have an RGB backlight or it has no backlight, ‎you may have to shorten the length of header (see the previous ‎step) until it matches and make sure the LCD fits over the ‎silkscreen outline.‎

If you already soldered all 18 pins but you have a 16 or 14 pin LCD, ‎simply cut off the right-most pin tops until it fits.‎

fits_37

Solder all the pins to the LCD display.‎

lcd_38

Flip over the shield and place it flat on the table so the long leads of ‎the header stick out.‎

Solder each of the header legs.‎

legs_38

legs_39

legs_40

Finish up by carefully clipping the leads. For some Arduinos, the long ‎leads may interfere with headers or parts on the Arduino board, so ‎we suggest just clipping them all. Do it carefully as these are a little ‎difficult to cut and may fly at you. We suggest doing it over a trash ‎can.‎

finish_41

finish_42

You're done!‎

Check out the next page for how to use the shield and libraries.‎

page_44

page_43

Text editor powered by tinymce.‎

Arduino Usage

The shield is really easy to use. Once you have attached the LCD of ‎choice, plug it onto the Arduino and download our library from ‎GitHub. The example included shows how to use the RGB backlight ‎control and reading from the keypad.‎

Download the Library

To interface with the LCD and buttons you must use our library ‎which translates the commands through the port expander.

Open up the Arduino library manager:‎

interface_45

Search for the Adafruit RGB LCD Shield library and install it.

search_46

We also have a great tutorial on Arduino library installation at:

http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-‎use

Adjusting Contrast

The shield uses a character LCD with an external contrast ‎potentiometer. The first time you use it, adjust the potentiometer in ‎the bottom right until you see the text clearly. If you don't upload ‎code to the Arduino, some boxes will appear instead.

If you don't see any text on the LCD, be sure to try twisting the ‎orange contrast potentiometer until the text appears. You may have ‎to turn it all the way around from one side to the other until you see ‎text.

Shared Pins

The I2C pins are shared with other pins, and each Arduino type ‎has a different sharing scheme. Those pins cannot be used for ‎anything else than I2C when this shield is used!

Uno/Duemilanove/Diecimila - I2C pins are also the same pins ‎as Analog 4 and Analog 5

Mega 1280 and 2560 - I2C pins are also the same pins as Digital ‎‎20 and 21

Leonardo and other 32u4-based - I2C pins are also the same pins ‎as Digital 2 and 3‎

Writing Your Own Sketches

The Adafruit_RGBLCDShield library is a derivative of ‎the LiquidCrystal library that comes with Arduino so you can call any ‎of the functions that you're used to, and they'll work just the same.‎

There are two extra functions you may want to use. One ‎is lcd.setBacklight(color); which will change the backlight color ‎assuming you have an RGB LCD on. At this time, the library does not ‎do any PWM on the RGB backlight, so you can select from 8 ‎different colors (including OFF) - if you place these #define's at the ‎top of your sketch you can simply call whichever color you want to ‎appear.‎

Download File

Copy Code
// These #defines make it easy to set the backlight color
#define OFF 0x0
#define RED 0x1
#define YELLOW 0x3
#define GREEN 0x2
#define TEAL 0x6
#define BLUE 0x4
#define VIOLET 0x5
#define WHITE 0x7 

‎Another extra of the shield is a 4-way directional keypad plus select ‎button. This will let you design your own control interface for 'stand-‎alone' Arduino projects. All the buttons are read at once when you ‎call lcd.readButtons(); which returns a variable that has individual ‎bits set for the buttons. You can easily test for which buttons were ‎held down at the time of the readButtons() call by using bitwise & as ‎seen in this code snippet.

‎Note that the library handles button debouncing internally. There ‎is no need to debounce the buttons in your code.‎

Download File

Copy Code
uint8_t buttons = lcd.readButtons();

  if (buttons) {
    if (buttons & BUTTON_UP) {
      lcd.setBacklight(RED);
    }
    if (buttons & BUTTON_DOWN) {
      lcd.setBacklight(YELLOW);
    }
    if (buttons & BUTTON_LEFT) {
      lcd.setBacklight(GREEN);
    }
    if (buttons & BUTTON_RIGHT) {
      lcd.setBacklight(TEAL);
    }
    if (buttons & BUTTON_SELECT) {
      lcd.setBacklight(VIOLET);
    }
  }

Using with Monochrome Displays

Displays with monochrome backlights are controlled by the RED pin ‎and will only respond to colors that have RED in them (RED, ‎YELLOW, VIOLET). For these displays, you can use ON and OFF ‎instead as in the snippet below:‎

Download File

Copy Code
uint8_t buttons = lcd.readButtons();

  if (buttons) {
    lcd.clear();
    lcd.setCursor(0,0);
    if (buttons & BUTTON_UP) {
      lcd.print("UP ");
      lcd.setBacklight(HIGH);
    }
    if (buttons & BUTTON_DOWN) {
      lcd.print("DOWN ");
      lcd.setBacklight(LOW);
    }

Detached Usage

If you want to have the shield disconnected from the Arduino (say to ‎panel mount it) or if you want to use it with a different type of ‎processor board, it’s very easy!‎

Just power the 5V pin with 5V, common ground to GND and then ‎connect the SCL labeled pin (top left) to I2C clock and SDA to I2C ‎data. Those are the only four wires you need to control the entire ‎shield.‎

  • On Uno-shaped Arduinos, SCL is also connected to Analog 5 ‎and SDA is connected to Analog 4.‎

  • On Mega Arduinos, SCL is also connected to Digital 21 ‎and SDA is connected to Digital 20.‎

  • On Leonardo Arduinos, SCL is also connected to Digital 3 ‎and SDA is connected to Digital 2.‎

Important: Wire +5V and GND to the shield pins shown in the ‎pictures! The GND pin next to the 5v pin is NOT connected. You must ‎use the one next to the VIN pin!‎

If you plan on using the reset button, you will need to attach a fifth ‎wire between the Arduino’s reset pin and the corresponding reset ‎pin on the shield.‎

diagram_47

Text editor powered by tinymce.‎

CircuitPython Usage

It's easy to use the RGB character LCD shield with CircuitPython and ‎the Adafruit CircuitPython CharLCD library. This library allows you to ‎easily write Python code that controls the RGB character LCD.‎

CircuitPython Microcontroller ‎Wiring

Assemble the shield kit as shown in the previous pages. Then, attach ‎it to a Metro M0 or Metro M4. It's that simple!‎

CircuitPython Installation of ‎CharLCD Library

You'll need to install the Adafruit CircuitPython CharLCD library on ‎your CircuitPython board.‎

First make sure you are running the latest version of Adafruit ‎CircuitPython for your board.‎

Next you'll need to install the necessary libraries to use the ‎hardware--carefully follow the steps to find and install these libraries ‎from Adafruit's CircuitPython library bundle. Our CircuitPython ‎starter guide has a great page on how to install the library bundle.‎

If you choose, you may manually install the libraries from the bundle:‎

  • adafruit_character_lcd

  • adafruit_mcp230xx

  • adafruit_bus_device

Before continuing make sure your board's lib folder or root ‎filesystem has the adafruit_character_lcd, ‎adafruit_mcp230xx, and adafruit_bus_device files and ‎folders copied over.‎

Next connect to the board's serial REPL so you are at the ‎CircuitPython >>> prompt.‎

CircuitPython Code

To demonstrate the usage of the character LCD we'll initialize it and ‎display text using CircuitPython code.‎

First, you'll need to import necessary modules, initialize the I2C bus, ‎and create an instance of the character LCD class. Paste the ‎following code into your REPL:‎

Download File

Copy Code
import board
import busio
import adafruit_character_lcd.character_lcd_rgb_i2c as character_lcd
lcd_columns = 16
lcd_rows = 2
i2c = busio.I2C(board.SCL, board.SDA)
lcd = character_lcd.Character_LCD_RGB_I2C(i2c, lcd_columns, lcd_rows)

‎Now you're ready to start writing text and characters on the ‎display! The usage of the LCD class is exactly the same as shown in ‎the parallel LCD wiring guide. Be sure to check out that guide for a ‎complete discussion of LCD usage.‎

As a quick test though you can run the following code to use ‎the color property to set the backlight to red and ‎the message property to write text to the display:‎

Download File

Copy Code
lcd.color = [100, 0, 0]
lcd.message = "Hello\nCircuitPython"

display_48

See the parallel LCD guide for more functions you can call to control ‎the LCD!‎

That's all there is to using the RGB character LCD shield kit with ‎CircuitPython!‎

Full Code Example

Copy the following example to code.py on your board and see a ‎demo of some of the different things the character LCD library has to ‎offer!‎

‎Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 ladyada for Adafruit Industries
# SPDX-License-Identifier: MIT

"""Simple test for I2C RGB character LCD shield kit"""
import time
import board
import adafruit_character_lcd.character_lcd_rgb_i2c as character_lcd

# Modify this if you have a different sized Character LCD
lcd_columns = 16
lcd_rows = 2

# Initialise I2C bus.
i2c = board.I2C()  # uses board.SCL and board.SDA
# i2c = board.STEMMA_I2C()  # For using the built-in STEMMA QT connector on a microcontroller

# Initialise the LCD class
lcd = character_lcd.Character_LCD_RGB_I2C(i2c, lcd_columns, lcd_rows)

lcd.clear()
# Set LCD color to red
lcd.color = [100, 0, 0]
time.sleep(1)
# Print two line message
lcd.message = "Hello\nCircuitPython"
# Wait 5s
time.sleep(5)
# Set LCD color to blue
lcd.color = [0, 100, 0]
time.sleep(1)
# Set LCD color to green
lcd.color = [0, 0, 100]
time.sleep(1)
# Set LCD color to purple
lcd.color = [50, 0, 50]
time.sleep(1)
lcd.clear()
# Print two line message right to left
lcd.text_direction = lcd.RIGHT_TO_LEFT
lcd.message = "Hello\nCircuitPython"
# Wait 5s
time.sleep(5)
# Return text direction to left to right
lcd.text_direction = lcd.LEFT_TO_RIGHT
# Display cursor
lcd.clear()
lcd.cursor = True
lcd.message = "Cursor! "
# Wait 5s
time.sleep(5)
# Display blinking cursor
lcd.clear()
lcd.blink = True
lcd.message = "Blinky Cursor!"
# Wait 5s
time.sleep(5)
lcd.blink = False
lcd.clear()
# Create message to scroll
scroll_msg = "<-- Scroll"
lcd.message = scroll_msg
# Scroll to the left
for i in range(len(scroll_msg)):
    time.sleep(0.5)
    lcd.move_left()
lcd.clear()
time.sleep(1)
lcd.message = "Going to sleep\nCya later!"
time.sleep(5)
# Turn off LCD backlights and clear text
lcd.color = [0, 0, 0]
lcd.clear()

View on GitHub

Text editor powered by tinymce.‎

F.A.Q.‎

I have a monochrome display and some of the buttons ‎don't work.‎

The monochrome display only responds to backlight colors with RED ‎in them. Use "ON" and "OFF" instead. See the code snippet ‎under "Using with Monochrome Displays."‎

What pins are used? What pins are available?‎

The shield uses only the SCL and SDA I2C pins, and 5V power and ‎ground. You can use the I2C pins for other I2C sensors/devices as ‎long as they do not share the same address. If you are using an ‎Arduino UNO, Analog 4 and Analog 5 are shared with SCL/SDA so ‎you can't use them. Likewise, Arduino Leonardo share SCL/SDA ‎with Digital 2 & Digital 3 so those would not be available.‎

I'm trying to compile and I'm getting error messages ‎like "No such file or directory" or "does not name a type".

If you're seeing error messages that look like any (or all) of the ‎following, it means that the Arduino IDE is not finding the Adafruit ‎libraries.

o error: Adafruit_MCP23017.h: No such file or directory
o error: Adafruit_RGBLCDShield.h: No such file or directory
o error: 'Adafruit_RGBLCDShield' does not name a type
o error: 'lcd' was not declared in this scope
o error: 'BUTTON_UP' was not declared in this scope
o error: 'BUTTON_DOWN' was not declared in this scope
o error: 'BUTTON_LEFT' was not declared in this scope
o error: 'BUTTON_RIGHT' was not declared in this scope
o error: 'BUTTON_SELECT' was not declared in this scope

‎There are three possible causes for this:

‎1. You didn't download the library folder.‎
Adafruit has written some extra software to make it easy to use your ‎shield. This software is contained in a library folder that you can ‎download here:‎
https://github.com/adafruit/Adafruit-RGB-LCD-Shield-Library
You download the folder by clicking on the Downloads button in the ‎top right. You will have the option of downloading the library in one ‎of two compressed formats: '.zip' or '.tar.gz'. Windows and Mac users ‎will probably want to select .zip, while Linux users may prefer .tar.gz.
MacOS will automatically uncompress the downloaded file into a ‎folder, which you should find in the Downloads folder.
Windows users can double-click on the downloaded file. This will ‎open an Explorer window which will allow you to extract the ‎compressed library folder.‎
(Continue to the next paragraph to find out what to do with the ‎uncompressed download)‎
‎2. The library folder has the wrong name.
After downloading and uncompressing the library folder, ‎you must change the name of the folder ‎to exactly "Adafruit_RGBLCDShield". Don't abbreviate, add any ‎spaces, underscores or other characters. Make sure the capitalization ‎is the same as shown here.‎
‎(Continue to the next paragraph to find out where to put the library ‎folder)‎
‎3. The library folder is in the wrong place.
When you installed your Arduino IDE, it created a 'sketch folder' for ‎you (if you don't already know where that sketch folder is, go into the ‎Arduino application's 'Sketch' menu, and select 'Show Sketch ‎Folder').
Inside of the sketch folder, there should be another folder called ‎‎'libraries'. If not, create a new folder inside of the sketch folder, and ‎name it "libraries" (the name must be exactly "libraries" - not ‎‎"library" or "librarys" - not even "Libraries" with a capital 'L' ! ).
‎Move your new Adafruit_RGBLCDShield folder into this libraries ‎folder.

Once you've made sure the folder has the right name and is in the ‎right place, you have to close and reopen the Arduino IDE, so that it ‎will recognize the new library.

‎if you're curious, you can learn more about libraries here:

http://learn.adafruit.com/arduino-tips-tricks-and-techniques/arduino-‎libraries

Does the shield do the button de-bounce logic ‎internally, or do I need to do that in software when ‎reading the buttons?‎

The Adafruit_RGBLCDShield library handles button debouncing for ‎you, when you use the readButtons() function.‎

Is this compatible with my Arduino? There are two extra ‎pins on the header that don't plug into anything.‎

The shield will work fine with older Arduino boards. Extra pins were ‎added to the R3 version of the Uno and Mega. These are duplicates ‎of other header pins and are not required for proper operation of the ‎shield. ‎

Does this work with the Raspberry Pi?‎

At this time, it does not! This shield is for Arduinos only!‎

I am using this detached from the Arduino and it ‎doesn't seem to be getting any power.‎

Only the ground pin next to the VIN pin is used. You need to connect ‎your ground wire to this pin.‎

Can I use this with 20x4 LCDs?‎

Technically, yes. The pinouts for 20x4 and 16x2 are identical. However, ‎the screen is way bigger, and it covers the buttons up, so we don't ‎suggest it.‎

Text editor powered by tinymce.‎

Downloads

Files

Schematic and Fab Print

Rev B

dimensions_49

dimensions_50

Rev A

dimensions_51

dimensions_52

Text editor powered by tinymce.

220UF 16V ELECTROLYTIC CAPACITOR
מק"ט יצרן # 2192
220UF 16V ELECTROLYTIC CAPACITOR
Adafruit Industries LLC
מק"ט יצרן # 1506
ADDRESS LED STRIP SERIAL RGB 1M
Adafruit Industries LLC
מק"ט יצרן # 772
LCD SHIELD KIT 16X2 DIPLAY BLU
Adafruit Industries LLC
מק"ט יצרן # 716
RGB LCD SHIELD KIT 16X2 DISPLAY
Adafruit Industries LLC
מק"ט יצרן # 714
RGB LCD 16X2 CHAR DISPLAY SHIELD
Adafruit Industries LLC
16MM PANEL MOUNT MOMENTARY PUSHB
מק"ט יצרן # 1502
16MM PANEL MOUNT MOMENTARY PUSHB
Adafruit Industries LLC
מק"ט יצרן # MCP23017T-E/SO
IC XPNDR 1.7MHZ I2C 28SOIC
Microchip Technology
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.