Maker.io main logo

SparkFun Triple Axis Accelerometer Breakout-BMA400 (Qwiic) Hookup Guide

130

2025-04-08 | By SparkFun Electronics

License: See Original Project Acceleration Movement Arduino Qwiic

Courtesy of SparkFun

Guide by El Duderino

Introduction

The SparkFun Triple Axis Accelerometer Breakout - BMA400 (Qwiic) (Standard and Micro) ‎offer a 3-axis acceleration sensor perfect for ultra-low power applications on a easy to use ‎Qwiic breakout boards. The Qwiic system allows for integration into your I2C system with ‎no soldering required. The standard size Qwiic breakout also includes 0.1"-spaced PTH ‎pins connected to the sensor's communication interface and interrupt pins for applications ‎that require a traditional soldered connection.‎

The BMA400 from Bosch Sensortech© has a full-scale acceleration range of ±2/±4/±8/±16g ‎with exceptionally low current consumption of < 14.5µA while operating at its highest ‎performance settings. The sensor also includes a complete feature set for on-chip ‎interrupts including step counter, activity recognition, orientation detection and tap/double ‎tap.‎

This guide will go into detail on the features of the BMA400 and hardware on these boards ‎as well as how to integrate it into a Qwiic circuit using the SparkFun BMA400 Arduino ‎Library.‎

Required Materials

To follow along with this guide, you will need a microcontroller to communicate with the ‎BMA400. Below are a few options that come Qwiic-enabled out of the box:‎

If your chosen microcontroller is not already Qwiic-enabled, you can add that functionality ‎with one or more of the following items:‎

You will also need at least one Qwiic cable to connect your sensor to your microcontroller.‎

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

qwiic_1

We also recommend taking a look at the following tutorials if you aren't familiar with the ‎concepts covered in them. If you are using one of the Qwiic Shields listed above, you may ‎want to read through their respective Hookup Guides as well before you get started with the ‎SparkFun Triple Axis Accelerometer Breakout - BMA400 (Qwiic).‎

Hardware Overview

Let's take a closer look at the BMA400 and other hardware features on these Qwiic ‎breakouts.‎

BMA400 3-Axis Accelerometer

The BMA400 3-axis accelerometer from Bosch Sensortec is an ultra-low power motion ‎sensor with a host of interrupt features making it ideal for battery-powered activity ‎monitoring applications.‎

bma400_2

bma400_3

The BMA400 features four user-selectable ranges of ±2/±4/±8/±16g and consumes just ‎‎14.5µA when measuring acceleration data at the highest performance settings. The ‎BMA400 also includes a robust interrupt feature set:‎

  • Auto Wakeup

  • Auto Low Power

  • Step Counter

  • Activity Recognition (Running, Walking, Standing Still)‎

  • Orientation Detection

  • Tap and Double Tap

The sensor has two interrupt pins available for all of the above interrupt conditions. The ‎table below outlines a few of the BMA400's sensing and operating parameters. For a full ‎overview of the BMA400, refer to the datasheet.‎

table_1

Communication Interfaces - I2C & SPI

The standard size version of these Qwiic breakouts communicates over I2C by default but ‎also supports communicating using SPI. The Qwiic Micro version only supports I2C ‎communication over the Qwiic connector on the board.‎

interface_4

interface_5

The standard size routes the I2C interface to a pair of Qwiic connectors as well as a 0.1"-‎spaced PTH header for users who prefer SPI or a traditional soldered connection. The ‎standard-size breakout routes both INT1 and INT2 to a pair of PTH pins. The Qwiic Micro ‎routes only INT1 to a PTH pin.‎

Both boards set the BMA400's I2C address to 0x14 by default. Adjust the ADR jumper to ‎change to the alternate address (0x15) or open it completely to use the SPI interface ‎‎(Standard size only). More information on this jumper in the Solder Jumpers section below.‎

Solder Jumpers

The Standard size breakout has four solder jumpers labeled PWR, ADR, I2C, and CS. The ‎Micro size has all but the CS jumper as the Micro version does not support SPI. Instead, the ‎Micro version pulls the CS pin to 3.3V. The table below outlines the jumpers' labels, default ‎state, functionality, and any notes regarding their use.‎

jumpers_6

jumpers_7

table_2

Board Dimensions

The boards match the Standard and Micro form-factors for Qwiic breakouts measuring 1" x ‎‎1" (Standard) and 0.5" x 0.3" (Micro). The Standard breakout has four mounting holes and ‎the Micro has one. All mounting holes fit a size 4-40 screw.‎

dimensions_8

dimensions_9

Hardware Assembly

Now that we're familiar with the BMA400, we can start assembling our circuit.‎

Qwiic/I2C Assembly

The fastest and easiest way to get started using the breakout is to connect the Qwiic ‎connector on the breakout to a Qwiic-enabled development board like the SparkFun ‎RedBoard Artemis with a Qwiic cable and as shown in the image below.‎

assembly_10

If you would prefer a more secure and permanent connection with the Standard Size ‎breakout, you can solder headers or wire to the PTH header on the board.‎

SPI Assembly (Standard Size Only)‎

Setting the breakout up to communicate with the sensor over SPI requires completely ‎opening the ADR jumper and we recommend soldering to the PTH header to make the ‎connections. If you are not familiar with through-hole soldering, take a read through this ‎tutorial:‎

tutorial_11

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.‎

Along with tools for soldering, you'll need either some hookup wire or headers and jumper ‎wires. Sever the trace between the "Center" and "Right" pads of the ADR jumper to switch to ‎SPI mode. After opening this jumper, connect the breakout to your controller's SPI bus pins.‎

Remember, the BMP384 operates at 3.3V logic so make sure to connect to a board running ‎at the same logic level like the RedBoard Artemis or use a level shifter to adjust it to the ‎correct voltage.‎

voltage_12

Open the ADR jumper completely to use SPI.‎

BMA400 Arduino Library

Note: This library assumes you are using the latest version of the Arduino IDE on your ‎desktop. If this is your first time using Arduino, please review our tutorial on installing the ‎Arduino IDE. If you have not previously installed an Arduino library, please check out ‎our installation guide.‎

The SparkFun BMA400 Arduino Library is based off the API for the sensor from Bosch to let ‎users get started reading data from the sensor and using the various interrupt options. ‎Install the library through the Arduino Library Manager tool by searching for "SparkFun ‎BMA400". Users who prefer to manually install the library can download a copy of it from ‎the GitHub repository by clicking the button below:‎

SparkFun BMA400 Arduino Library (ZIP)‎

Library Functions

The list below outlines and describes the functions available in the SparkFun BMA400 ‎Arduino Library. For detailed information on the available parameters and use of all ‎functions, refer to the .cpp file in the library.‎

Sensor Initialization and Configuration

  • int8_t BMA400::beginI2C(uint8_t address, TwoWire& wirePort); - Initialize the sensor ‎over I2C at the specified address and port.‎

  • int8_t BMA400::beginSPI(uint8_t csPin, uint32_t clockFrequency); - Initialize the ‎sensor over SPI with the specified Chip Select pin and clock frequency.‎

  • int8_t setMode(uint8_t mode); - Set the power mode.‎

  • int8_t getMode(uint8_t* mode); - Returns the setting for power mode.‎

  • int8_t setAutoWakeup(bma400_auto_wakeup_conf* config); - Enable Auto Wakeup.‎

  • int8_t setAutoLowPower(bma400_auto_lp_conf* config); - Enable Auto Low Power

  • int8_t setRange(uint8_t range); - Set the measurement range.‎

  • int8_t getRange(uint8_t* range); - Returns the value stored for measurement range.‎

  • int8_t setODR(uint8_t odr); - Set the output data rate.‎

  • int8_t getODR(uint8_t* odr); - Returns the value stored for output data rate.‎

  • int8_t setOSRLP(uint8_t osrLP); - Set the output data rate for Low Power.‎

  • int8_t getOSRLP(uint8_t* osrLP); - Returns the value stored for output data rate for ‎Low Power.‎

  • int8_t setDataSource(uint8_t source); - Set the data source filter. Options are Default ‎with variable ODR, 100Hz ODR, and 100Hz with 1Hz bandwidth.‎

  • int8_t getDataSource(uint8_t* source); - Returns the value for data source.‎

  • int8_t setFilter1Bandwidth(uint8_t bw); - Set the low pass filter bandwidth.‎

  • int8_t getFilter1Bandwidth(uint8_t* bw); - Returns the value set for low pass filter ‎bandwidth.‎

  • int8_t getStepCount(uint32_t* count, uint8_t* activityType); - Returns the number of ‎steps measured along with activity type (Still, Walk, and Run).‎

  • int8_t selfTest(); - Runs self test to determine if the sensor is behaving correctly.‎

Sensor Data

  • int8_t getSensorData(bool sensorTime = false); - Requests acceleration data from ‎the BMA400. This must be called to update the data structure.‎

  • int8_t getTemperature(float* temp); - Returns the temperature data recorded in °C.‎

Interrupt Control and Feature Selection

  • int8_t setInterruptPinMode(bma400_int_chan channel, uint8_t mode); - Set the ‎interrupt pin mode. Options are push/pull and active high/low.‎

  • int8_t enableInterrupt(bma400_int_type intType, bool enable); - Enable interrupt ‎condition.‎

  • int8_t getInterruptStatus(uint16_t* status); - Returns interrupt status flags for the ‎various interrupt conditions (wakeup, activity, step, etc.).‎

  • int8_t setDRDYInterruptChannel(bma400_int_chan channel); - Select the interrupt ‎pin for the data ready interrupt condition.‎

  • int8_t setGeneric1Interrupt(bma400_gen_int_conf* config); - Set the generic 1 ‎interrupt configuration.‎

  • int8_t setGeneric2Interrupt(bma400_gen_int_conf* config); - Set the generic 2 ‎interrupt configuration.‎

  • int8_t setOrientationChangeInterrupt(bma400_orient_int_conf* config); - Set the ‎orientation change interrupt configuration.‎

  • int8_t setTapInterrupt(bma400_tap_conf* config); - Set the tap interrupt ‎configuration.‎

  • int8_t setStepCounterInterrupt(bma400_step_int_conf* config); - Set the step ‎counter interrupt configuration.‎

  • int8_t setActivityChangeInterrupt(bma400_act_ch_conf* config); - Set the activity ‎change interrupt configuration.‎

  • int8_t setWakeupInterrupt(bma400_wakeup_conf* config); - Set the device wakeup ‎interrupt configuration.‎

FIFO Buffer Control

  • int8_t setFIFOConfig(bma400_fifo_conf* config); - Enable and configure the FIFO ‎buffer.‎

  • int8_t getFIFOLength(uint16_t* numData); - Set the number of samples to store in ‎the FIFO buffer.‎

  • int8_t getFIFOData(BMA400_SensorData* data, uint16_t* numData); - Pull data ‎stored in FIFO buffer.‎

  • int8_t flushFIFO(); - Flush the FIFO buffer.‎

Arduino Examples

The BMA400 Arduino Library includes twelve examples covering all major features of the ‎accelerometer. In this section we'll take a closer look at three of them.‎

Example 1 - Basic Readings I2C

Example 1 demonstrates how to set the BMA400 up to communicate basic motion data ‎over I2C. Open the example by navigating to File > Examples > SparkFun BMA400 Arduino ‎Library > Example01_BasicReadingsI2C. Select your Board and Port and click Upload. ‎Open the serial monitor after the upload completes with the baud set to 115200 to watch ‎motion data print out.‎

If you have adjusted the ADR jumper to change to the alternate I2C address for the BMA400 ‎comment/uncomment the line with the correct value:‎

Copy Code
uint8_t i2cAddress = BMA400_I2C_ADDRESS_DEFAULT; // 0x14
//uint8_t i2cAddress = BMA400_I2C_ADDRESS_SECONDARY; // 0x15

The example attempts to initialize the sensor with default settings in I2C at the specified ‎address. If it cannot initialize properly, the code prints out an error in over serial:‎

Copy Code
while(accelerometer.beginI2C(i2cAddress) != BMA400_OK)
    {
        // Not connected, inform user
        Serial.println("Error: BMA400 not connected, check wiring and I2C address!");

        // Wait a bit to see if connection is established
        delay(1000);
    }

‎If you see this error, double check the sensor is connected properly and set to the correct I2C ‎address and reset the development board or re-upload the code.‎

The loop polls the BMA400 for acceleration data every 20ms using the 'getSensorData();' ‎function and prints out acceleration for all three axes in g's:‎

Copy Code
void loop()
{
    // Get measurements from the sensor. This must be called before accessing
    // the acceleration data, otherwise it will never update
    accelerometer.getSensorData();

    // Print acceleration data
    Serial.print("Acceleration in g's");
    Serial.print("\t");
    Serial.print("X: ");
    Serial.print(accelerometer.data.accelX, 3);
    Serial.print("\t");
    Serial.print("Y: ");
    Serial.print(accelerometer.data.accelY, 3);
    Serial.print("\t");
    Serial.print("Z: ");
    Serial.println(accelerometer.data.accelZ, 3);

    // Print 50x per second
    delay(20);
}

Move the sensor around in different directions and watch the acceleration data change with ‎the motion.‎

Example 6 - Motion Detection

Example 6 - Motion Detection demonstrates how to configure one of the BMA400's ‎interrupt pins (INT1) to trigger when the sensor detects motion over 1g on the Z axis.‎

The code defaults to use 'D2' as the interrupt pin on a connected development board. If your ‎development board does not support external interrupts on 'D2' change the value here:‎

Copy Code
int interruptPin = 2;

‎If you're not sure which pins on your board support external interrupts, this reference ‎page has lists available interrupt pins for most common Arduino development boards.‎

After initializing the BMA400 over I2C, the code configures the interrupt feature:‎

Copy Code
bma400_gen_int_conf config =
    {
        .gen_int_thres = 5, // 8mg resolution (eg. gen_int_thres=5 results in 40mg)
        .gen_int_dur = 5, // 10ms resolution (eg. gen_int_dur=5 results in 50ms)
        .axes_sel = BMA400_AXIS_XYZ_EN, // Which axes to evaluate for interrupts (X/Y/Z in any combination)
        .data_src = BMA400_DATA_SRC_ACCEL_FILT_2, // Which filter to use (must be 100Hz, datasheet recommends filter 2)
        .criterion_sel = BMA400_ACTIVITY_INT, // Trigger interrupts when active or inactive
        .evaluate_axes = BMA400_ANY_AXES_INT, // Logical combining of axes for interrupt condition (OR/AND)
        .ref_update = BMA400_UPDATE_EVERY_TIME, // Whether to automatically update reference values
        .hysteresis = BMA400_HYST_96_MG, // Hysteresis acceleration for noise rejection
        .int_thres_ref_x = 0, // Raw 12-bit acceleration value
        .int_thres_ref_y = 0, // Raw 12-bit acceleration value
        .int_thres_ref_z = 512, // Raw 12-bit acceleration value (at 4g range (default), 512 = 1g)
        .int_chan = BMA400_INT_CHANNEL_1 // Which pin to use for interrupts
    };
    accelerometer.setGeneric1Interrupt(&config);

    // Here we configure the INT1 pin to push/pull mode, active high
    accelerometer.setInterruptPinMode(BMA400_INT_CHANNEL_1, BMA400_INT_PUSH_PULL_ACTIVE_1);

    // Enable generic 1 interrupt condition
    accelerometer.enableInterrupt(BMA400_GEN1_INT_EN, true);

    // Setup interrupt handler
    attachInterrupt(digitalPinToInterrupt(interruptPin), bma400InterruptHandler, RISING);

This configures INT1 to operate in push/pull mode and active HIGH whenever the BMA400 ‎reports motion the Z axis over 1g among other settings. It also enables the interrupt ‎condition and sets up the interrupt handler.‎

The main loop waits for an interrupt event to happen and prints out whenever an interrupt ‎occurs, and motion is detected.‎

Example 10 - Step Counter

Example 10 - Step Counter shows how to use the BMA400's Step Counter feature ‎commonly found in smart watches and other activity monitors. The sensor handles step ‎detection and counting so we'll leave those settings as default. They can technically be ‎altered but we do not recommend it as it's not well documented and can cause ‎unpredictable behavior.‎

After initializing the sensor, we select and configure INT1 for interrupts and enable step ‎counting:‎

Copy Code
bma400_step_int_conf config =
    {
        .int_chan = BMA400_INT_CHANNEL_1 // Which pin to use for interrupts
    };
    accelerometer.setStepCounterInterrupt(&config);

    // Here we configure the INT1 pin to push/pull mode, active high
    accelerometer.setInterruptPinMode(BMA400_INT_CHANNEL_1, BMA400_INT_PUSH_PULL_ACTIVE_1);

    // Enable step counter interrupt condition. This must be set to enable step
    // counting at all, even if you don't want interrupts to be generated.
    // In that case,  set the interrupt channel above to BMA400_UNMAP_INT_PIN
    accelerometer.enableInterrupt(BMA400_STEP_COUNTER_INT_EN, true);

    // Setup interrupt handler
    attachInterrupt(digitalPinToInterrupt(interruptPin), bma400InterruptHandler, RISING);

The main loop checks for a step detection interrupt event and prints the step count and ‎activity type over serial. Try moving the sensor around or attach it to your wrist to simulate a ‎smart watch and walk/run around. You should see the data update with new step values ‎and activity states.‎

Troubleshooting

General Troubleshooting

Not working as expected and need help?

‎If you need technical assistance and more information on a product that is not working as ‎you expected, we recommend heading on over to the SparkFun Technical Assistance page ‎for some initial troubleshooting.

SparkFun Technical Assistance Page

‎If you don't find what you need there, the SparkFun Forums are a great place to find and ask ‎for help. If this is your first visit, you'll need to create a Forum Account to search product ‎forums and post questions.

Resources and Going Further

That's all for this tutorial. For more information about the BMA400 and these breakouts, ‎check out the resources below:‎

  • Schematics

o Standard
o Micro
  • Eagle Files

o Standard
o Micro
  • Board Dimensions

o Standard
o Micro
מק"ט יצרן # 15081
QWIIC CABLE KIT
SparkFun Electronics
מק"ט יצרן # 14495
QWIIC ADAPTER
SparkFun Electronics
מק"ט יצרן # 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
מק"ט יצרן # 16790
QWIIC SHIELD FOR THING PLUS
SparkFun Electronics
מק"ט יצרן # 14427
QWIIC CABLE - 100MM
SparkFun Electronics
מק"ט יצרן # 14426
QWIIC CABLE - 50MM
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.