Maker.io main logo

Split Ortho Keyboard with TCA8418 Matrix Expanders

284

2023-01-03 | By Adafruit Industries

License: See Original Project 3D Printing Programmers STEMMA

Courtesy of Adafruit

Guide by John Park

Overview

Forget about that staggered key layout -- a holdover from ‎mechanical typewriters -- and build your own custom ortholinear ‎keyboard! Honor the angle of your wrists with the split design.‎

Keyboard_1

Keyboard_2

This 60% layout is fast and efficient (once you practice and get used ‎to a new way of working) -- keyboard "layers" allow you to access ‎any key you need by "lowering" or "raising" to whole new sets of keys.‎

Pick your favorite MX compatible key switches and press them into ‎the socketed 6x5 NeoKey PCB. Build a 3D printed or 3D printed/laser ‎cut acrylic combo case.‎

Two TCA8418 matrix expanders handle reading the diode key ‎matrices, and a Kee Boar KB2040 running CircuitPython does the ‎rest, acting as a USB HID keyboard device.‎

Create and edit your own custom layouts with ‎the keymaps.py config file. The layout I used was inspired by this ‎keyboard project.‎

create_3

Parts

You'll want to pick some keycaps. If you are highly elite and need no ‎legends, try one of the choices below. Otherwise, search online for ‎‎"MX compatible ortholinear keycap set". The ones used in this ‎guide are the Drop MT3 profile Dancer ortho kit.‎

Or

Build the Split Ortho Keyboard

fritzing_4

Setup

Both sides of the Split Ortho Keyboard contain their own 6x5 diode ‎matrix keyswitch PCB wired to the column and row pins of a ‎TCA8418 keypad matrix expander.‎

Each TCA8418 takes care of handling keypress decoding and sends ‎the event queue to the QT Py RP2040 over I2C.‎

Since only one address is possible on the TCA8418 you'll use the two ‎independent I2C buses of the QT Py RP2040.‎

Wire Columns and Rows

Solder a wire to each column and row pad on the 6x5 PCBs.‎

Run these to their corresponding column and row pins on the ‎TCA8418.‎

Repeat this for the second side.‎

wire_5

wire_6

wire_7

QT Py Prep

In order to plug the STEMMA QT cable into the second I2C bus, solder ‎the STEMMA QT/Qwiic breakout to the SDA, SCL, 3V, and GND pins ‎as shown here.‎

Note, both sockets on the breakout run to the same on-board I2C ‎bus, so one TCA8418 will plug into the breakout, while the other will ‎plug into the QT Py's on-board STEMMA QT connector.‎

prep_8

prep_9

Case Build

You have two options for the case build -- fully 3D printed, or mixed ‎‎3D printed with laser cut/CNC acrylic (or other materials).‎

Download the files from the link below.‎

‎3D and 2D fabrication files

3D Files‎

If you go with the fully 3D build, print the following files in PLA at ‎‎~0.2mm layer height and ~10% infill:‎

  • sok_plate x2‎

  • sok_top x2

  • sok_base_L

  • sok_baseR

fab_10

‎3D/2D Mix Files‎

If you opt for a mix of 3D printed and 2D, here are the files you'll use:‎

‎3D Printed‎

  • sok_qt

  • sok_mid x2‎

‎2D Laser Cut/CNC Milled‎

  • sok_curves x2

printed_11

Frame Prep

Use your soldering iron to press a threaded M3 brass heat set insert ‎into each of the six mounting holes of the base walls. You use these ‎to screw on the top plate later.‎

If doing the 3D + laser cut frame, insert a second set of inserts on the ‎back side as well so you can screw on the top plate and the back ‎plate.‎

frame_13

frame_12

frame_14

frame_15

Base Prep

Screw in M2.5 stand-offs to support the PCB and breakout board as ‎shown.‎

You can also add rubber bumper feet.‎

Then, screw the back plate on using M3 screws (only necessary for ‎the hybrid case build).‎

base_16

base_17

base_18

base_19

base_20

Switch Plate

To stabilize the keyswitches, snap them into the switch plate. Be ‎sure their header pins are all oriented in the same direction as ‎shown here.‎

switch_21

switch_22

switch_23

switch_24

Attach Keys to PCBs

Carefully align all the pins to the sockets and gently, slowly press the ‎keys into place.‎

This takes patience and massaging, so maybe put on some soothing ‎music and light a good candle first.‎

Then add your keycaps. (Ignore the photo that shows the caps ‎already in place during the first step.)‎

attach_25

attach_26

Right Side Mounting

On the right side, mount just the TCA8418 and the keyswitch PCB as ‎shown.‎

right_27

right_28

right_29

right_30

Stemma QT Cable Right Side

If you don't think you want to fully disconnect the halves, plug in the ‎STEMMA QT cable as shown. This provides a neater appearance and ‎allows you to push the cable in to adjust the slack.‎

cable_31

QT Py Mount

Click the QT Py into its mount, facing the base. This will allow access ‎to the reset and boot buttons through the case bottom's holes.‎

mount_32

STEMMA QT Connection

Connect the long STEMMA QT cable for the right half keyboard to the ‎STEMMA QT/Qwiic breakout, using the standoff hardware as ‎routing/strain relief.‎

connection_33

Plug the short STEMMA QT cable from the QT Py to the TCA8418.‎

short_34

tca_35

Case Top

Add the case top and screw it down using M3 screws into the ‎treaded inserts.‎

case_36

case_37

case_38

Connect the Halves

If you didn't connect the right half STEMMA QT cable before closing ‎the case, do so at this time.‎

half_39

half_40

half_41

half_42

half_43

half_44

half_45

USB Cable

Plug in a USB-C cable and you're ready to code and use the ‎keyboard.‎

usb_45

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

Download the latest version of CircuitPython for this board via ‎circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

download_46

boot_47

To enter the bootloader, hold down the BOOT/BOOTSEL ‎button (highlighted in red above), and while continuing to hold it ‎‎(don't let go!), press and release the reset button (highlighted in ‎blue above). Continue to hold the BOOT/BOOTSEL button until the ‎RPI-RP2 drive appears!‎

If the drive does not appear, release all the buttons, and then repeat ‎the process above.‎

You can also start with your board unplugged from USB, press, and ‎hold the BOOTSEL button (highlighted in red above), continue to ‎hold it while plugging it into USB, and wait for the drive to appear ‎before releasing the button.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.

You will see a new disk drive appear called RPI-RP2.‎‎

‎Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.‎

disk_48

disk_49

The RPI-RP2 drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.‎

That's it, you're done! :)‎

disk_50

Safe Mode

You want to edit your code.py or modify the files on ‎your CIRCUITPY drive but find that you can't. Perhaps your board ‎has gotten into a state where CIRCUITPY is read-only. You may have ‎turned off the CIRCUITPY drive altogether. Whatever the reason, safe ‎mode can help.‎

Safe mode in CircuitPython does not run any user code on startup ‎and disables auto-reload. This means a few things. First, safe ‎mode bypasses any code in boot.py (where you can ‎set CIRCUITPY read-only or turn it off completely). Second, it does ‎not run the code in code.py. And finally, it does not automatically ‎soft-reload when data is written to the CIRCUITPY drive.

Therefore, whatever you may have done to put your board in a non-‎interactive state, safe mode gives you the opportunity to correct it ‎without losing all of the data on the CIRCUITPY drive.‎

Entering Safe Mode in CircuitPython 6.x

This section explains entering safe mode on CircuitPython 6.x.‎

section_51

To enter safe mode when using CircuitPython 6.x, plug in your board ‎or hit reset (highlighted in red above). Immediately after the board ‎starts up or resets, it waits 700ms. On some boards, the onboard ‎status LED (highlighted in green above) will turn solid yellow during ‎this time. If you press reset during that 700ms, the board will start up ‎in safe mode. It can be difficult to react to the yellow LED, so you ‎may want to think of it simply as a slow double click of the reset ‎button. (Remember, a fast double click of reset enters the ‎bootloader.)‎

Entering Safe Mode in CircuitPython 7.x

This section explains entering safe mode on CircuitPython 7.x.‎

To enter safe mode when using CircuitPython 7.x, plug in your board ‎or hit reset (highlighted in red above). Immediately after the board ‎starts up or resets, it waits 1000ms. On some boards, the onboard ‎status LED (highlighted in green above) will blink yellow during that ‎time. If you press reset during that 1000ms, the board will start up in ‎safe mode. It can be difficult to react to the yellow LED, so you may ‎want to think of it simply as a slow double click of the reset button. ‎‎(Remember, a fast double click of reset enters the bootloader.)‎

In Safe Mode

Once you've entered safe mode successfully in CircuitPython 6.x, the ‎LED will pulse yellow.‎

If you successfully enter safe mode on CircuitPython 7.x, the LED will ‎intermittently blink yellow three times.‎

If you connect to the serial console, you'll find the following message.‎

Copy Code
Auto-reload is off.
Running in safe mode! Not running saved code.

CircuitPython is in safe mode because you pressed the reset button during boot. Press again to exit safe mode.

Press any key to enter the REPL. Use CTRL-D to reload.

You can now edit the contents of the CIRCUITPY drive. ‎Remember, your code will not run until you press the reset button, or ‎unplug and plug in your board, to get out of safe mode.

Flash Resetting UF2‎

If your board ever gets into a really weird state and doesn't even ‎show up as a disk drive when installing CircuitPython, try loading ‎this 'nuke' UF2 which will do a 'deep clean' on your Flash ‎Memory. You will lose all the files on the board, but at least you'll be ‎able to revive it! After loading this UF2, follow the steps above to re-‎install CircuitPython.‎

Download flash erasing "nuke" UF2

Code the Split Ortho Keyboard

Text Editor

Adafruit recommends using the Mu editor for editing your ‎CircuitPython code. You can get more info in this guide.‎

Alternatively, you can use any text editor that saves simple text files.‎

Download the Project Bundle

Your project will use a specific set of CircuitPython libraries, ‎the code.py file and the keymaps.py file. To get everything you need, ‎click on the Download Project Bundle link below, and uncompress ‎the .zip file.‎

Drag the contents of the uncompressed bundle directory onto your ‎board's CIRCUITPY drive, replacing any existing files or directories ‎with the same names, and adding any new ones that are necessary.‎

board_52

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: Copyright (c) 2022 John Park & Tod Kurt for Adafruit Industries
#
# SPDX-License-Identifier: MIT
# Ortho split keyboard
import time
import board
from adafruit_tca8418 import TCA8418
import usb_hid
from adafruit_hid.keyboard import Keyboard
from adafruit_hid.keycode import Keycode
from keymaps import layer_keymaps # keymaps are saved in keymaps.py file

kbd = Keyboard(usb_hid.devices)
num_layers = len(layer_keymaps)
current_layer = 1

i2c_left = board.STEMMA_I2C()  # uses QT Py RP2040 STEMMA QT port
i2c_right = board.I2C()  # I2C channel on the QT Py RP2040 pads broken out on board
tca_left = TCA8418(i2c_left)
tca_right = TCA8418(i2c_right)

tcas = (tca_left, tca_right)  # put the TCA objects in a list for easy iteration later

# set up a R0-R7 pins and C0-C4 pins as keypads
KEYPADPINS = (
                TCA8418.R0, TCA8418.R1, TCA8418.R2, TCA8418.R3, TCA8418.R4,
                TCA8418.C0, TCA8418.C1, TCA8418.C2, TCA8418.C3, TCA8418.C4, TCA8418.C5
)

for tca in tcas:
    for pin in KEYPADPINS:
        tca.keypad_mode[pin] = True
        tca.enable_int[pin] = True
        tca.event_mode_fifo[pin] = True
    tca.key_intenable = True

print("Ortho Split Keyboard")


while True:
    for i in range(len(tcas)):
        tca = tcas[i]  # get the TCA we're working with
        keymap = layer_keymaps[current_layer][i]  # get the corresponding keymap for it
        if tca.key_int:
            events = tca.events_count
            for _ in range(events):
                keyevent = tca.next_event
                keymap_number = (keyevent & 0x7F)
                (modifier, keycode) = keymap[keymap_number]  # get keycode & modifer from keymap
                #  print("\tKey event: 0xX - key #%d " % (keyevent, keyevent & 0x7F))
                if keycode is None:
                    pass

                else:
                    if keyevent & 0x80:  # if key is pressed
                        if modifier == 0:  # normal keypress
                            kbd.press(keycode)
                        elif modifier == 1:  # lower
                            current_layer = min(max((current_layer-1), 0), num_layers-1)
                        elif modifier == 2:  # raise
                            current_layer = min(max((current_layer+1), 0), num_layers-1)
                        elif modifier == 7:  # cap mod
                            kbd.press(Keycode.SHIFT, keycode)

                    else:  # key released
                        if modifier == 7:  # capped shifted key requires special handling
                            kbd.release(Keycode.SHIFT, keycode)
                        else:
                            kbd.release(keycode)

            tca.key_int = True  # clear the IRQ by writing 1 to it
            time.sleep(0.01)

View on GitHub

How It Works

The keyboard uses two TCA8418 expanders to read the matrix ‎columns and rows of the keyboard halves. The events are queued up ‎and sent over I2C to the QT Py RP2040 which then correlates each ‎keypress with a keycode from the keymaps.py file. These keypresses ‎are then sent to the computer as USB HID keys.‎

Libraries

You'll import libraries to provide functionality in the code:‎

  • time

  • board

  • adafruit_tca8418

  • usb_hid

  • adafruit_hid.keyboard

  • adafruit_hid.keycode‎

The keymaps file is imported as well so that the layer_keymaps can be ‎accessed inside of code.py.

Download File

Copy Code
import time
import board
from adafruit_tca8418 import TCA8418
import usb_hid
from adafruit_hid.keyboard import Keyboard
from adafruit_hid.keycode import Keycode
from keymaps import layer_keymaps

HID Setup

The USB HID keyboard is set up along with variables for the key ‎layers.‎

Download File

Copy Code
kbd = Keyboard(usb_hid.devices)
num_layers = len(layer_keymaps)
current_layer = 1

I2C Setup

You'll use both I2C channels on the QT Py RP2040 to connect to the ‎two TCA8418 boards. Since they share the same address which ‎cannot be changed, they can't be on the same I2C bus.‎

Download File

Copy Code
i2c_left = board.STEMMA_I2C()  # uses QT Py RP2040 STEMMA QT port
i2c_right = board.I2C()  # I2C channel on the QT Py RP2040 pads broken out on board
tca_left = TCA8418(i2c_left)
tca_right = TCA8418(i2c_right)
tcas = (tca_left, tca_right)  # put the TCA objects in a list for easy iteration later

Matrix Pins

The column and row pins of the TCA8418 are fixed, so we'll specify ‎the ones we're using for the six columns and five rows of the ‎keyboard halves.‎

Then, each pin is set to keypad_mode with enable and fifo (first in, first ‎out) set.‎

Download File

Copy Code
KEYPADPINS = (
                TCA8418.R0, TCA8418.R1, TCA8418.R2, TCA8418.R3, TCA8418.R4,
                TCA8418.C0, TCA8418.C1, TCA8418.C2, TCA8418.C3, TCA8418.C4, TCA8418.C5
)

for tca in tcas:
    for pin in KEYPADPINS:
        tca.keypad_mode[pin] = True
        tca.enable_int[pin] = True
        tca.event_mode_fifo[pin] = True
    tca.key_intenable = True

Main Loop

The main loop of the program checks each TCA8418 for events in the ‎queue. If a key has been pressed or released it is checked against ‎the keymap file to see which keycode to press or release. These can ‎vary depending on modifiers and layers as well.‎

Download File

Copy Code
while True:
    for i in range(len(tcas)):
        tca = tcas[i]  # get the TCA we're working with
        keymap = layer_keymaps[current_layer][i]  # get the corresponding keymap for it
        if tca.key_int:
            events = tca.events_count
            for _ in range(events):
                keyevent = tca.next_event
                keymap_number = (keyevent & 0x7F)
                (modifier, keycode) = keymap[keymap_number]  # get keycode & modifer from keymap
                #  print("\tKey event: 0xX - key #%d " % (keyevent, keyevent & 0x7F))
                if keycode is None:
                    pass

                else:
                    if keyevent & 0x80:  # if key is pressed
                        if modifier == 0:  # normal keypress
                            kbd.press(keycode)
                        elif modifier == 1:  # lower
                            current_layer = min(max((current_layer-1), 0), num_layers-1)
                        elif modifier == 2:  # raise
                            current_layer = min(max((current_layer+1), 0), num_layers-1)
                        elif modifier == 7:  # cap mod
                            kbd.press(Keycode.SHIFT, keycode)

                    else:  # key released
                        if modifier == 7:  # capped shifted key requires special handling
                            kbd.release(Keycode.SHIFT, keycode)
                        else:
                            kbd.release(keycode)

            tca.key_int = True  # clear the IRQ by writing 1 to it
            time.sleep(0.01)

keymaps.py

Download File

Copy Code
# SPDX-FileCopyrightText: Copyright (c) 2022 John Park & Tod Kurt for Adafruit Industries
#
# SPDX-License-Identifier: MIT
from adafruit_hid.keycode import Keycode
# https://docs.circuitpython.org/projects/hid/en/latest/api.html#adafruit-hid-keycode-keycode
# keymap is keynumber, (modifier, keycode)
# lower keymap layer
km_lf_0 = {
            (1) : (0, Keycode.F11),
            (2) : (0, Keycode.F1),
            (3) : (0, Keycode.F2),
            (4) : (0, Keycode.F3),
            (5) : (0, Keycode.F4),
            (6) : (0, Keycode.F5),

            (11) : (0, None),
            (12) : (0, None),
            (13) : (0, None),
            (14) : (0, None),
            (15) : (0, None),
            (16) : (0, None),

            (21) : (0, None),
            (22) : (0, None),
            (23) : (0, None),
            (24) : (0, None),
            (25) : (0, None),
            (26) : (0, None),

            (31) : (0, None),
            (32) : (0, None),
            (33) : (0, None),
            (34) : (0, None),
            (35) : (0, None),
            (36) : (0, None),

            (41) : (0, Keycode.CONTROL),
            (42) : (0, Keycode.GUI),
            (43) : (0, Keycode.ALT),
            (44) : (0, Keycode.GUI),
            (45) : (1, Keycode.L),  # lower (the keycode doesn't matter here, it's never typed)
            (46) : (0, Keycode.SPACE)
}

km_rt_0 = {
            (1) : (0, Keycode.F6),
            (2) : (0, Keycode.F7),
            (3) : (0, Keycode.F8),
            (4) : (0, Keycode.F9),
            (5) : (0, Keycode.F10),
            (6) : (0, Keycode.F12),

            (11) : (0, Keycode.HOME),
            (12) : (0, Keycode.PAGE_DOWN),
            (13) : (0, Keycode.PAGE_UP),
            (14) : (0, Keycode.END),
            (15) : (0, Keycode.INSERT),
            (16) : (0, Keycode.DELETE),

            (21) : (0, None),
            (22) : (0, None),
            (23) : (0, None),
            (24) : (0, None),
            (25) : (0, None),
            (26) : (0, None),

            (31) : (0, None),
            (32) : (0, None),
            (33) : (0, None),
            (34) : (0, None),
            (35) : (0, None),
            (36) : (0, None),

            (41) : (0, Keycode.SPACE),
            (42) : (2, Keycode.R),  # raise
            (43) : (0, Keycode.LEFT_ARROW),
            (44) : (0, Keycode.DOWN_ARROW),
            (45) : (0, Keycode.UP_ARROW),
            (46) : (0, Keycode.RIGHT_ARROW)
}

# main keymap layer
km_lf_1 = {
            (1) : (0, Keycode.GRAVE_ACCENT),
            (2) : (0, Keycode.ONE),
            (3) : (0, Keycode.TWO),
            (4) : (0, Keycode.THREE),
            (5) : (0, Keycode.FOUR),
            (6) : (0, Keycode.FIVE),

            (11) : (0, Keycode.ESCAPE),
            (12) : (0, Keycode.Q),
            (13) : (0, Keycode.W),
            (14) : (0, Keycode.E),
            (15) : (0, Keycode.R),
            (16) : (0, Keycode.T),

            (21) : (0, Keycode.TAB),
            (22) : (0, Keycode.A),
            (23) : (0, Keycode.S),
            (24) : (0, Keycode.D),
            (25) : (0, Keycode.F),
            (26) : (0, Keycode.G),

            (31) : (0, Keycode.SHIFT),
            (32) : (0, Keycode.Z),
            (33) : (0, Keycode.X),
            (34) : (0, Keycode.C),
            (35) : (0, Keycode.V),
            (36) : (0, Keycode.B),

            (41) : (0, Keycode.CONTROL),
            (42) : (0, Keycode.GUI),
            (43) : (0, Keycode.ALT),
            (44) : (0, Keycode.GUI),
            (45) : (1, Keycode.L),  # lower
            (46) : (0, Keycode.SPACE)
}

km_rt_1 = {
            (1) : (0, Keycode.SIX),
            (2) : (0, Keycode.SEVEN),
            (3) : (0, Keycode.EIGHT),
            (4) : (0, Keycode.NINE),
            (5) : (0, Keycode.ZERO),
            (6) : (0, Keycode.BACKSPACE),

            (11) : (0, Keycode.Y),
            (12) : (0, Keycode.U),
            (13) : (0, Keycode.I),
            (14) : (0, Keycode.O),
            (15) : (0, Keycode.P),
            (16) : (0, Keycode.BACKSLASH),

            (21) : (0, Keycode.H),
            (22) : (0, Keycode.J),
            (23) : (0, Keycode.K),
            (24) : (0, Keycode.L),
            (25) : (0, Keycode.SEMICOLON),
            (26) : (0, Keycode.QUOTE),

            (31) : (0, Keycode.N),
            (32) : (0, Keycode.M),
            (33) : (0, Keycode.COMMA),
            (34) : (0, Keycode.PERIOD),
            (35) : (0, Keycode.FORWARD_SLASH),
            (36) : (0, Keycode.ENTER),

            (41) : (0, Keycode.SPACE),
            (42) : (2, Keycode.R),  # raise
            (43) : (0, Keycode.LEFT_ARROW),
            (44) : (0, Keycode.DOWN_ARROW),
            (45) : (0, Keycode.UP_ARROW),
            (46) : (0, Keycode.RIGHT_ARROW)
}

# upper keymap layer
km_lf_2 = {
            (1) : (0, None),
            (2) : (0, None),
            (3) : (0, None),
            (4) : (0, None),
            (5) : (0, None),
            (6) : (0, None),

            (11) : (0, Keycode.ESCAPE),
            (12) : (0, None),
            (13) : (0, None),
            (14) : (0, None),
            (15) : (0, None),
            (16) : (0, None),

            (21) : (0, Keycode.TAB),
            (22) : (0, None),
            (23) : (0, None),
            (24) : (0, Keycode.MINUS),
            (25) : (0, Keycode.EQUALS),
            (26) : (7, Keycode.BACKSLASH),  # PIPE '|'

            (31) : (0, Keycode.SHIFT),
            (32) : (0, None),
            (33) : (0, None),
            (34) : (7, Keycode.MINUS),  # UNDERSCORE
            (35) : (0, Keycode.KEYPAD_PLUS),
            (36) : (0, Keycode.BACKSLASH),

            (41) : (0, Keycode.CONTROL),
            (42) : (0, Keycode.GUI),
            (43) : (0, Keycode.ALT),
            (44) : (0, Keycode.GUI),
            (45) : (1, Keycode.L),  # lower
            (46) : (0, Keycode.SPACE)
}

km_rt_2 = {
            (1) : (0, None),
            (2) : (0, None),
            (3) : (0, None),
            (4) : (0, None),
            (5) : (0, None),
            (6) : (0, Keycode.BACKSPACE),

            (11) : (0, None),
            (12) : (0, None),
            (13) : (0, None),
            (14) : (0, None),
            (15) : (0, None),
            (16) : (0, Keycode.BACKSLASH),

            (21) : (0, None),
            (22) : (0, Keycode.LEFT_BRACKET),
            (23) : (0, Keycode.RIGHT_BRACKET),
            (24) : (0, None),
            (25) : (0, None),
            (26) : (0, Keycode.QUOTE),

            (31) : (0, None),
            (32) : (7, Keycode.LEFT_BRACKET),
            (33) : (7, Keycode.RIGHT_BRACKET),
            (34) : (0, None),
            (35) : (0, None),
            (36) : (0, Keycode.ENTER),

            (41) : (0, Keycode.SPACE),
            (42) : (2, Keycode.R),  # raise
            (43) : (0, Keycode.LEFT_ARROW),
            (44) : (0, Keycode.DOWN_ARROW),
            (45) : (0, Keycode.UP_ARROW),
            (46) : (0, Keycode.RIGHT_ARROW)
}

# put the keymaps in layer lists for easy iteration later
keymaps_1 = (km_lf_0, km_rt_0)
keymaps_2 = (km_lf_1, km_rt_1)
keymaps_3 = (km_lf_2, km_rt_2)
layer_keymaps = (keymaps_1, keymaps_2, keymaps_3)

View on GitHub

The keymaps.py file first imports the adafruit_hid.keycode library.‎

from adafruit_hid.keycode import Keycode

The file is organized by keymap sides (left/right), layers (0, 1, 2), and ‎row clusters (1-6, 11-16, 21-26, etc.) These are dictionaries which have a ‎‎"key" which corresponds to the key number as reported by the ‎TCA8418, and a value tuple which tells the code two things: ‎which modifier, and which keycode to use.‎

The modifier is usually 0 which means the keycode is sent as a ‎normal keypress/release.‎

Modifer 1 means the "lower" key has been pressed, so a different ‎keymap set is to be used until the "raise" key is pressed.‎

Modifier 2 means "raise"‎.

Modifier 7 means a Keycode.SHIFT + the keycode are pressed at the ‎same time. Normally you use the shift key to get this effect, but in ‎some cases, you may want to assign a key that is normally only ‎invoked via shift. For example, a { key is usually shift ‎‎+ Keycode.LEFT_BRACKET, but if you want a key to press { all on its own, ‎use modifier 7.

מק"ט יצרן # 4900
QT PY RP2040
Adafruit Industries LLC
מק"ט יצרן # 5385
STEMMA QT/QWIIC CABLE 400MM
Adafruit Industries LLC
מק"ט יצרן # 4918
ADAFRUIT TCA8418 KEYPAD MATRIX A
Adafruit Industries LLC
מק"ט יצרן # 4953
KAILH MECHANICAL KEY SWITCHES -
Adafruit Industries LLC
מק"ט יצרן # 5005
BLUE DSA KEYCAPS FOR MX COMPATIB
Adafruit Industries LLC
מק"ט יצרן # 5016
BLUE DSA KEYCAP FOR MXCOM 1=10PC
Adafruit Industries LLC
מק"ט יצרן # 5174
CYAN MA KEYCAPS - 5 PACK
Adafruit Industries LLC
מק"ט יצרן # 4255
BRASS HEAT-SET M3X4M 1=BAG/50PCS
Adafruit Industries LLC
מק"ט יצרן # 4685
BLACK NYLON SCREW AND STAND-OFF
Adafruit Industries LLC
מק"ט יצרן # 3299
BLACK NYLON SCREW AND STAND-OFF
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.