Maker.io main logo

Traffic Light Conference Badge

66

2022-08-23 | By Adafruit Industries

License: See Original Project 3D Printing Wearables ESP32 STEMMA

Courtesy of Adafruit

Guide by Liz Clark

Overview

When you're out and about at a convention or conference ‎sometimes you want to be a social butterfly, but other times you'd ‎prefer to float anonymously amongst the crowds. In this project, ‎you'll build a conference badge utilizing a tiny traffic light that you ‎can use to symbolize to the world your socializing preferences in the ‎moment:‎

  • Red for "no socializing please"‎

  • Yellow for "lets connect if we really know each other"

  • Green for "I want to talk to every single person"‎

project_1

The badge uses a QT Py ESP32-S2 with a LiPo BFF running ‎CircuitPython. This makes for an ultra-portable electronics solution ‎with code you can customize even while you're at the con.‎

The badge is themed as a tiny road diorama to match the mini traffic ‎light model. You can paint and customize the case with model ‎accessories such as grass, plants, or other small details.‎

badge_2

There is a cutout in the case for a STEMMA cable. You can use it for ‎additional electronics, plugging in SAO boards or adding your ‎favorite STEMMA sensor.‎

sensor_3

Parts

Diorama Parts and Paint

  • ‎1 x Mini Green Grass

  • ‎1 x Mini Meadowland Bushes

  • ‎1 x Acrylic paint

  • ‎1 x E6000 glue

Circuit Diagram

diagram_4

Button

  • Button output to board pin A0

  • Button ground to board GND

Traffic Light

  • Red wire to board pin A1

  • Yellow wire to board pin A2

  • Green wire to board pin A3

  • Black wire to board 3V‎‎

3D Printing

3d_5

The badge may be housed in a 3D printed case, described below. ‎The case consists of three parts: a bottom lid, a main badge case, ‎and a tiny manhole cover. The main badge case benefits from some ‎supports.‎

The STL files can be downloaded directly here or from Thingiverse.‎

Thingiverse download

trafficLightBadgeSTLfiles.zip

You can use support blockers in your slicer software to only have ‎supports in the center of the main badge case. This should provide ‎enough support for your printer to bridge the wall.‎

slicer_6

slicer_7

The badge has slots and cutouts for the button, traffic light, and QT ‎Py ESP32-S2's STEMMA cable. If you don't want to use the STEMMA ‎cable, you can cover the hole with the tiny manhole cover.‎

slots_8

Painting

You can print the parts in white PLA so that you can paint the ‎different details of the badge. Acrylic paint works great for covering ‎PLA. ‎

painting_9

You can add diorama grass and plants on the side of the road. Add a ‎thin layer of E6000 glue over the surface of the grass area and ‎sprinkle the grass on top.‎

grass_10

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

Download the latest version of CircuitPython for this board via ‎circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

file_11

board_12

Plug your board into your computer, using a known-good data-sync ‎cable, directly, or via an adapter if needed.‎

Click the reset button once (highlighted in red above), and then click ‎it again when you see the RGB status LED(s) (highlighted in green ‎above) turn purple (approximately half a second later). Sometimes it ‎helps to think of it as a "slow double-click" of the reset button.‎

For this board, tap reset and wait for the LED to turn purple, and as ‎soon as it turns purple, tap reset again. The second tap needs to ‎happen while the LED is still purple.‎

Once successful, you will see the RGB status LED(s) turn green ‎‎(highlighted in green above). If you see red, try another port, or if ‎you're using an adapter or hub, try without the hub, or different ‎adapter or hub.‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.‎

If after several tries, and verifying your USB cable is data-ready, you ‎still cannot get to the bootloader, it is possible that the bootloader is ‎missing or damaged. Check out the Install UF2 Bootloader page for ‎details on resolving this issue.‎

You will see a new disk drive appear called QTPYS2BOOT.‎‎ ‎

Drag the adafruit_circuitpython_etc.uf2 file to QTPYS2BOOT.‎

disk_13

The BOOT drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.‎

That's it!‎

boot_14

Coding the Traffic Light ‎Conference Badge

Once you've finished setting up your QT Py ESP32-S2 with ‎CircuitPython, you can access the code and necessary libraries by ‎downloading the Project Bundle.‎

To do this, click on the Download Project Bundle button in the ‎window below. It will download as a zipped folder.‎

‎Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2022 Liz Clark for Adafruit Industries
# SPDX-License-Identifier: MIT

import time
import board
import alarm
from digitalio import DigitalInOut, Direction, Pull
#  setup pins for the traffic light LEDs
red_light = DigitalInOut(board.A1)
yellow_light = DigitalInOut(board.A2)
green_light = DigitalInOut(board.A3)
#  array of LEDs
lights = [red_light, yellow_light, green_light]
#  the traffic light is common anode
#  the pins will need to be pulled down to ground
#  to turn on the LEDs. they are setup as inputs
#  so that the pull can be toggled
#  Pull.UP turns the LEDs off to start
for light in lights:
    light.direction = Direction.INPUT
    light.pull = Pull.UP
#  button pin setup
pin_alarm = alarm.pin.PinAlarm(pin=board.A0, value=False, pull=True)
#  count to track which light is on
count = 2
#  tracks the last light
last_count = 1
while True:
    #  increase count by 1, loop through 0-2
    count = (count+1) % 3
    #  turn off the last LED
    lights[last_count].pull = Pull.UP
    #  turn on the current LED
    lights[count].pull = Pull.DOWN
    #  print(count)
    #  delay to keep count
    time.sleep(1)
    #  reset last LED for next loop
    last_count = count
    #  go into light sleep mode until button is pressed again
    alarm.light_sleep_until_alarms(pin_alarm)

View on GitHub

Upload the Code and Libraries to the QT Py ‎ESP32-S2‎

After downloading the Project Bundle, plug your QT Py ESP32-S2 ‎into the computer's USB port with a known good USB data+power ‎cable. You should see a new flash drive appear in the computer's File ‎Explorer or Finder (depending on your operating system) ‎called CIRCUITPY. Unzip the folder and copy the following items to ‎the QT Py ESP32-S2's CIRCUITPY drive. ‎

  • lib folder

  • code.py

Your QT Py ESP32-S2 CIRCUITPY drive should look like this after ‎copying the lib folder and the code.py file.‎

qt_15

How the CircuitPython Code Works

The traffic light model's LEDs are common anode, meaning that the ‎three LEDs share power (the black wire). The red, yellow, and green ‎wires need to be tied to ground to turn on the LEDs.‎

In the code, the three LEDs' pins are set as inputs so that ‎their pull direction can be toggled either UP or DOWN. When a ‎pin's pull is set to Pull.UP, the LED is off. When a pin's pull is set ‎to Pull.DOWN, the pin is tied to ground and the LED turns on.‎

‎Download File

Copy Code
#  setup pins for the traffic light LEDs
red_light = DigitalInOut(board.A1)
yellow_light = DigitalInOut(board.A2)
green_light = DigitalInOut(board.A3)
#  array of LEDs
lights = [red_light, yellow_light, green_light]
#  the traffic light is common anode
#  the pins will need to be pulled down to ground
#  to turn on the LEDs. they are setup as inputs
#  so that the pull can be toggled
#  Pull.UP turns the LEDs off to start
for light in lights:
    light.direction = Direction.INPUT
    light.pull = Pull.UP

PinAlarm

The ESP32-S2 has the ability to use deep_sleep and light_sleep to save ‎battery life. sleep can be exited with alarms using the alarm library. ‎One type of alarm is a PinAlarm where if a pin's state changes, ‎then sleep is interrupted. In this case, the button's pin is setup ‎as pin_alarm.‎

‎Download File

Copy Code
#  button pin setup
pin_alarm = alarm.pin.PinAlarm(pin=board.A0, value=False, pull=True)

Variables

count and last_count keep track of the button presses. ‎The count determines which LED in the traffic light is turned on.‎

‎Download File‎

Copy Code
#  count to track which light is on
count = 2
#  tracks the last light
last_count = 1

The Loop

In the loop, count increases by 1 for a range of 0 to 2. The last LED ‎that was turned on has its pull set to Pull.UP to turn it off. The current ‎LED is turned on by setting its pull to Pull.DOWN. Finally, the ESP32-S2 ‎goes into light_sleep to preserve battery life. It will stay in this state ‎until the button is pressed again. Once the button is pressed, the ‎loop will repeat.‎

‎Download File‎

Copy Code
while True:
    #  increase count by 1, loop through 0-2
    count = (count+1) % 3
    #  turn off the last LED
    lights[last_count].pull = Pull.UP
    #  turn on the current LED
    lights[count].pull = Pull.DOWN
    #  print(count)
    #  delay to keep count
    time.sleep(1)
    #  reset last LED for next loop
    last_count = count
    #  go into light sleep mode until button is pressed again
    alarm.light_sleep_until_alarms(pin_alarm)

Solder the ESP32-S2 and Lipoly ‎Charger BFF

solder_16

Solder the short end of the headers to the LiPo BFF.‎

short_17

Place the QT Py ESP32-S2 onto the headers on the LiPo BFF. Make ‎sure that the pins are matched. The QT Py's USB port should be on ‎the other side of the LiPo BFF's LiPo port. ‎

Solder the QT Py to the headers.‎

place_18

Your QT Py ESP32-S2 is ready to be battery-powered!‎

ready_19

Wiring

wiring_20

Button

Cut, splice, and tin two pieces of wire.‎

cut_21

Solder the wires to the button. The wires should be soldered to leads ‎diagonal from each other.‎

solder_22

Apply heat shrink to the button's solder connections.‎

apply_23

Solder one wire to the QT Py ESP32-S2's GND pin. Solder the second ‎wire to pin A0.

apply_23a

Traffic Light

Tin the traffic light's four wires.‎

tin_24

Insert the traffic light's wires through the 3D printed case's mounting ‎hole.‎

insert_25

insert_26

Solder the traffic light's wires to the QT Py ESP32-S2:‎

  • Black wire to board 3V

  • Red wire to board A1

  • Yellow wire to board A2

  • Green wire to board A3

wires_27

And that completes the wiring!‎

complete_28

Assembly

Push the button into the side cutout in the badge case.‎

assembly_29

Insert the QT Py ESP32-S2 into the holder in the bottom lid of the ‎case.‎

holder_30

Plug a lipo battery into the LiPo BFF board.‎

plug_31

That completes the assembly!‎

completes_32

Usage

usage_33

Flip the switch on the LiPo BFF and you're ready to use your traffic ‎light badge. Press the button on the side to change the color of the ‎traffic light.‎

You can plug a STEMMA QT cable into the QT Py ESP32-S2 and route ‎it to the top of the badge housing.‎

cable_34

You can use the STEMMA cable to plug in SAO badge add-ons...‎

addon_35

Your favorite artisanal LEDs or other breadboard circuit...‎

favorite_36

Or a STEMMA sensor for extra badge functionality.‎

sensor_37

If you don't want to use a STEMMA cable, you can cover the hole with ‎the 3D printed manhole cover for a full-on cute roadside diorama.‎

manhole_38

מק"ט יצרן # 5435
MINI TRAFFIC LIGHT - 6.5CM TALL
Adafruit Industries LLC
מק"ט יצרן # 4183
SOFT SILICONE TOP 6MM PUSH-BUTTO
Adafruit Industries LLC
מק"ט יצרן # 3987
CIRCUIT PLAYGROUND LANYARD
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.