Maker.io main logo

How Adafruit developed Circuit Playground2

37

2016-07-05 | By Adafruit Industries

Circuit Playground

While you’ve probably done a bit of Googling, now is the time got to get serious about researching your idea. You’ll need to review platforms, evaluate price points, and perform a competitive analysis. Now might also be a great time to look into existing intellectual property.

In this second video Ladyada the engineer will explain how she researches potential designs:

The toughest part is often being able to get the programming itself to be accessible. Look at various online and offline tools such as Scratch, Blockly, Johnny5/Nodejs, Firmata, codebender, etc.

A lot have compatibility with Arduino which we know really well. Other hardware tools that do the same are like MaKey MaKey, CodeBug and Micro Bit (and possibly even others we haven’t seen) but they depend on a fully-online-only and/or special compiler which are not ideal. It’s good to be able to have a wide range of programming languages available ranging from Scratch up to C++.

You may ask yourself things like do I want to have Bluetooth LE, or Wi-Fi? On one hand these are great features, but on the other it will add a lot of complexities. We decided to go with Arduino as it’s the lowest-cost and/or simplest platform possible that can do what we needed.

Come up with a name and trademark then search the registry on USPTO. Hopefully you’ll have picked something brand new.

Recommended Reading

מק"ט יצרן # 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
מק"ט יצרן # 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
מק"ט יצרן # 3915
CASE PLASTIC TRANSPARENT
Adafruit Industries LLC
מק"ט יצרן # 3816
CIRCUIT PLAYGROUND BOLT-ON KIT
Adafruit Industries LLC
מק"ט יצרן # 3987
CIRCUIT PLAYGROUND LANYARD
Adafruit Industries LLC
מק"ט יצרן # 4320
BREADBOARD GENERAL PURPOSE
Adafruit Industries LLC
מק"ט יצרן # 3093
CRICKIT CIRCUIT PLAYGROUND EXP
Adafruit Industries LLC
מק"ט יצרן # 4011
CIRCUIT PLAYGROUND SNOW GLOBE KI
Adafruit Industries LLC
מק"ט יצרן # 2769
CIRCUIT PLAYGROUND EXPRESS EDUCA
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.