Maker.io main logo

How Adafruit developed Circuit Playground8

35

2016-08-15 | By Adafruit Industries

Circuit Playground

Ahhh, production time. The sweet smell of your final BOM in the air, you’re ready to start making some serious decisions. First, you’ll want to decide what demand might be—how much should you order? You’ll also need to think about the manufacturing supply chain, which will involve making decisions about board houses, manufacturers, and assembly houses.

OK – the fun time! Now that the PCB is done we panelize it for production and place orders for components. You will have to decide what amount of money you’re willing to silk into parts cost, keeping in mind you have to buy full reels to get good savings. We also order a stencil and schedule the first production run. The board is programmed into the pick and place and we run it through the machinery. Each board must then be functionally tested, and reworked if it doesn’t pass.

Recommended Reading

מק"ט יצרן # 3333
CIRCUIT PLAYGROUND EXPRESS
Adafruit Industries LLC
מק"ט יצרן # 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
מק"ט יצרן # 3915
CASE PLASTIC TRANSPARENT
Adafruit Industries LLC
מק"ט יצרן # 3816
CIRCUIT PLAYGROUND BOLT-ON KIT
Adafruit Industries LLC
מק"ט יצרן # 3987
CIRCUIT PLAYGROUND LANYARD
Adafruit Industries LLC
מק"ט יצרן # 4320
BREADBOARD GENERAL PURPOSE
Adafruit Industries LLC
מק"ט יצרן # 3093
CRICKIT CIRCUIT PLAYGROUND EXP
Adafruit Industries LLC
מק"ט יצרן # 4011
CIRCUIT PLAYGROUND SNOW GLOBE KI
Adafruit Industries LLC
מק"ט יצרן # 2769
CIRCUIT PLAYGROUND EXPRESS EDUCA
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.