Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
LVDS-Slide12

Flex circuits are suitable for very short runs, but it is difficult to shield them. They can be used as interconnects between boards within a system. If flex circuits are used, a system design engineer should closely couple the members of differential pairs where (S < W). Do not run signal pairs near the edges of the cable, as these are not balanced. Use a ground plane to establish the impedance. Use ground shield traces between the pairs if there is room. Connect these ground traces to the ground plane through vias at frequent intervals.

PTM פורסם ב: