Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Slide13

The ATS re-circulating chiller’s front panel display shows water level, pressure, and temperature during operation. The PID controller manages the system to small temperature fluctuations, enabling fast response time. The chillers are lightweight and portable, allowing the system to easily be moved to the application site. In the event of poor ventilation, a safety feature is included which provides automatic shut-off to protect the component from over pressure and compressor overload. 

PTM פורסם ב: