Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Slide3

In the ATS re-circulating chillers, the temperature of the chilled fluid can be easily set from the front panel. The front panel also shows the pressure drop between the inlet and the outlet. ATS’ chillers have a fast response time because of the precise PID control system, with small temperature fluctuations.

PTM פורסם ב: