Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List

A3987-Slide6

The current control section sets a constant current by looking at the voltage generated through the motor winding current going through the externally supplied sense resistor, R sense. The current control section then compares it to a voltage derived from an externally applied reference voltage, VREF and D to A inputs from the logic section. When VR sense equals the derived voltage from the logic section, the proper output transistor is turned off for a fixed “off-time” set by an external resistor from the logic voltage supply to R oscillator input. During the fixed off time, the current in the motor winding decays until the transistor is turned back on and the cycle starts all over again.

PTM פורסם ב: