Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
A3987-Slide3

Allegro has developed the A3987 to take the complexity out of using bipolar stepper motors in mid-voltage range positioning or motion control systems, reducing engineering development time for faster time to market. Though the use of Allegro’s unique Step and Direction translator interface; full, half, quarter and sixteenth step capability are easily implemented with just 2 digital logic level inputs (MS1 and MS2). A step logic level input (STEP), which simply requires a pulse for each step to be taken, and a direction of rotation logic level input (DIR), to set which direction the motor turns. No more: large “look up” tables, D to A outputs or complex phase, enable, or current level instructions to the motor driver are required from your micro.

PTM פורסם ב: