Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
A49xx-Slide13

During the PWM off-time the current in a full bridge can recirculate in 3 ways. Slow decay; where the current flows through the two low side drivers, fast decay; where the bridge reverses direction during the off-time causing current to decay rapidly, and mixed decay; which uses a combination of fast and slow decay.

PTM פורסם ב: