Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
A49xx-Slide3

The step and direction interface is the simplest microstepping method available. The built-in translator automatically increments state with a rising edge on the step input and the polarity on the direction pin. Two digital pins are used to select the step mode.

PTM פורסם ב: