Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Functional Description (cont’d)

After the execution of a command (busy=0) the expected data can be read as illustrated in Figure 3, or if no data is returned by the command the next command can be sent. All mandatory I2C- bus protocol features are implemented. Optional features like clock stretching and 10-bit slave address, are not supported by the sensor’s interface.

PTM פורסם ב: