Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
AS516-Slide14

Lab measurements show that at 1000 A/m, which is the maximum stress limit required by all OEMs, AS5161 and AS5162 do not show any output voltage drift over the 360 degree. A competitor part instead shows a significant voltage drift which changes over the whole output dynamic.

PTM פורסם ב: