Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Detectors-Slide19

The Analog Devices ADL5902, which was looked at a few slides back, is an example of an RMS-responding detector. It shows excellent immunity to the changing crest factors of QAM signals, has a measurement range of 60dB, temperature stability of plus and minus 0.5dB, and can be operated at frequencies up to 9GHz.

PTM פורסם ב: