Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Detectors-Slide4

RF detectors have two distinct transfer functions. The blue trace on the left has a so-called linear-in-dB transfer function. So, as the input power changes dB for dB, the output voltage, scaled on the left axis, changes by a constant amount. As a result, devices like this are generally talked about having a constant with a unit of millivolts-per-dB. In contrast to this, the black trace on the right does not have a constant millivolts-per-dB slope. Instead it appears to increase exponentially on this plot. However, if this transfer function were to be plotted on a volts out versus volts in plot, it would show a straight line. This has given rise to the term linear in volts-per-volt detector. This linear in volts-per-volt transfer function, by the way, is the transfer function that would be expected from a discrete diode-based RF Detector. RF detectors with linear in volts-per-volt transfer functions tend to have lower dynamic range due to the fact that their transfer functions flatten out at lower input power levels.

PTM פורסם ב: