Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
RF-IF-Slide10

As shown in the left graph, the ADL5320 driver amplifier does well in ACPR (Adjacent channel power ratio) performance. At an output power of 10dBm the ACPR is still very low at −70dBc, making the device particularly suitable for PA driver applications. The right-hand graph shows that the ADL5320 also provides 42dBm of OIP3 and 25.7dBm of P1dB at 2.14GHz at only 104mA.

PTM פורסם ב: