Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 16

The Q(inj) introduces a step change in output voltage when switching. The change in output voltage is a function of the amount of Q(inj) and the load capacitance, or DeltaV = Q(inj)/Cload. This leads to DC errors in system, and varies with input signal/source voltage. Q(inj) generally varies from negative to positive as the input is swept from Vss or 0V to Vdd.

PTM פורסם ב: