Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 17

Two important terms when referring to Leakage Current are Source Off or Is(off), and Drain Off or Id(off). Is(off) is the algebraic sum of leakage currents into or out of an Off channel source input and is predominately caused by parasitic reverse-bias diode junctions. Id(off) is the algebraic sum of leakage currents into or out of a disabled/off channel drain input and is mainly due to parasitic reverse-bias diode junctions.

PTM פורסם ב: