Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
atmosphere-slide13

To program firmware built from Atmosphere Developer, launch Atmosphere Programmer. This is a local programming software that programs the module from the Anaren MSDK with the project created. All that needs to be done to program is to plug the MSDK into the computer using the provided USB cable, select the project and USB port, and click “Program.” The firmware will then reside inside the MSDK’s A20737 module.

PTM פורסם ב: