Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
atmosphere-slide6

Using Atmosphere to develop a product can be broken down into a simple process: First, build the project in Atmosphere Developer, the integrated development environment. This will simultaneously build the project’s embedded firmware and software for a mobile app. From there, the project is compiled within the Atmosphere cloud server. Next, use Atmosphere Programmer -- downloadable software from Anaren -- to program the Anaren MSDK with the firmware built in Atmosphere Developer. Concurrently, the Atmosphere cloud server will have updated the Atmosphere mobile app with the mobile interface created from the project. Finally, open the Atmosphere app, connect to the Anaren MSDK, and from within the app one can control various sensors based on the project built. In that process alone, Atmosphere has enabled IoT connectivity to the device. This can be done all in under 15 minutes.

PTM פורסם ב: