Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Waterproof Connectors Slide 13

The termination options for the waterproof RJ45 panel mount jacks include IDC, PCB, and a rear RJ45 Jack. For front panel installation, place the gasket against the back of the connector flange and insert the back of the receptacle through the recommended panel cut-out.  Then insert the washers and screws through the front of the flange and tighten until the gasket is snug between the flange and panel.

PTM פורסם ב: