Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
temp-sensor-slide5

AT30TS75 is a drop-in software and hardware compatible temperature sensor to the industry standard LM75, TS75 and TMP75 series devices, but it also provides unique features not available in all of the legacy devices. One of these new features is a one-shot mode which allows the device to be turned on only when necessary and is ideal for battery powered applications. In addition to power savings, the AT30TS75 also provides an SMBus timeout mode to improve system reliability.

PTM פורסם ב: