Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
temp-sensor-slide7

Similar to the AT30TS750 temperature sensor, the AT30TSE752, 754, and 758 are supersets of the 750 device. In addition to all the features of the TS750 device, the TS752, 754, and 758 devices also integrate 2-Kbits, 4-Kbits, and 8-Kbits of EEPROM respectively. They are also available in the same package styles as the TS75. The EEPROM can store configuration and threshold settings to ensure the system operates in known preset conditions. This enhances product reliability, reduces manufacture’s liability from user mis-configuration as well as storing critical customer product data.

PTM פורסם ב: