Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Slide5
This curve was generated using a 1 V/µs slew rate ramp. This provides a good description of how the device will behave under transient conditions. Note that as the voltage across the device is increased beyond the current trigger threshold, the current through the device will slowly increase. This is analogous to the voltage across a TVS diode increasing as the current through it increases.
PTM פורסם ב: