Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Slide15
These two photographs clearly demonstrate the dramatic reduction in the stress level that the physical layer device (PHY) would be subjected to when the TCS-DL004-250-WH is used. In the left hand photo, only a 5 V TVS diode is used to protect the PHY. It can be seen that the peak voltage across the differential signal input to the PHY is just over 12 V while the peak current into the PHY is ~4 A. When the TCS-DL004-250-WH is added to the circuit, Bourns first noticed the dramatic reduction in the PHY input current. After the initial peak of 0.5 A, it quickly (<50 ns) folds back to ~250 mA. The TCS™ device also provides voltage isolation between the TVS diode and the PHY under protection.
PTM פורסם ב: