Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
ip chart
IP ratings are presented as a 2-digit number that follows the letters IP. The first digit denotes the protection from particles. The second digit expresses the level of protection from liquids. As with NEMA, there are specific tests that have been established to verify the manufacturer’s claims. So, for example, a product that is tested and rated as IP65 is dust tight and also protects against powerful water jets that are sprayed on the box.
PTM פורסם ב: